Hi Experts,
The Linux SDK versions are only installable in Ubuntu 12 and 10. Near future any possibility for the support in Ubuntu 14 or is still there is any way to do it ?
What is the reason behind not supporting for Ubuntu 14 ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI lyf sci,
The recommended versions are Ubuntu 10.04 LTS or Ubuntu 12.04 LTS.
It is not that you cannot use the latest version, 14.04. You can give it a try by going through the script file and modify it accordingly and also it would be helpful to the community if you are able to dod so.
We are not sure when will be the next release of LINUX SDK happen as it depends on lot of factors like number of bugs reported in Linux SDK e.t.c.
Regards,
Shankari
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
--------------------------------------------------------------------------------------------------------