This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

openmp c6678

I do an experiment on ccs,on which I run an openmp program ,but I met some questions ,please help me.

  1. I run the Helloworld Demo on our ownboard,the project could run successfully on simulator ,but failed on emulator,with the mistake ipc_attach ,and how to solve it?
  2. I can not find the omp_config_oe66,and where is the library.  
  3.  . I used the ti.omp.examples.platforms.evm.6678 ,and what is the relationship between it and ti/omp-1-01-03-02/packages/ti/omp/platform/evm6678?  
  4. I want to know how to modify the platform ,and I want to use our own general board .Because the DDR’S address  range on evm is from 0x80000000 to 0x9fffffff,but on our general board is from ox80000000 to 0xffffffff .And the MSMSRAM_Nocache on EVM is oxa0100000,but on the general board is 0x50000000.How to modify theXDC script ?

        5.The tools I used are as the following :

Compiler version :TI v7.4.1

IPC           :1.25.0.04

MCSDK PDK TMS320C6678 : 1.1.2.6

OpenMP BIOS runtime library:1.1.3.0.2

SYS/BIOS     :6.34.2.18

Are there problems about the tools I used?

I am a beginner,with many problems,and I am very appreciated with your timely and patient reply.