Other Parts Discussed in Thread: TPS65217
Dear TI E2E community,
Actually I was using dts was unable to succeeed TI sdk 7 BSP,
since my reference uda134x.c driver code is already implemented based on board file concept so I switched to ti sdk 6 & did the necessary changes as below hoping should work staright forward,
I am porting uda134x.c audio codec driver (already ported for mach-mini2440.c & s3c24xx_uda134x.c based on board file) in TI SDK 6 for which I have added the platform data in the board-am335xevm.c & I have done the necessary changes that is to be done in davinci-evm.c as shown below, but the problem is my client driver i., uda134x.c is not getting invoked, & I have attached the logs also below,
Could anybody please kindly do the needful & would appreciate a lot if anybody points out whether am missing any configuration in this board file ie.,board-am335xevm.c or davinci-evm.c file inorder to get my client driver invoked & get sound card registered & pcm nodes created
Kindly do the needful as early as possible, as am struggling from past 4 weeks & stuck with it, still am unable to proceed further
board-am335xevm.c
==================
#include <sound/uda134x.h>
struct am335x_uda134x_platform_data {
int l3_clk;
int l3_mode;
int l3_data;
void (*power) (int);
int model;
};
static struct am335x_uda134x_platform_data am335x_audio_pins = {
.l3_clk = GPIO_TO_PIN(0, 10), //10,//S3C2410_GPB(4),GPIO_TO_PIN(0, 10)
.l3_mode = GPIO_TO_PIN(2, 17),//81,//S3C2410_GPB(2),GPIO_TO_PIN(2, 17)
.l3_data = GPIO_TO_PIN(0, 8),//8,//S3C2410_GPB(3),GPIO_TO_PIN(0, 8)
.model = UDA134X_UDA1345
};
static struct platform_device am335x_audio = {
.name = "davinci_evm",
.id = 0,
.dev = {
.platform_data = &am335x_audio_pins,
},
};
static struct platform_device uda1345_codec = {
.name = "uda134x-codec",
.id = -1,
};
static void am335x_audio_init(int evm_id, int profile)
{
int err;
err = platform_device_register(&am335x_audio);
if (err) {
printk("failed to register am335x_audio_init PLATFORM DATA FOR UDA134X IN AM335X BOARD FILE\n");
}
else
{
printk("SUCCESSFULL am335x_audio_init PLATFORM DATA FOR UDA134X IN AM335X BOARD FILE\n");
}
}
static void uda134x_audio_init(int evm_id, int profile)
{
int err;
err = platform_device_register(&uda1345_codec);
if (err) {
printk("failed to register uda134x_audio_init PLATFORM DATA FOR UDA134X IN AM335X BOARD FILE\n");
}
else
{
printk("SUCCESSFULL uda134x_audio_init PLATFORM DATA FOR UDA134X IN AM335X BOARD FILE\n");
}
}
static u8 am335x_iis_serializer_direction0[] = {
INACTIVE_MODE, INACTIVE_MODE, TX_MODE, RX_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
};
static struct snd_platform_data am335x_evm_snd_data0 = {
.tx_dma_offset = 0x46000000, /* McASP0 */
.rx_dma_offset = 0x46000000,
.op_mode = DAVINCI_MCASP_IIS_MODE,
.num_serializer = ARRAY_SIZE(am335x_iis_serializer_direction0),
.tdm_slots = 2,
.serial_dir = am335x_iis_serializer_direction0,
.asp_chan_q = EVENTQ_2,
.version = MCASP_VERSION_3,
.txnumevt = 32,
.rxnumevt = 32,
.get_context_loss_count =
omap_pm_get_dev_context_loss_count,
};
/* Module pin mux for mcasp0 */
static struct pinmux_config mcasp0_pin_mux[] = {
{"mcasp0_ahclkx.mcasp0_ahclkx", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLDOWN}, //sysclk / mclk
{"mcasp0_aclkx.mcasp0_aclkx", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLDOWN}, // bck
{"mcasp0_fsx.mcasp0_fsx", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLDOWN}, //ws
{"mcasp0_axr0.mcasp0_axr0", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLDOWN},//datao
{"mcasp0_axr1.mcasp0_axr1", OMAP_MUX_MODE0 |
AM33XX_PIN_INPUT_PULLDOWN}, // datai
{NULL, 0},
};
/* Setup McASP 0 */
static void mcasp0_init(int evm_id, int profile)
{
/* Configure McASP */
setup_pin_mux(mcasp0_pin_mux);
switch (evm_id) {
case EVM_SK:
am335x_register_mcasp(&am335x_evm_sk_snd_data1, 1);
break;
default:
am335x_register_mcasp(&am335x_evm_snd_data0, 1);
}
return;
}
/* Beaglebone Black */
static struct evm_dev_cfg beagleboneblack_dev_cfg[] = {
{am335x_rtc_init, DEV_ON_BASEBOARD, PROFILE_NONE},
{clkout2_enable, DEV_ON_BASEBOARD, PROFILE_NONE},
{tps65217_init, DEV_ON_BASEBOARD, PROFILE_NONE},
{mii1_init, DEV_ON_BASEBOARD, PROFILE_NONE},
{usb0_init, DEV_ON_BASEBOARD, PROFILE_NONE},
{usb1_init, DEV_ON_BASEBOARD, PROFILE_NONE},
{mmc1_emmc_init, DEV_ON_BASEBOARD, PROFILE_NONE},
{mcasp1_init, DEV_ON_DGHTR_BRD, PROFILE_NONE},
{mcasp0_init, DEV_ON_DGHTR_BRD, PROFILE_NONE},
{am335x_audio_init, DEV_ON_DGHTR_BRD, PROFILE_NONE},
{uda134x_audio_init, DEV_ON_DGHTR_BRD, PROFILE_NONE},
{mmc0_init, DEV_ON_BASEBOARD, PROFILE_NONE},
{i2c1_init, DEV_ON_BASEBOARD, PROFILE_NONE},
{i2c2_init, DEV_ON_BASEBOARD, PROFILE_NONE},
{sgx_init, DEV_ON_BASEBOARD, PROFILE_NONE},
{NULL, 0, 0},
};
static struct platform_device *audio_devices[] __initdata = {
&am335x_audio,
&uda1345_codec,
};
/* BeagleBone Black */
static void setup_beagleboneblack(void)
{
pr_info("The board is a AM335x Beaglebone Black.\n");
/* Beagle Bone has Micro-SD slot which doesn't have Write Protect pin */
am335x_mmc[0].gpio_wp = -EINVAL;
platform_add_devices(audio_devices, ARRAY_SIZE(audio_devices));
_configure_device(BEAGLE_BONE_BLACK, beagleboneblack_dev_cfg,
PROFILE_NONE);
/* TPS65217 regulator has full constraints */
regulator_has_full_constraints();
am33xx_cpsw_init(AM33XX_CPSW_MODE_MII, NULL, NULL);
}
sound/soc/davinci/davinci-evm.c
===============================
#include <linux/gpio.h>
#include <sound/uda134x.h>
#include <sound/l3.h>
//#include "uda134x.h"
#define AUDIO_FORMAT (SND_SOC_DAIFMT_DSP_B | \
SND_SOC_DAIFMT_CBM_CFM | SND_SOC_DAIFMT_IB_NF)
struct am335x_uda134x_platform_data {
int l3_clk;
int l3_mode;
int l3_data;
void (*power) (int);
int model;
};
static struct am335x_uda134x_platform_data *am335x_uda134x_l3_pins;
/* Common DAPM widgets */
static const struct snd_soc_dapm_widget uda134x_dapm_widgets[] = {
SND_SOC_DAPM_INPUT("VINL1"),
SND_SOC_DAPM_INPUT("VINR1"),
//SND_SOC_DAPM_INPUT("VINL2"),
//SND_SOC_DAPM_INPUT("VINR2"),
SND_SOC_DAPM_OUTPUT("VOUTL"),
SND_SOC_DAPM_OUTPUT("VOUTR"),
};
static const struct snd_soc_dapm_route uda134x_dapm_routes[] = {
{ "ADC", NULL, "VINL1" },
{ "ADC", NULL, "VINR1" },
//{ "ADC", NULL, "VINL2" },
//{ "ADC", NULL, "VINR2" },
{ "VOUTL", NULL, "DAC" },
{ "VOUTR", NULL, "DAC" },
};
static int evm_uda134x_init(struct snd_soc_pcm_runtime *rtd)
{
struct snd_soc_codec *codec = rtd->codec;
struct snd_soc_dapm_context *dapm = &codec->dapm;
//struct device_node *np = codec->card->dev->of_node;
//int ret;
printk(KERN_ALERT "evm_uda134x_init DAVINCIEVM.C DEBUG: Passed %s %d \n",__FUNCTION__,__LINE__);
snd_soc_dapm_new_controls(dapm, uda134x_dapm_widgets,
ARRAY_SIZE(uda134x_dapm_widgets));
/* Set up davinci-evm specific audio path audio_map */
printk("DAVINCIIIIIIIIIII UDA134XXXXX DAPM ROUTING\n");
snd_soc_dapm_add_routes(dapm, uda134x_dapm_routes, ARRAY_SIZE(uda134x_dapm_routes));
#if 0
/* not connected */
snd_soc_dapm_disable_pin(dapm, "MONO_LOUT");
snd_soc_dapm_disable_pin(dapm, "HPLCOM");
snd_soc_dapm_disable_pin(dapm, "HPRCOM");
/* always connected */
snd_soc_dapm_enable_pin(dapm, "Headphone Jack");
snd_soc_dapm_enable_pin(dapm, "Line Out");
snd_soc_dapm_enable_pin(dapm, "Mic Jack");
snd_soc_dapm_enable_pin(dapm, "Line In");
#endif
return 0;
}
static struct snd_soc_dai_link am335x_evm_dai = {
.name = "UDA134X",
.stream_name = "UDA134X",
.codec_name = "uda134x-codec",
.codec_dai_name = "uda134x-hifi",
.cpu_dai_name = "davinci-mcasp.0",
.ops = &evm_ops,
.platform_name = "davinci-pcm-audio",
.init = evm_uda134x_init,
};
static void setdat(int v)
{
gpio_set_value(am335x_uda134x_l3_pins->l3_data, v > 0);
}
static void setclk(int v)
{
gpio_set_value(am335x_uda134x_l3_pins->l3_clk, v > 0);
}
static void setmode(int v)
{
gpio_set_value(am335x_uda134x_l3_pins->l3_mode, v > 0);
}
/* FIXME - This must be codec platform data but in which board file ?? */
static struct uda134x_platform_data am335x_uda134x = {
.l3 = {
.setdat = setdat,
.setclk = setclk,
.setmode = setmode,
.data_hold = 1,
.data_setup = 1,
.clock_high = 1,
.mode_hold = 1,
.mode = 1,
.mode_setup = 1,
},
};
static int am335x_uda134x_setup_pin(int pin, char *fun)
{
if (gpio_request(pin, "am335x_uda134x") < 0) {
printk(KERN_ERR "AM335X_UDA134X SoC Audio: "
"l3 %s pin already in use", fun);
return -EBUSY;
}
gpio_direction_output(pin, 0);
return 0;
}
static int davinci_evm_probe(struct platform_device *pdev)
{
struct snd_soc_card *evm_snd_dev_data;
int index = 0;
int ret;
printk(KERN_INFO "DAVINCIIIIIIIII_EVMMM_PROBEEEEEEEEEE SoC Audio driver\n");
if (machine_is_am335xevm()) {
printk(KERN_INFO "davinci_evm_probe machine_is_am335xevm SoC Audio driver\n");
evm_snd_dev_data = &am335x_snd_soc_card;
index = 0;
}
else{
printk(KERN_INFO "NOTTTTTTTTTTTTT machine_is_am335xevm())))))))))))))))))))))))))))) SoC Audio driver\n");
return -EINVAL;
}
#if 1
am335x_uda134x_l3_pins = pdev->dev.platform_data;
if (am335x_uda134x_l3_pins == NULL) {
printk(KERN_ERR "AM335X_UDA134X SoC Audio: "
"unable to find platform data\n");
return -ENODEV;
}
am335x_uda134x.power = am335x_uda134x_l3_pins->power;
am335x_uda134x.model = am335x_uda134x_l3_pins->model;
printk("am335x_uda134x_l3_pins->l3_clk %d\n",am335x_uda134x_l3_pins->l3_clk);
printk("am335x_uda134x_l3_pins->l3_data %d\n", am335x_uda134x_l3_pins->l3_data);
printk("am335x_uda134x_l3_pins->l3_mode %d\n", am335x_uda134x_l3_pins->l3_mode);
printk("am335x_uda134x_l3_pins->power %d\n", am335x_uda134x_l3_pins->power);
printk("am335x_uda134x_l3_pins->model %d\n", am335x_uda134x_l3_pins->model);
printk("am335x_uda134x.power %d\n", am335x_uda134x.power);
printk("am335x_uda134x.model %d\n", am335x_uda134x.model);
if (am335x_uda134x_setup_pin(am335x_uda134x_l3_pins->l3_data,
"data") < 0)
return -EBUSY;
if (am335x_uda134x_setup_pin(am335x_uda134x_l3_pins->l3_clk,
"clk") < 0) {
gpio_free(am335x_uda134x_l3_pins->l3_data);
return -EBUSY;
}
if (am335x_uda134x_setup_pin(am335x_uda134x_l3_pins->l3_mode,
"mode") < 0) {
gpio_free(am335x_uda134x_l3_pins->l3_data);
gpio_free(am335x_uda134x_l3_pins->l3_clk);
return -EBUSY;
}
#endif
evm_snd_device = platform_device_alloc("soc-audio", -1);
if (!evm_snd_device)
{
printk(KERN_ALERT "FAILUREEEEEE davinci_evm_probe DAVINCIEVM.C DEBUG: Passed %s %d \n",__FUNCTION__,__LINE__);
return -ENOMEM;
}
else
{
printk(KERN_ALERT "SUCCESSFULLL davinci_evm_probe DAVINCIEVM.C DEBUG: Passed %s %d \n",__FUNCTION__,__LINE__);
}
platform_set_drvdata(evm_snd_device, evm_snd_dev_data);
ret = platform_device_add_data(evm_snd_device, &am335x_uda134x, sizeof(am335x_uda134x));
printk(KERN_ALERT " davinci_evm_probe platform_device_add_data %d \n",ret);
ret = platform_device_add(evm_snd_device); /////problemmmmmmmmmmm
if (ret)
{
printk(KERN_ALERT "SUCCESSFULLL davinci_evm_probe platform_device_add %d \n",ret);
platform_device_put(evm_snd_device);
}
else
{
printk(KERN_ALERT "FAILUREEEEEEE davinci_evm_probe platform_device_add %d \n",ret);
}
return ret;
}
static int davinci_evm_remove(struct platform_device *pdev)
{
#if 1
gpio_free(am335x_uda134x_l3_pins->l3_data);
gpio_free(am335x_uda134x_l3_pins->l3_clk);
gpio_free(am335x_uda134x_l3_pins->l3_mode);
#endif
return 0;
}
static struct platform_driver davinci_evm_driver = {
.probe = davinci_evm_probe,
.remove = davinci_evm_remove,
.driver = {
.name = "davinci_evm",
.owner = THIS_MODULE,
.pm = &snd_soc_pm_ops,
},
};
static int __init evm_init(void)
{
struct snd_soc_card *evm_snd_dev_data;
int index;
int ret;
printk(KERN_INFO "DAVINCIIIIIIII_EVMMMMMMM_INITTTTTT_UDA134X SoC Audio driver\n");
return platform_driver_register(&davinci_evm_driver); // added for uda134x
if (machine_is_davinci_evm()) {
evm_snd_dev_data = &dm6446_snd_soc_card_evm;
index = 0;
} else if (machine_is_davinci_dm355_evm()) {
evm_snd_dev_data = &dm355_snd_soc_card_evm;
index = 1;
} else if (machine_is_davinci_dm365_evm()) {
evm_snd_dev_data = &dm365_snd_soc_card_evm;
index = 0;
} else if (machine_is_davinci_dm6467_evm()) {
evm_snd_dev_data = &dm6467_snd_soc_card_evm;
index = 0;
} else if (machine_is_davinci_da830_evm()) {
evm_snd_dev_data = &da830_snd_soc_card;
index = 1;
} else if (machine_is_davinci_da850_evm()) {
evm_snd_dev_data = &da850_snd_soc_card;
index = 0;
} else if (machine_is_am335xevm()) {
evm_snd_dev_data = &am335x_snd_soc_card;
#ifdef CONFIG_MACH_AM335XEVM
if (am335x_evm_get_id() == EVM_SK)
evm_snd_dev_data = &am335x_evm_sk_snd_soc_card;
#endif
index = 0;
} else
return -EINVAL;
evm_snd_device = platform_device_alloc("soc-audio", index);
if (!evm_snd_device)
return -ENOMEM;
platform_set_drvdata(evm_snd_device, evm_snd_dev_data);
ret = platform_device_add(evm_snd_device);
if (ret)
platform_device_put(evm_snd_device);
return ret;
}
logs:
[ 13.625000] DAVINCIIIIIIII_EVMMMMMMM_INITTTTTT_UDA134X SoC Audio driver
[ 13.631958] DAVINCIIIIIIIII_EVMMM_PROBEEEEEEEEEE SoC Audio driver
[ 13.638336] davinci_evm_probe machine_is_am335xevm SoC Audio driver
[ 13.644897] am335x_uda134x_l3_pins->l3_clk 10
[ 13.649444] am335x_uda134x_l3_pins->l3_data 8
[ 13.653991] am335x_uda134x_l3_pins->l3_mode 81
[ 13.658630] am335x_uda134x_l3_pins->power 0
[ 13.662994] am335x_uda134x_l3_pins->model 4
[ 13.667388] am335x_uda134x.power 0
[ 13.670928] am335x_uda134x.model 4
[ 13.674499] SUCCESSFULLL davinci_evm_probe DAVINCIEVM.C DEBUG: Passed davinci_evm_probe 524
[ 13.683319] davinci_evm_probe platform_device_add_data 0
[ 13.689056] SUCCESSFULLLL platform_device_add if (!pdev) DEBUG: Passed platform_device_add 275
[ 13.698272] pdev->id == -1 platform_device_add DEBUG: Passed platform_device_add 294 0
[ 13.706542] Registering platform device 'soc-audio'. Parent at platform
[ 13.713684] FAILUREEEEEEE davinci_evm_probe platform_device_add 0
Awaiting for your replies,
Many Many thanks in advance