This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need u-boot source code for DM8168 platform



Hi Team, 

Please suggest me the link where i can download U-boot source code. And also if possible please suggest me some good documentation to build U-boot for SPI.

Thanks in Advance!

BR

Ajay

  • Hi Ajay,

    First of all, you are using wrong forum, I will move this thread to the DM816x.

    Ajay Kumar KR said:
    Please suggest me the link where i can download U-boot source code.

    You can take the latest u-boot version from the below link:

    If you are planning to use DVR RDK, you can get u-boot from:

    Click on the most upper right "snapshot" button, download and extract the tar file. Thus you will have the source code.

    Other option is to download the latest DM816x EZSDK which comes with older version of the u-boot:

    The u-boot source will be in folder ti-ezsdk_dm816x-evm_5_05_02_00/board-support/u-boot-2010.06-psp04.04.00.01/

    Ajay Kumar KR said:
    And also if possible please suggest me some good documentation to build U-boot for SPI.

    See the below wiki:

    Regards,
    Pavel