This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm388 ipnc end-to-end latency measurement

Other Parts Discussed in Thread: DM388

Hi!

I'm testing tmdsipcam388imx136

I try to repeat measurements according to IPNC_RDK_InstallGuide.pdf. Firware is ubifs_ipnc_low_power (also try full future ) from IPNC_RDK_V3.8.0 (dir: Binaries/DM388/Rev2/nand/IMX136_Appro).

Using VLC Player 2.0.3 (and others) on Win7(x64)  Best result: 320 ms End-To-End Latency (more often = 400 ms).

If I use iexplorer activeX player (GoDB IPNCWebDlls.CAB) best result is 160 ms (more often = 200 ms) (at other equal conditions). According to pdf, result must be 141 ms on VLC player. Camera setups: VNF_SPEED SINGLESTREAM SINGLE_H264 APPRO2A AEWB 1080P_D1 H264 HIGH_SPEED1. 

Where is mistake?

The picture in pdf don't look like a vlc player