I was using a Beaglebone Black as a pulse generator for controlling scientific experiment timing and was wondering if there is any data on the timing precision of the PRU.
I know that the clock cycle is 200 MHz and so 5 ns instruction time but if I set a continuous series of pulses at a particular frequency I'm interested in the uncertainty in the time between pulses. I have access to a 2 GHz oscilloscope but haven't seen any jitter/deviation from the set frequency on a sample of pulses to the nearest 500 ps.