Hi,
I have questions about AM437x and PMIC TPS65218.
1. To run the AM437x in Nitro(OPP), the typical voltage is 1.325V. But TPS65218 can't output 1.325V.
The closest voltage which TPS65218 can output are 1.320V or 1.330V.
Both voltage satisfies the specification of AM437x, but which voltage should be chosen?
2. Question about the following AM437x Power Supply pins.
*CAP_VDDS1P8V_IOLDO (BALL Number:D6)
*VDDS3P3V_IOLDO (BALL Number:F8)
What should be connected to these two power supply pins?
In the GP EVM, CAP_VDDS1P8V_IOLDO is unconnected and VDDS3P3V_IOLDO is connected to the GND.
But in the Industrial EVM(IDK), it seem that CAP_VDDS1P8V_IOLDO is connected to VDDS pins and 3.3V is supplied to VDDS3P3V_IOLDO.
3. In the schematic of GP EVM and IDK, the following pins are separated from other VDDS/VDD_CORE and is processed.
Is this means the following pins need some special processing?
*AD8 pin (VDDS)
*AD9 pin (VDD_CORE)
*AD12 pin (VDSS)
In GP EVM and IDK, Ferrite Beads is connected to AD12 pin but it is not connected to other VDDS pins.
And in IDK, decoupling capacitor(0.01uF) is connected to AD8 pin and AD9 pin but
it isn't connected to other VDDS and VDD_CORE pin.
best regards,
g.f.