Other Parts Discussed in Thread: TEST2
Hello,
I am working on C66XX multicore DSP processor using CCS 5.1.1.00031.
I want to align individual elements of structure by 128 bytes.
For Example:
typedef struct
{
uint8_t array1[20];
uint32_t array2[32];
}Test1_s;
typedef struct
{
uint8_t array3[20];
uint32_t array4[32];
}Test2_s;
typedef struct
{
Test1_s Test1 ;
Test2_s Test2 ;
}Test3_s;
I want to align Test1 and Test2 by 128 bytes.
#pragma DATA_ALIGN (Test2, 128)
#pragma DATA_ALIGN (Test1, 128)
#pragma DATA_ALIGN (gTest, 128)
Test3_s gTest = {0};
But it is not working and showing warning as :
#837-D pragma can only be applied to a file level symbol, not 'Test1'
#837-D pragma can only be applied to a file level symbol, not 'Test2'
Thanks,
Aman