Other Parts Discussed in Thread: AM1705, AM1707, OMAPL138, OMAP-L138, AM3354
Hi, I'm currently trying to design a board using the AM1705 processor, because it seems like this is the only chip I can find that has a hand-solderable package (non-bga) and can still run Linux. I don't want to use uCLinux on a microcontroller.
Is there any way to boot this device from removable media such as an SD card?
There is a boot configuration mode for SPI, could I boot from the SD card via SPI?