Hi,
I created a CCS minimum example project of DSP/BIOS, then enabled the clock module and added an instance using the GUI tool, then compiled and debugged the project, but found the clock instance had never been fired.
Then I found a example in the resource explorer, found that the clock instance is run-time created and obviously it works.
So my question is that why the static configured clock instance won't work? if that's mean to be then the GUI tool seem make no sense anymore.
Here is the code and the cfg file: any conments are appreciated.
/* * ======== main.c ======== */ #include <xdc/std.h> #include <xdc/runtime/System.h> #include <ti/sysbios/BIOS.h> #include <ti/sysbios/knl/Task.h> #include <ti/sysbios/knl/Clock.h> /* * ======== taskFxn ======== */ Void taskFxn(UArg a0, UArg a1) { System_printf("enter taskFxn()\n"); while (1) { Task_sleep(500); System_flush(); } } /* * ======== clk0Fxn ======= */ Void clk0Fxn(UArg arg0) { UInt32 time; time = Clock_getTicks(); if (time % 1000 == 0) { System_printf("System time in clk0Fxn = %lu\n", (ULong)time); } } /* * ======== main ======== */ Int main() { /* * use ROV->SysMin to view the characters in the circular buffer */ System_printf("enter main()\n"); BIOS_start(); /* does not return */ return(0); }
===========================================
var Defaults = xdc.useModule('xdc.runtime.Defaults'); var Diags = xdc.useModule('xdc.runtime.Diags'); var Error = xdc.useModule('xdc.runtime.Error'); var Log = xdc.useModule('xdc.runtime.Log'); var LoggerBuf = xdc.useModule('xdc.runtime.LoggerBuf'); var Main = xdc.useModule('xdc.runtime.Main'); var SysMin = xdc.useModule('xdc.runtime.SysMin'); var System = xdc.useModule('xdc.runtime.System'); var Text = xdc.useModule('xdc.runtime.Text'); var BIOS = xdc.useModule('ti.sysbios.BIOS'); var Hwi = xdc.useModule('ti.sysbios.hal.Hwi'); var Task = xdc.useModule('ti.sysbios.knl.Task'); var Clock = xdc.useModule('ti.sysbios.knl.Clock'); /* * Uncomment this line to globally disable Asserts. * All modules inherit the default from the 'Defaults' module. You * can override these defaults on a per-module basis using Module.common$. * Disabling Asserts will save code space and improve runtime performance. Defaults.common$.diags_ASSERT = Diags.ALWAYS_OFF; */ /* * Uncomment this line to keep module names from being loaded on the target. * The module name strings are placed in the .const section. Setting this * parameter to false will save space in the .const section. Error and * Assert messages will contain an "unknown module" prefix instead * of the actual module name. */ Defaults.common$.namedModule = false; /* * Minimize exit handler array in System. The System module includes * an array of functions that are registered with System_atexit() to be * called by System_exit(). */ System.maxAtexitHandlers = 4; /* * Uncomment this line to disable the Error print function. * We lose error information when this is disabled since the errors are * not printed. Disabling the raiseHook will save some code space if * your app is not using System_printf() since the Error_print() function * calls System_printf(). Error.raiseHook = null; */ /* * Uncomment this line to keep Error, Assert, and Log strings from being * loaded on the target. These strings are placed in the .const section. * Setting this parameter to false will save space in the .const section. * Error, Assert and Log message will print raw ids and args instead of * a formatted message. */ Text.isLoaded = false; /* * Uncomment this line to disable the output of characters by SysMin * when the program exits. SysMin writes characters to a circular buffer. * This buffer can be viewed using the SysMin Output view in ROV. */ SysMin.flushAtExit = false; /* * The BIOS module will create the default heap for the system. * Specify the size of this default heap. */ BIOS.heapSize = 0x0; /* System stack size (used by ISRs and Swis) */ Program.stack = 0x400; /* Circular buffer size for System_printf() */ SysMin.bufSize = 128; /* * Create and install logger for the whole system */ var loggerBufParams = new LoggerBuf.Params(); loggerBufParams.numEntries = 4; var logger0 = LoggerBuf.create(loggerBufParams); Defaults.common$.logger = logger0; Main.common$.diags_INFO = Diags.ALWAYS_ON; System.SupportProxy = SysMin; /* * Build a custom BIOS library. The custom library will be smaller than the * pre-built "instrumented" (default) and "non-instrumented" libraries. * * The BIOS.logsEnabled parameter specifies whether the Logging is enabled * within BIOS for this custom build. These logs are used by the RTA and * UIA analysis tools. * * The BIOS.assertsEnabled parameter specifies whether BIOS code will * include Assert() checks. Setting this parameter to 'false' will generate * smaller and faster code, but having asserts enabled is recommended for * early development as the Assert() checks will catch lots of programming * errors (invalid parameters, etc.) */ BIOS.libType = BIOS.LibType_Custom; BIOS.logsEnabled = false; BIOS.assertsEnabled = true; /* * Create a task. The 'taskFxn' function can be found in main.c. */ var task0Params = new Task.Params(); var task0 = Task.create("&taskFxn", task0Params); var clock0Params = new Clock.Params(); clock0Params.instance.name = "clock0"; clock0Params.period = 1; Program.global.clock0 = Clock.create("&clk0Fxn", 5, clock0Params);