Hi, All
My am335x based board is working fine with MT's DDR3 and Samsung's K4B2G1646C. When DDR3 is replaced with K4B2G1646Q, the board with u-boot can boot in case of power-up, but boot failed in warm reset. If WEC7+Eboot is burnt in, the board boot OK in both cases. The sdram_init function is already with parameters of K4B2G1646. With trace, I found the boot failed just after lowlevel_init and before jump to _main. Please let me know hot to fix this issue if anybody encountered similiar case. Thanks a lot.
BR
Cheng Shi
www.emtronix.com