This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does sitara ti-ezsdk-evm6.0and so on need pay for it?The system will restart while long term test.(china beaglebone black board)

Hardware platform: Beaglebone black(China)
Software platform: ti-ezsdk-6.00& 7.00.00 in ubunt2
I start the embed system study from 2014-Nov;
Issue description:
1. Long term test find, both sdk6.0 and 7.0 app will restart, the com print information without any issue report, same as power on.
2.Compared: evmsk no this issue.

I need help to confirm the root cause:
1. Does the power manage IC cause this issue?
2. Does kernel is the root cause, while the kernel is open source, and ti say its stable by test, so the kernel must not has issue.
3. And then the file system?

if the sdk has no issue at all, then is the PC ubunt2 has issue?
I want to know if sdk is full free?

It's appreciate that you can provide the detail information, thank you very much for your kindly help.