Other Parts Discussed in Thread: OMAP-L138
I have an OMAP 138 EVM Beta Kit with the C6748 SOM installed. When I plug in the USB cable (yes I'm plugging into the correct USB port), Windows identifies the hardware as dual RS232. I have tried this with the S7 dip switches all off and with S7 - 5 and 8 ON.
I have a second OMAP138 EVM board that is identified correctly as XDS100. I have rebooted the PC, power cycled the board, and I get the same result.
What could the issue be?
--John