We are power optimizing on our OMAP4430 platform. We wish to turn off some external power rails but the OMAP4430 data manual is not clear regarding which internal domains are powered by which power pins. Please provide a detailed internal power distribution document. The following need to be addressed:
VDDA_CSI21, VDDA_CSI22 -
VDDA_DSI1, VDDA_DSI2
VDDA_USBA0OTG_1P8V
VDDA_USBA0OTG_3P3V
VDDA_HDMI_VDAC
Also, we wish to power down or disable internal blocks that are not used. How do we implement that for the following blocks:
CSI2, DSI
USB OTG - can we disable OTG_1P8 and OTG_3P3 and still wake on USB insertion