Other Parts Discussed in Thread: SYSCONFIG
Hi !
I'm using a Mistral EVM Board (OMAP 3530) with Code Composer Studio 4 (CCS4), but I have some problems in configure e use SDMA with McBSP2.
I'm setting the SDMA module to be active when McBSP2_TX is asserted and start to transfer data.. I'm configuring SDMA as below:
DMA4_OCP_SYSCONFIG = 0x00000002; // Reset
while ( (DMA4_SYSSTATUS & 0x00000001) == 0); // Waits Finish Reset
DMA4_CSR10 = 0x00001FFE; // Reset Status Register
DMA4_OCP_SYSCONFIG = 0x00001028; // Clock Free Running , DMA Ignores MSuspend Signal
DMA4_CSDP10 = 0x00000001; // Select Endiness For Source And Destination
DMA4_CCR10 = 0x07081001; // Select DMA Interrupt Request , Type Of Increment
DMA4_CEN10 = 0x00000080; // 128 Elements
DMA4_CFN10 = 0x00000006; // 6 Frame
DMA4_CICR10 = 0x00000008; // Enable End Of Frame Interrupt
DMA4_CSSA10 = (unsigned int)TSP; // Source Start Address
DMA4_CDSA10 = (unsigned int)0x49022008; // Destination Start Address McBSP2_DXR
DMA4_IRQENABLE_L0 = 0x00000400; // Enable Interrupt For Channel 10
DMA4_CCR10 = DMA4_CCR10 | 0x00000080; // Enable Logical Channel
The McBSP2 is configure as below:
McBSP2_SPCR2 = 0x00000200; // Set Run Free Mode For TX And RX
McBSP2_SPCR1 = 0x00000200;
McBSP2_XCR2 = 0x00000000; // Set 8 bits Transmitter With No Delay
McBSP2_XCR1 = 0x00000040; // Set 1 Word Per Frame 8 Bits Word
McBSP2_PCR = 0x00000A0A; // Set Frame Sync Mode With Polarity Low For TX Clock Polarity Negative , SCLKME = 0
McBSP2_SRGR1 = 0x00000F01; // Setting Up Frame Sync Width (16 Bits) And Clock Divider
McBSP2_SRGR2 = 0x000012DE; // Configure Clock Settings And Frame Width , CLKSM = 0
MCBSP2_XCCR = MCBSP2_XCCR & 0xFFFFFFF7; // Set Interrupt For DMA
McBSP2_SPCR2 = McBSP2_SPCR2 | 0x00000040; // Set Interrupt For DMA
McBSP2_SPCR2 = McBSP2_SPCR2 | 0x00000080; // Enables Frame Sync Logic
McBSP2_SPCR2 = McBSP2_SPCR2 | 0x00000001; // Enables Transmitter
All these configuration are made in DSP and I'm emulating it with XDS510 in CCS4.
Could anyone see something missing or some mistake I'm making?
I'm not configuring the RTSC and DSP/Bios files in CCS4, are they nedded ?
Could be something I'm not enabling, like INTC Module?
Tanks all.
Best Regards