Hello.
We are trying to boot the c6678 EVM card using the IBL and the TFTP mode. We have no problem on using the ethernet port on the front panel (SGMII1): the IBL downloads the program properly from the server and then execute it.
On the other hand, we'd like to to the same thing using the SGMII0, i.e. the port on the AMC backplane. Unfortunately we don't find how to modify the IBL in order to use that port instead of the default one on the front panel. We suppose it should be pretty easy (some variable to be modified?). Can you help us?
This is what we've discovered so far. We've used a gel file to modify the IP addresses used by the IBL as well as the name of the files, but in that file does not seem to have nothing to modify the used interface. We can see only ibl_PORT_SWITCH_ALL that seems to enable both the ports. Furthermore, according to the ethernet switch in the crate, the ethernet link on the backplane is not enabled by the IBL.