This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

mix_tuning_database.exe missing from DCCSetup_Full.exe

I tried to install this image tuning tool program.  I got it to unpack the installer (so it accepted my licence file) and then I tried to install the program DCCSetup_Full.exe.  First I had to install MCRInstaller-7.13-Win.exe which I found on the internet somewhere and it pulled in the VC redistributable files.  When that was done, DCCSetup_Full.exe would proceed with the installation, but it had an error about a missing mix_tuning_database.exe.

I tried to ignore the error so it finished installing, but then the application complained about missing the mix_tuning_database and didn't have any plugins.