This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

delay added due to ECU in VOLIB

Hi,

Please help me to calculate the delay added due to the ECU unit in VOLIB

thanks

Ajay

  • Hi Raja,

    Two delays are included in ECU: framing delay and processing delay. Framing delay can be 5ms or 10ms depending on your configuration. The processing delay is cycles/clock rate, where the cycles can be caculated from MIPS number of ECU. For example, the C55x MIPS for 10ms frame multi-segment EC after converge is 10.22, so the cycles = 10.22M/s * 80 sample / 8KHz = 10.22M/s * 10ms = ~0.1M = 100000, and the processing delay would be 100000 / 100MHz (c5515 clock rate) = 1ms, and the total delay is framing delay 10ms + processing delay 1ms = 11ms.

    Regards,
    Garrett