Other Parts Discussed in Thread: OMAP3530, DAC7512, TCA6416, TCA8418, LM8323, LM8333, TPS65910, LP8727, BQ24190, TPS65010, TPS65090, TPS65217, TPS65218, TPS65912, TWL6040, LM3533, LP3971, LP3972, TPS51632, TPS62360, TPS65023, LM3530, LM3642, LP3944, LP5521, LP5523, LP5562, LP8501, DAC124S085, TCA6507
Hello,
We are using a custom Board with a Sitara AM335xx CPU 256MB RAM, 256MB NAND. We are using Arago with the official kernel 3.12.10 from EZSDK.
When Plugging in a Huawei E303h-2 USB dongle, usb_modeswitch triggers correctly through udev to switch the device in modem mode, the NIC appears in "ip link" however when bringing the interface up with "ip link set eth1 up" the kernel panics with an SKB BUG_ON line 98 of net/core/skbuff.c I get it each single time, sometimes with a few seconds delay. The stack trace of the Oops is always different
Do you have any idea if this is an already known issue, or how to fix it?
This is really important because our company wants to ship this IoT device with possibility to plug a 3G dongle and a WiFi+BLE dongle on top of the integrated Ethernet and PAN (ZigBee) technologies.
The Oops:
[ 67.965455] skbuff: skb_over_panic: text:c02d526c len:1555 put:1555 head:cdb43f00 data:cdb43f42 tail:0xcdb4451
[ 67.978439] ------------[ cut here ]------------
[ 67.983318] kernel BUG at net/core/skbuff.c:98!
[ 67.988103] Internal error: Oops - BUG: 0 [#1] ARM
[ 67.993172] CPU: 0 PID: 0 Comm: swapper Not tainted 3.12.17Standard #1
[ 68.000069] task: c086c420 ti: c0862000 task.ti: c0862000
[ 68.005794] PC is at skb_panic+0x54/0x60
[ 68.009939] LR is at skb_panic+0x54/0x60
[ 68.014083] pc : [<c041dfb0>] lr : [<c041dfb0>] psr: 60070193
[ 68.014083] sp : c0863e60 ip : 00000000 fp : 00000018
[ 68.026211] r10: 00000100 r9 : 00000006 r8 : c0862000
[ 68.031729] r7 : cdb44540 r6 : 00000613 r5 : cdb43f00 r4 : cdb43f42
[ 68.038624] r3 : 00000000 r2 : c088f96c r1 : 20070193 r0 : 0000007b
[ 68.045521] Flags: nZCv IRQs off FIQs on Mode SVC_32 ISA ARM Segment kernel
[ 68.053334] Control: 10c5387d Table: 8f59c019 DAC: 00000015
[ 68.059402] Process swapper (pid: 0, stack limit = 0xc0862240)
[ 68.065563] Stack: (0xc0863e60 to 0xc0864000)
[ 68.070170] 3e60: 00000613 cdb43f00 cdb43f42 cdb44555 cdb44540 cd831800 00000613 cdb44555
[ 68.078814] 3e80: 00000000 c0378424 c02d524c cd831c20 cf6b5240 cdbda200 00000000 c02d526c
[ 68.087458] 3ea0: c02d524c cf6b5240 60070113 00000000 00000000 c02e150c c0863ec8 cd914ce8
[ 68.096101] 3ec0: cd914cec c02e160c c0863ec8 c0863ec8 00000000 c088cb9c c08ba2c0 c003a1a4
[ 68.104744] 3ee0: c088eb88 00000001 00000018 c08ba31c c08ba300 c003a2e4 cf005240 c005f5dc
[ 68.113387] 3f00: c088f668 0000000a ffffa55d 00200000 00000021 60070193 00000021 00000000
[ 68.122031] 3f20: c08b9408 00000001 413fc082 00000000 00000000 c003a45c c0862000 c003a6b4
[ 68.130674] 3f40: c0895ef8 c000f250 fa200000 00000021 c0863f70 c0008770 c000f3dc c000f3d4
[ 68.139317] 3f60: 60070013 ffffffff c0863fa4 c0011bc0 ffffffed 00000000 c08a9398 00000000
[ 68.147961] 3f80: c0862000 c086a0ac c08b8847 c08b8847 00000001 413fc082 00000000 00000000
[ 68.156604] 3fa0: 01000000 c0863fb8 c000f3dc c000f3d4 60070013 ffffffff c088f770 c005eddc
[ 68.165248] 3fc0: c0aee700 c05469b0 ffffffff ffffffff c05464f0 00000000 00000000 c0574150
[ 68.173892] 3fe0: 00000000 10c53c7d c086a040 c057414c c086d550 80008070 00000000 00000000
[ 68.182559] [<c041dfb0>] (skb_panic+0x54/0x60) from [<c0378424>] (skb_put+0x4c/0x50)
[ 68.190768] [<c0378424>] (skb_put+0x4c/0x50) from [<c02d526c>] (rx_complete+0x20/0x1e8)
[ 68.199247] [<c02d526c>] (rx_complete+0x20/0x1e8) from [<c02e150c>] (__usb_hcd_giveback_urb+0x60/0xf0)
[ 68.209091] [<c02e150c>] (__usb_hcd_giveback_urb+0x60/0xf0) from [<c02e160c>] (usb_giveback_urb_bh+0x70/0xa0)
[ 68.219579] [<c02e160c>] (usb_giveback_urb_bh+0x70/0xa0) from [<c003a1a4>] (tasklet_action+0x60/0xb4)
[ 68.229329] [<c003a1a4>] (tasklet_action+0x60/0xb4) from [<c003a2e4>] (__do_softirq+0xc8/0x1ac)
[ 68.238525] [<c003a2e4>] (__do_softirq+0xc8/0x1ac) from [<c003a45c>] (do_softirq+0x48/0x54)
[ 68.247354] [<c003a45c>] (do_softirq+0x48/0x54) from [<c003a6b4>] (irq_exit+0x94/0xe0)
[ 68.255734] [<c003a6b4>] (irq_exit+0x94/0xe0) from [<c000f250>] (handle_IRQ+0x34/0x84)
[ 68.264108] [<c000f250>] (handle_IRQ+0x34/0x84) from [<c0008770>] (omap3_intc_handle_irq+0x64/0x74)
[ 68.273678] [<c0008770>] (omap3_intc_handle_irq+0x64/0x74) from [<c0011bc0>] (__irq_svc+0x40/0x50)
[ 68.283142] Exception stack(0xc0863f70 to 0xc0863fb8)
[ 68.288479] 3f60: ffffffed 00000000 c08a9398 00000000
[ 68.297123] 3f80: c0862000 c086a0ac c08b8847 c08b8847 00000001 413fc082 00000000 00000000
[ 68.305765] 3fa0: 01000000 c0863fb8 c000f3dc c000f3d4 60070013 ffffffff
[ 68.312764] [<c0011bc0>] (__irq_svc+0x40/0x50) from [<c000f3d4>] (arch_cpu_idle+0x28/0x38)
[ 68.321511] [<c000f3d4>] (arch_cpu_idle+0x28/0x38) from [<c005eddc>] (cpu_startup_entry+0x4c/0xe8)
[ 68.330994] [<c005eddc>] (cpu_startup_entry+0x4c/0xe8) from [<c05469b0>] (start_kernel+0x29c/0x2f0)
[ 68.340555] Code: e58d4008 e58de00c e59f0008 ebfff836 (e7f001f2)
[ 68.346995] ---[ end trace ccf0e1d07cd91acf ]---
[ 68.351873] Kernel panic - not syncing: Fatal exception in interrupt
[ 68.358585] Rebooting in 3 seconds..
The kernel Config:
#
# Automatically generated file; DO NOT EDIT.
# Linux/arm 3.12.17 Kernel Configuration
#
CONFIG_ARM=y
CONFIG_SYS_SUPPORTS_APM_EMULATION=y
CONFIG_HAVE_PROC_CPU=y
CONFIG_STACKTRACE_SUPPORT=y
CONFIG_HAVE_LATENCYTOP_SUPPORT=y
CONFIG_LOCKDEP_SUPPORT=y
CONFIG_TRACE_IRQFLAGS_SUPPORT=y
CONFIG_RWSEM_GENERIC_SPINLOCK=y
CONFIG_ARCH_HAS_CPUFREQ=y
CONFIG_ARCH_HAS_BANDGAP=y
CONFIG_GENERIC_HWEIGHT=y
CONFIG_GENERIC_CALIBRATE_DELAY=y
CONFIG_NEED_DMA_MAP_STATE=y
CONFIG_VECTORS_BASE=0xffff0000
CONFIG_ARM_PATCH_PHYS_VIRT=y
CONFIG_GENERIC_BUG=y
CONFIG_DEFCONFIG_LIST="/lib/modules/$UNAME_RELEASE/.config"
CONFIG_IRQ_WORK=y
CONFIG_BUILDTIME_EXTABLE_SORT=y
#
# General setup
#
CONFIG_BROKEN_ON_SMP=y
CONFIG_INIT_ENV_ARG_LIMIT=32
CONFIG_CROSS_COMPILE=""
# CONFIG_COMPILE_TEST is not set
CONFIG_LOCALVERSION="Standard"
CONFIG_LOCALVERSION_AUTO=y
CONFIG_HAVE_KERNEL_GZIP=y
CONFIG_HAVE_KERNEL_LZMA=y
CONFIG_HAVE_KERNEL_XZ=y
CONFIG_HAVE_KERNEL_LZO=y
CONFIG_HAVE_KERNEL_LZ4=y
# CONFIG_KERNEL_GZIP is not set
CONFIG_KERNEL_LZMA=y
# CONFIG_KERNEL_XZ is not set
# CONFIG_KERNEL_LZO is not set
# CONFIG_KERNEL_LZ4 is not set
CONFIG_DEFAULT_HOSTNAME="CBox"
# CONFIG_SWAP is not set
CONFIG_SYSVIPC=y
CONFIG_SYSVIPC_SYSCTL=y
CONFIG_POSIX_MQUEUE=y
CONFIG_POSIX_MQUEUE_SYSCTL=y
# CONFIG_FHANDLE is not set
# CONFIG_AUDIT is not set
#
# IRQ subsystem
#
CONFIG_GENERIC_IRQ_PROBE=y
CONFIG_GENERIC_IRQ_SHOW=y
CONFIG_HARDIRQS_SW_RESEND=y
CONFIG_GENERIC_IRQ_CHIP=y
CONFIG_IRQ_DOMAIN=y
# CONFIG_IRQ_DOMAIN_DEBUG is not set
CONFIG_IRQ_FORCED_THREADING=y
CONFIG_SPARSE_IRQ=y
CONFIG_KTIME_SCALAR=y
CONFIG_GENERIC_CLOCKEVENTS=y
CONFIG_GENERIC_CLOCKEVENTS_BUILD=y
#
# Timers subsystem
#
CONFIG_TICK_ONESHOT=y
CONFIG_NO_HZ_COMMON=y
# CONFIG_HZ_PERIODIC is not set
CONFIG_NO_HZ_IDLE=y
CONFIG_NO_HZ=y
CONFIG_HIGH_RES_TIMERS=y
#
# CPU/Task time and stats accounting
#
CONFIG_TICK_CPU_ACCOUNTING=y
# CONFIG_IRQ_TIME_ACCOUNTING is not set
CONFIG_BSD_PROCESS_ACCT=y
CONFIG_BSD_PROCESS_ACCT_V3=y
CONFIG_TASKSTATS=y
CONFIG_TASK_DELAY_ACCT=y
CONFIG_TASK_XACCT=y
CONFIG_TASK_IO_ACCOUNTING=y
#
# RCU Subsystem
#
CONFIG_TINY_RCU=y
# CONFIG_PREEMPT_RCU is not set
# CONFIG_RCU_STALL_COMMON is not set
# CONFIG_TREE_RCU_TRACE is not set
# CONFIG_IKCONFIG is not set
CONFIG_LOG_BUF_SHIFT=16
CONFIG_GENERIC_SCHED_CLOCK=y
# CONFIG_CGROUPS is not set
# CONFIG_CHECKPOINT_RESTORE is not set
CONFIG_NAMESPACES=y
CONFIG_UTS_NS=y
CONFIG_IPC_NS=y
CONFIG_USER_NS=y
CONFIG_PID_NS=y
CONFIG_NET_NS=y
CONFIG_UIDGID_STRICT_TYPE_CHECKS=y
# CONFIG_SCHED_AUTOGROUP is not set
# CONFIG_SYSFS_DEPRECATED is not set
# CONFIG_RELAY is not set
CONFIG_BLK_DEV_INITRD=y
CONFIG_INITRAMFS_SOURCE="initramfs.cpio.lzma"
CONFIG_INITRAMFS_ROOT_UID=0
CONFIG_INITRAMFS_ROOT_GID=0
CONFIG_RD_GZIP=y
CONFIG_RD_BZIP2=y
CONFIG_RD_LZMA=y
CONFIG_RD_XZ=y
CONFIG_RD_LZO=y
CONFIG_RD_LZ4=y
CONFIG_INITRAMFS_COMPRESSION_NONE=y
# CONFIG_INITRAMFS_COMPRESSION_GZIP is not set
# CONFIG_INITRAMFS_COMPRESSION_BZIP2 is not set
# CONFIG_INITRAMFS_COMPRESSION_LZMA is not set
# CONFIG_INITRAMFS_COMPRESSION_XZ is not set
# CONFIG_INITRAMFS_COMPRESSION_LZO is not set
# CONFIG_CC_OPTIMIZE_FOR_SIZE is not set
CONFIG_SYSCTL=y
CONFIG_ANON_INODES=y
CONFIG_HAVE_UID16=y
# CONFIG_EXPERT is not set
CONFIG_UID16=y
# CONFIG_SYSCTL_SYSCALL is not set
CONFIG_KALLSYMS=y
# CONFIG_KALLSYMS_ALL is not set
CONFIG_PRINTK=y
CONFIG_BUG=y
CONFIG_ELF_CORE=y
CONFIG_BASE_FULL=y
CONFIG_FUTEX=y
CONFIG_EPOLL=y
CONFIG_SIGNALFD=y
CONFIG_TIMERFD=y
CONFIG_EVENTFD=y
CONFIG_SHMEM=y
CONFIG_AIO=y
# CONFIG_EMBEDDED is not set
CONFIG_HAVE_PERF_EVENTS=y
CONFIG_PERF_USE_VMALLOC=y
#
# Kernel Performance Events And Counters
#
CONFIG_PERF_EVENTS=y
# CONFIG_DEBUG_PERF_USE_VMALLOC is not set
CONFIG_VM_EVENT_COUNTERS=y
CONFIG_COMPAT_BRK=y
CONFIG_SLAB=y
# CONFIG_SLUB is not set
# CONFIG_PROFILING is not set
CONFIG_HAVE_OPROFILE=y
# CONFIG_JUMP_LABEL is not set
# CONFIG_HAVE_64BIT_ALIGNED_ACCESS is not set
CONFIG_HAVE_KPROBES=y
CONFIG_HAVE_KRETPROBES=y
CONFIG_HAVE_ARCH_TRACEHOOK=y
CONFIG_HAVE_DMA_ATTRS=y
CONFIG_HAVE_DMA_CONTIGUOUS=y
CONFIG_GENERIC_SMP_IDLE_THREAD=y
CONFIG_GENERIC_IDLE_POLL_SETUP=y
CONFIG_HAVE_REGS_AND_STACK_ACCESS_API=y
CONFIG_HAVE_CLK=y
CONFIG_HAVE_DMA_API_DEBUG=y
CONFIG_HAVE_HW_BREAKPOINT=y
CONFIG_HAVE_ARCH_JUMP_LABEL=y
CONFIG_ARCH_WANT_IPC_PARSE_VERSION=y
CONFIG_HAVE_ARCH_SECCOMP_FILTER=y
CONFIG_HAVE_CONTEXT_TRACKING=y
CONFIG_HAVE_IRQ_TIME_ACCOUNTING=y
CONFIG_HAVE_MOD_ARCH_SPECIFIC=y
CONFIG_MODULES_USE_ELF_REL=y
CONFIG_CLONE_BACKWARDS=y
CONFIG_OLD_SIGSUSPEND3=y
CONFIG_OLD_SIGACTION=y
#
# GCOV-based kernel profiling
#
# CONFIG_GCOV_KERNEL is not set
CONFIG_HAVE_GENERIC_DMA_COHERENT=y
CONFIG_SLABINFO=y
CONFIG_RT_MUTEXES=y
CONFIG_BASE_SMALL=0
# CONFIG_MODULES is not set
CONFIG_BLOCK=y
CONFIG_LBDAF=y
# CONFIG_BLK_DEV_BSG is not set
# CONFIG_BLK_DEV_BSGLIB is not set
# CONFIG_BLK_DEV_INTEGRITY is not set
# CONFIG_BLK_CMDLINE_PARSER is not set
#
# Partition Types
#
CONFIG_PARTITION_ADVANCED=y
# CONFIG_ACORN_PARTITION is not set
# CONFIG_AIX_PARTITION is not set
# CONFIG_OSF_PARTITION is not set
# CONFIG_AMIGA_PARTITION is not set
# CONFIG_ATARI_PARTITION is not set
# CONFIG_MAC_PARTITION is not set
CONFIG_MSDOS_PARTITION=y
# CONFIG_BSD_DISKLABEL is not set
# CONFIG_MINIX_SUBPARTITION is not set
# CONFIG_SOLARIS_X86_PARTITION is not set
# CONFIG_UNIXWARE_DISKLABEL is not set
# CONFIG_LDM_PARTITION is not set
# CONFIG_SGI_PARTITION is not set
# CONFIG_ULTRIX_PARTITION is not set
# CONFIG_SUN_PARTITION is not set
# CONFIG_KARMA_PARTITION is not set
CONFIG_EFI_PARTITION=y
# CONFIG_SYSV68_PARTITION is not set
# CONFIG_CMDLINE_PARTITION is not set
#
# IO Schedulers
#
CONFIG_IOSCHED_NOOP=y
CONFIG_IOSCHED_DEADLINE=y
CONFIG_IOSCHED_CFQ=y
# CONFIG_DEFAULT_DEADLINE is not set
CONFIG_DEFAULT_CFQ=y
# CONFIG_DEFAULT_NOOP is not set
CONFIG_DEFAULT_IOSCHED="cfq"
CONFIG_ASN1=y
CONFIG_INLINE_SPIN_UNLOCK_IRQ=y
CONFIG_INLINE_READ_UNLOCK=y
CONFIG_INLINE_READ_UNLOCK_IRQ=y
CONFIG_INLINE_WRITE_UNLOCK=y
CONFIG_INLINE_WRITE_UNLOCK_IRQ=y
# CONFIG_FREEZER is not set
#
# System Type
#
CONFIG_MMU=y
# CONFIG_ARCH_MULTIPLATFORM is not set
# CONFIG_ARCH_INTEGRATOR is not set
# CONFIG_ARCH_REALVIEW is not set
# CONFIG_ARCH_VERSATILE is not set
# CONFIG_ARCH_AT91 is not set
# CONFIG_ARCH_CLPS711X is not set
# CONFIG_ARCH_GEMINI is not set
# CONFIG_ARCH_EBSA110 is not set
# CONFIG_ARCH_EP93XX is not set
# CONFIG_ARCH_FOOTBRIDGE is not set
# CONFIG_ARCH_NETX is not set
# CONFIG_ARCH_IOP13XX is not set
# CONFIG_ARCH_IOP32X is not set
# CONFIG_ARCH_IOP33X is not set
# CONFIG_ARCH_IXP4XX is not set
# CONFIG_ARCH_DOVE is not set
# CONFIG_ARCH_KIRKWOOD is not set
# CONFIG_ARCH_MV78XX0 is not set
# CONFIG_ARCH_ORION5X is not set
# CONFIG_ARCH_MMP is not set
# CONFIG_ARCH_KS8695 is not set
# CONFIG_ARCH_W90X900 is not set
# CONFIG_ARCH_LPC32XX is not set
# CONFIG_ARCH_PXA is not set
# CONFIG_ARCH_MSM is not set
# CONFIG_ARCH_SHMOBILE is not set
# CONFIG_ARCH_RPC is not set
# CONFIG_ARCH_SA1100 is not set
# CONFIG_ARCH_S3C24XX is not set
# CONFIG_ARCH_S3C64XX is not set
# CONFIG_ARCH_S5P64X0 is not set
# CONFIG_ARCH_S5PC100 is not set
# CONFIG_ARCH_S5PV210 is not set
# CONFIG_ARCH_EXYNOS is not set
# CONFIG_ARCH_SHARK is not set
# CONFIG_ARCH_DAVINCI is not set
# CONFIG_ARCH_OMAP1 is not set
CONFIG_ARCH_OMAP2PLUS=y
#
# Multiple platform selection
#
#
# CPU Core family selection
#
# CONFIG_ARCH_MULTI_V6 is not set
CONFIG_ARCH_MULTI_V7=y
CONFIG_ARCH_MULTI_V6_V7=y
# CONFIG_ARCH_MULTI_CPU_AUTO is not set
# CONFIG_ARCH_MVEBU is not set
# CONFIG_ARCH_BCM is not set
# CONFIG_GPIO_PCA953X is not set
# CONFIG_KEYBOARD_GPIO_POLLED is not set
# CONFIG_ARCH_HIGHBANK is not set
# CONFIG_ARCH_KEYSTONE is not set
# CONFIG_ARCH_MXC is not set
#
# System Type
#
CONFIG_MMU=y
# CONFIG_ARCH_MULTIPLATFORM is not set
# CONFIG_ARCH_INTEGRATOR is not set
# CONFIG_ARCH_REALVIEW is not set
# CONFIG_ARCH_VERSATILE is not set
# CONFIG_ARCH_AT91 is not set
# CONFIG_ARCH_CLPS711X is not set
# CONFIG_ARCH_GEMINI is not set
# CONFIG_ARCH_EBSA110 is not set
# CONFIG_ARCH_EP93XX is not set
# CONFIG_ARCH_FOOTBRIDGE is not set
# CONFIG_ARCH_NETX is not set
# CONFIG_ARCH_IOP13XX is not set
# CONFIG_ARCH_IOP32X is not set
# CONFIG_ARCH_IOP33X is not set
# CONFIG_ARCH_IXP4XX is not set
# CONFIG_ARCH_DOVE is not set
# CONFIG_ARCH_KIRKWOOD is not set
# CONFIG_ARCH_MV78XX0 is not set
# CONFIG_ARCH_ORION5X is not set
# CONFIG_ARCH_MMP is not set
# CONFIG_ARCH_KS8695 is not set
# CONFIG_ARCH_W90X900 is not set
# CONFIG_ARCH_LPC32XX is not set
# CONFIG_ARCH_PXA is not set
# CONFIG_ARCH_MSM is not set
# CONFIG_ARCH_SHMOBILE is not set
# CONFIG_ARCH_RPC is not set
# CONFIG_ARCH_SA1100 is not set
# CONFIG_ARCH_S3C24XX is not set
# CONFIG_ARCH_S3C64XX is not set
# CONFIG_ARCH_S5P64X0 is not set
# CONFIG_ARCH_S5PC100 is not set
# CONFIG_ARCH_S5PV210 is not set
# CONFIG_ARCH_EXYNOS is not set
# CONFIG_ARCH_SHARK is not set
# CONFIG_ARCH_DAVINCI is not set
# CONFIG_ARCH_OMAP1 is not set
CONFIG_ARCH_OMAP2PLUS=y
#
# Multiple platform selection
#
#
# CPU Core family selection
#
# CONFIG_ARCH_MULTI_V6 is not set
CONFIG_ARCH_MULTI_V7=y
CONFIG_ARCH_MULTI_V6_V7=y
# CONFIG_ARCH_MULTI_CPU_AUTO is not set
# CONFIG_ARCH_MVEBU is not set
# CONFIG_ARCH_BCM is not set
# CONFIG_GPIO_PCA953X is not set
# CONFIG_KEYBOARD_GPIO_POLLED is not set
# CONFIG_ARCH_HIGHBANK is not set
# CONFIG_ARCH_KEYSTONE is not set
# CONFIG_ARCH_MXC is not set
#
# TI OMAP Common Features
#
#
# OMAP Feature Selections
#
# CONFIG_POWER_AVS_OMAP is not set
CONFIG_OMAP_RESET_CLOCKS=y
CONFIG_OMAP_MUX=y
CONFIG_OMAP_MUX_DEBUG=y
CONFIG_OMAP_MUX_WARNINGS=y
CONFIG_OMAP_32K_TIMER=y
# CONFIG_OMAP3_L2_AUX_SECURE_SAVE_RESTORE is not set
CONFIG_OMAP_DM_TIMER=y
CONFIG_OMAP_PM_NOOP=y
CONFIG_MACH_OMAP_GENERIC=y
CONFIG_ARCH_OMAP=y
CONFIG_ARCH_OMAP3=y
CONFIG_ARCH_OMAP4=y
# CONFIG_SOC_OMAP5 is not set
CONFIG_SOC_AM33XX=y
# CONFIG_SOC_AM43XX is not set
#
# TI OMAP2/3/4 Specific Features
#
CONFIG_ARCH_OMAP2PLUS_TYPICAL=y
CONFIG_SOC_HAS_OMAP2_SDRC=y
# CONFIG_SOC_DRA7XX is not set
# CONFIG_SOC_OMAP3430 is not set
# CONFIG_SOC_TI81XX is not set
#
# OMAP Board Type
#
# CONFIG_MACH_OMAP3_BEAGLE is not set
# CONFIG_MACH_DEVKIT8000 is not set
# CONFIG_MACH_OMAP_LDP is not set
# CONFIG_MACH_OMAP3530_LV_SOM is not set
# CONFIG_MACH_OMAP3_TORPEDO is not set
# CONFIG_MACH_OVERO is not set
# CONFIG_MACH_OMAP3EVM is not set
# CONFIG_MACH_OMAP3517EVM is not set
# CONFIG_MACH_CRANEBOARD is not set
# CONFIG_MACH_OMAP3_PANDORA is not set
# CONFIG_MACH_TOUCHBOOK is not set
# CONFIG_MACH_OMAP_3430SDP is not set
# CONFIG_MACH_NOKIA_RM680 is not set
# CONFIG_MACH_NOKIA_RX51 is not set
# CONFIG_MACH_OMAP_ZOOM2 is not set
# CONFIG_MACH_OMAP_ZOOM3 is not set
# CONFIG_MACH_CM_T35 is not set
# CONFIG_MACH_CM_T3517 is not set
# CONFIG_MACH_IGEP0020 is not set
# CONFIG_MACH_IGEP0030 is not set
# CONFIG_MACH_SBC3530 is not set
# CONFIG_MACH_OMAP_3630SDP is not set
# CONFIG_OMAP3_EMU is not set
# CONFIG_OMAP3_SDRC_AC_TIMING is not set
# CONFIG_OMAP4_ERRATA_I688 is not set
# CONFIG_ARCH_ROCKCHIP is not set
# CONFIG_ARCH_SOCFPGA is not set
# CONFIG_PLAT_SPEAR is not set
# CONFIG_ARCH_STI is not set
# CONFIG_ARCH_SHMOBILE_MULTI is not set
# CONFIG_ARCH_SUNXI is not set
# CONFIG_ARCH_SIRF is not set
# CONFIG_ARCH_TEGRA is not set
# CONFIG_ARCH_U8500 is not set
# CONFIG_ARCH_VEXPRESS is not set
# CONFIG_ARCH_VIRT is not set
# CONFIG_ARCH_WM8850 is not set
# CONFIG_ARCH_ZYNQ is not set
#
# Processor Type
#
CONFIG_CPU_V7=y
CONFIG_CPU_32v6K=y
CONFIG_CPU_32v7=y
CONFIG_CPU_ABRT_EV7=y
CONFIG_CPU_PABRT_V7=y
CONFIG_CPU_CACHE_V7=y
CONFIG_CPU_CACHE_VIPT=y
CONFIG_CPU_COPY_V6=y
CONFIG_CPU_TLB_V7=y
CONFIG_CPU_HAS_ASID=y
CONFIG_CPU_CP15=y
CONFIG_CPU_CP15_MMU=y
#
# Processor Features
#
# CONFIG_ARM_LPAE is not set
# CONFIG_ARCH_PHYS_ADDR_T_64BIT is not set
CONFIG_ARM_THUMB=y
CONFIG_ARM_THUMBEE=y
CONFIG_ARM_VIRT_EXT=y
# CONFIG_SWP_EMULATE is not set
# CONFIG_CPU_ICACHE_DISABLE is not set
# CONFIG_CPU_DCACHE_DISABLE is not set
# CONFIG_CPU_BPREDICT_DISABLE is not set
CONFIG_KUSER_HELPERS=y
CONFIG_OUTER_CACHE=y
CONFIG_OUTER_CACHE_SYNC=y
CONFIG_CACHE_L2X0=y
CONFIG_CACHE_PL310=y
CONFIG_ARM_L1_CACHE_SHIFT_6=y
CONFIG_ARM_L1_CACHE_SHIFT=6
CONFIG_ARM_DMA_MEM_BUFFERABLE=y
CONFIG_ARM_NR_BANKS=8
CONFIG_MULTI_IRQ_HANDLER=y
# CONFIG_ARM_ERRATA_430973 is not set
# CONFIG_ARM_ERRATA_458693 is not set
# CONFIG_ARM_ERRATA_460075 is not set
CONFIG_PL310_ERRATA_588369=y
CONFIG_ARM_ERRATA_720789=y
CONFIG_PL310_ERRATA_727915=y
# CONFIG_ARM_ERRATA_743622 is not set
# CONFIG_ARM_ERRATA_751472 is not set
# CONFIG_PL310_ERRATA_753970 is not set
CONFIG_ARM_ERRATA_754322=y
# CONFIG_PL310_ERRATA_769419 is not set
CONFIG_ARM_ERRATA_775420=y
# CONFIG_ARM_ERRATA_773022 is not set
CONFIG_TI_PRIV_EDMA=y
#
# Bus support
#
# CONFIG_PCI_SYSCALL is not set
# CONFIG_PCCARD is not set
#
# Kernel Features
#
CONFIG_HAVE_SMP=y
# CONFIG_SMP is not set
CONFIG_HAVE_ARM_ARCH_TIMER=y
CONFIG_VMSPLIT_3G=y
# CONFIG_VMSPLIT_2G is not set
# CONFIG_VMSPLIT_1G is not set
CONFIG_PAGE_OFFSET=0xC0000000
# CONFIG_ARM_PSCI is not set
CONFIG_ARCH_NR_GPIO=0
CONFIG_PREEMPT_NONE=y
# CONFIG_PREEMPT_VOLUNTARY is not set
# CONFIG_PREEMPT is not set
CONFIG_HZ_FIXED=0
CONFIG_HZ_100=y
# CONFIG_HZ_200 is not set
# CONFIG_HZ_250 is not set
# CONFIG_HZ_300 is not set
# CONFIG_HZ_500 is not set
# CONFIG_HZ_1000 is not set
CONFIG_HZ=100
CONFIG_SCHED_HRTICK=y
# CONFIG_THUMB2_KERNEL is not set
CONFIG_AEABI=y
CONFIG_OABI_COMPAT=y
CONFIG_ARCH_HAS_HOLES_MEMORYMODEL=y
# CONFIG_ARCH_SPARSEMEM_DEFAULT is not set
# CONFIG_ARCH_SELECT_MEMORY_MODEL is not set
CONFIG_HAVE_ARCH_PFN_VALID=y
CONFIG_HIGHMEM=y
CONFIG_HIGHPTE=y
# CONFIG_HW_PERF_EVENTS is not set
CONFIG_ARCH_WANT_GENERAL_HUGETLB=y
CONFIG_FLATMEM=y
CONFIG_FLAT_NODE_MEM_MAP=y
CONFIG_HAVE_MEMBLOCK=y
# CONFIG_HAVE_BOOTMEM_INFO_NODE is not set
CONFIG_PAGEFLAGS_EXTENDED=y
CONFIG_SPLIT_PTLOCK_CPUS=4
# CONFIG_COMPACTION is not set
# CONFIG_PHYS_ADDR_T_64BIT is not set
CONFIG_ZONE_DMA_FLAG=0
CONFIG_BOUNCE=y
# CONFIG_KSM is not set
CONFIG_DEFAULT_MMAP_MIN_ADDR=4096
CONFIG_CROSS_MEMORY_ATTACH=y
CONFIG_NEED_PER_CPU_KM=y
CONFIG_CLEANCACHE=y
# CONFIG_CMA is not set
# CONFIG_ZBUD is not set
CONFIG_FORCE_MAX_ZONEORDER=12
CONFIG_ALIGNMENT_TRAP=y
# CONFIG_UACCESS_WITH_MEMCPY is not set
# CONFIG_SECCOMP is not set
# CONFIG_CC_STACKPROTECTOR is not set
# CONFIG_XEN is not set
#
# Boot options
#
CONFIG_USE_OF=y
CONFIG_ATAGS=y
# CONFIG_DEPRECATED_PARAM_STRUCT is not set
CONFIG_ZBOOT_ROM_TEXT=0x0
CONFIG_ZBOOT_ROM_BSS=0x0
# CONFIG_ARM_APPENDED_DTB is not set
CONFIG_CMDLINE="console=ttyO2,115200"
CONFIG_CMDLINE_FROM_BOOTLOADER=y
# CONFIG_CMDLINE_EXTEND is not set
# CONFIG_CMDLINE_FORCE is not set
# CONFIG_XIP_KERNEL is not set
# CONFIG_KEXEC is not set
# CONFIG_CRASH_DUMP is not set
CONFIG_AUTO_ZRELADDR=y
#
# CPU Power Management
#
#
# CPU Frequency scaling
#
CONFIG_CPU_FREQ=y
CONFIG_CPU_FREQ_TABLE=y
CONFIG_CPU_FREQ_GOV_COMMON=y
CONFIG_CPU_FREQ_STAT=y
CONFIG_CPU_FREQ_STAT_DETAILS=y
# CONFIG_CPU_FREQ_DEFAULT_GOV_PERFORMANCE is not set
CONFIG_CPU_FREQ_DEFAULT_GOV_USERSPACE=y
# CONFIG_CPU_FREQ_DEFAULT_GOV_ONDEMAND is not set
# CONFIG_CPU_FREQ_DEFAULT_GOV_CONSERVATIVE is not set
CONFIG_CPU_FREQ_GOV_PERFORMANCE=y
CONFIG_CPU_FREQ_GOV_POWERSAVE=y
CONFIG_CPU_FREQ_GOV_USERSPACE=y
CONFIG_CPU_FREQ_GOV_ONDEMAND=y
CONFIG_CPU_FREQ_GOV_CONSERVATIVE=y
CONFIG_GENERIC_CPUFREQ_CPU0=y
#
# ARM CPU frequency scaling drivers
#
# CONFIG_ARM_KIRKWOOD_CPUFREQ is not set
CONFIG_ARM_OMAP2PLUS_CPUFREQ=y
#
# CPU Idle
#
CONFIG_CPU_IDLE=y
# CONFIG_CPU_IDLE_MULTIPLE_DRIVERS is not set
CONFIG_CPU_IDLE_GOV_LADDER=y
CONFIG_CPU_IDLE_GOV_MENU=y
#
# ARM CPU Idle Drivers
#
# CONFIG_ARCH_NEEDS_CPU_IDLE_COUPLED is not set
#
# Floating point emulation
#
#
# At least one emulation must be selected
#
# CONFIG_FPE_NWFPE is not set
# CONFIG_FPE_FASTFPE is not set
CONFIG_VFP=y
CONFIG_VFPv3=y
CONFIG_NEON=y
# CONFIG_KERNEL_MODE_NEON is not set
#
# Userspace binary formats
#
CONFIG_BINFMT_ELF=y
CONFIG_ARCH_BINFMT_ELF_RANDOMIZE_PIE=y
CONFIG_CORE_DUMP_DEFAULT_ELF_HEADERS=y
CONFIG_BINFMT_SCRIPT=y
# CONFIG_HAVE_AOUT is not set
CONFIG_BINFMT_MISC=y
CONFIG_COREDUMP=y
#
# Power management options
#
# CONFIG_SUSPEND is not set
CONFIG_PM_RUNTIME=y
CONFIG_PM=y
CONFIG_PM_DEBUG=y
CONFIG_PM_ADVANCED_DEBUG=y
# CONFIG_APM_EMULATION is not set
CONFIG_ARCH_HAS_OPP=y
CONFIG_PM_OPP=y
CONFIG_PM_CLK=y
# CONFIG_WQ_POWER_EFFICIENT_DEFAULT is not set
CONFIG_CPU_PM=y
CONFIG_ARCH_SUSPEND_POSSIBLE=y
CONFIG_ARM_CPU_SUSPEND=y
CONFIG_NET=y
#
# Networking options
#
CONFIG_PACKET=y
# CONFIG_PACKET_DIAG is not set
CONFIG_UNIX=y
# CONFIG_UNIX_DIAG is not set
CONFIG_XFRM=y
CONFIG_XFRM_ALGO=y
# CONFIG_XFRM_USER is not set
# CONFIG_XFRM_SUB_POLICY is not set
# CONFIG_XFRM_MIGRATE is not set
# CONFIG_XFRM_STATISTICS is not set
CONFIG_XFRM_IPCOMP=y
# CONFIG_NET_KEY is not set
CONFIG_INET=y
# CONFIG_IP_MULTICAST is not set
# CONFIG_IP_ADVANCED_ROUTER is not set
CONFIG_IP_PNP=y
CONFIG_IP_PNP_DHCP=y
CONFIG_IP_PNP_BOOTP=y
# CONFIG_IP_PNP_RARP is not set
CONFIG_NET_IPIP=y
# CONFIG_NET_IPGRE_DEMUX is not set
CONFIG_NET_IP_TUNNEL=y
# CONFIG_SYN_COOKIES is not set
# CONFIG_NET_IPVTI is not set
CONFIG_INET_AH=y
CONFIG_INET_ESP=y
CONFIG_INET_IPCOMP=y
CONFIG_INET_XFRM_TUNNEL=y
CONFIG_INET_TUNNEL=y
CONFIG_INET_XFRM_MODE_TRANSPORT=y
CONFIG_INET_XFRM_MODE_TUNNEL=y
CONFIG_INET_XFRM_MODE_BEET=y
CONFIG_INET_LRO=y
# CONFIG_INET_DIAG is not set
# CONFIG_TCP_CONG_ADVANCED is not set
CONFIG_TCP_CONG_CUBIC=y
CONFIG_DEFAULT_TCP_CONG="cubic"
# CONFIG_TCP_MD5SIG is not set
# CONFIG_IPV6 is not set
# CONFIG_NETLABEL is not set
# CONFIG_NETWORK_SECMARK is not set
# CONFIG_NETWORK_PHY_TIMESTAMPING is not set
# CONFIG_NETFILTER is not set
# CONFIG_IP_DCCP is not set
# CONFIG_IP_SCTP is not set
# CONFIG_RDS is not set
# CONFIG_TIPC is not set
# CONFIG_ATM is not set
CONFIG_L2TP=y
# CONFIG_L2TP_DEBUGFS is not set
# CONFIG_L2TP_V3 is not set
# CONFIG_BRIDGE is not set
CONFIG_HAVE_NET_DSA=y
# CONFIG_VLAN_8021Q is not set
# CONFIG_DECNET is not set
# CONFIG_LLC2 is not set
# CONFIG_IPX is not set
# CONFIG_ATALK is not set
# CONFIG_X25 is not set
# CONFIG_LAPB is not set
# CONFIG_PHONET is not set
# CONFIG_IEEE802154 is not set
# CONFIG_NET_SCHED is not set
# CONFIG_DCB is not set
CONFIG_DNS_RESOLVER=y
# CONFIG_BATMAN_ADV is not set
# CONFIG_OPENVSWITCH is not set
# CONFIG_VSOCKETS is not set
# CONFIG_NETLINK_MMAP is not set
# CONFIG_NETLINK_DIAG is not set
# CONFIG_NET_MPLS_GSO is not set
CONFIG_NET_RX_BUSY_POLL=y
CONFIG_BQL=y
#
# Network testing
#
# CONFIG_NET_PKTGEN is not set
# CONFIG_HAMRADIO is not set
# CONFIG_CAN is not set
# CONFIG_IRDA is not set
# CONFIG_BT is not set
# CONFIG_AF_RXRPC is not set
CONFIG_WIRELESS=y
# CONFIG_CFG80211 is not set
# CONFIG_LIB80211 is not set
#
# CFG80211 needs to be enabled for MAC80211
#
# CONFIG_WIMAX is not set
# CONFIG_RFKILL is not set
# CONFIG_RFKILL_REGULATOR is not set
# CONFIG_NET_9P is not set
# CONFIG_CAIF is not set
# CONFIG_CEPH_LIB is not set
# CONFIG_NFC is not set
CONFIG_HAVE_BPF_JIT=y
#
# Device Drivers
#
#
# Generic Driver Options
#
CONFIG_UEVENT_HELPER_PATH="/sbin/hotplug"
CONFIG_DEVTMPFS=y
CONFIG_DEVTMPFS_MOUNT=y
CONFIG_STANDALONE=y
CONFIG_PREVENT_FIRMWARE_BUILD=y
CONFIG_FW_LOADER=y
CONFIG_FIRMWARE_IN_KERNEL=y
CONFIG_EXTRA_FIRMWARE="am335x-pm-firmware.bin"
CONFIG_EXTRA_FIRMWARE_DIR="../"
# CONFIG_FW_LOADER_USER_HELPER is not set
# CONFIG_DEBUG_DRIVER is not set
# CONFIG_DEBUG_DEVRES is not set
# CONFIG_SYS_HYPERVISOR is not set
# CONFIG_GENERIC_CPU_DEVICES is not set
CONFIG_SOC_BUS=y
CONFIG_REGMAP=y
CONFIG_REGMAP_I2C=y
CONFIG_REGMAP_IRQ=y
# CONFIG_DMA_SHARED_BUFFER is not set
#
# Bus devices
#
# CONFIG_OMAP_OCP2SCP is not set
CONFIG_OMAP_INTERCONNECT=y
CONFIG_ARM_CCI=y
# CONFIG_CONNECTOR is not set
CONFIG_MTD=y
# CONFIG_MTD_REDBOOT_PARTS is not set
CONFIG_MTD_CMDLINE_PARTS=y
# CONFIG_MTD_AFS_PARTS is not set
CONFIG_MTD_OF_PARTS=y
# CONFIG_MTD_AR7_PARTS is not set
#
# User Modules And Translation Layers
#
CONFIG_MTD_BLKDEVS=y
CONFIG_MTD_BLOCK=y
# CONFIG_FTL is not set
# CONFIG_NFTL is not set
# CONFIG_INFTL is not set
# CONFIG_RFD_FTL is not set
# CONFIG_SSFDC is not set
# CONFIG_SM_FTL is not set
# CONFIG_MTD_OOPS is not set
#
# RAM/ROM/Flash chip drivers
#
# CONFIG_MTD_CFI is not set
# CONFIG_MTD_JEDECPROBE is not set
CONFIG_MTD_MAP_BANK_WIDTH_1=y
CONFIG_MTD_MAP_BANK_WIDTH_2=y
CONFIG_MTD_MAP_BANK_WIDTH_4=y
# CONFIG_MTD_MAP_BANK_WIDTH_8 is not set
# CONFIG_MTD_MAP_BANK_WIDTH_16 is not set
# CONFIG_MTD_MAP_BANK_WIDTH_32 is not set
CONFIG_MTD_CFI_I1=y
CONFIG_MTD_CFI_I2=y
# CONFIG_MTD_CFI_I4 is not set
# CONFIG_MTD_CFI_I8 is not set
# CONFIG_MTD_RAM is not set
# CONFIG_MTD_ROM is not set
# CONFIG_MTD_ABSENT is not set
#
# Mapping drivers for chip access
#
# CONFIG_MTD_COMPLEX_MAPPINGS is not set
# CONFIG_MTD_PLATRAM is not set
#
# Self-contained MTD device drivers
#
# CONFIG_MTD_DATAFLASH is not set
# CONFIG_MTD_M25P80 is not set
# CONFIG_MTD_SST25L is not set
# CONFIG_MTD_SLRAM is not set
# CONFIG_MTD_PHRAM is not set
# CONFIG_MTD_MTDRAM is not set
# CONFIG_MTD_BLOCK2MTD is not set
#
# Disk-On-Chip Device Drivers
#
# CONFIG_MTD_DOCG3 is not set
CONFIG_BCH_CONST_M=13
CONFIG_MTD_NAND_ECC=y
# CONFIG_MTD_NAND_ECC_SMC is not set
CONFIG_MTD_NAND=y
CONFIG_MTD_NAND_BCH=y
CONFIG_MTD_NAND_ECC_BCH=y
# CONFIG_MTD_SM_COMMON is not set
# CONFIG_MTD_NAND_DENALI is not set
# CONFIG_MTD_NAND_GPIO is not set
CONFIG_MTD_NAND_OMAP2=y
CONFIG_MTD_NAND_OMAP_BCH=y
CONFIG_MTD_NAND_IDS=y
# CONFIG_MTD_NAND_DISKONCHIP is not set
# CONFIG_MTD_NAND_DOCG4 is not set
# CONFIG_MTD_NAND_NANDSIM is not set
# CONFIG_MTD_NAND_PLATFORM is not set
# CONFIG_MTD_ONENAND is not set
#
# LPDDR flash memory drivers
#
# CONFIG_MTD_LPDDR is not set
CONFIG_MTD_UBI=y
CONFIG_MTD_UBI_WL_THRESHOLD=4096
CONFIG_MTD_UBI_BEB_LIMIT=20
# CONFIG_MTD_UBI_FASTMAP is not set
# CONFIG_MTD_UBI_GLUEBI is not set
CONFIG_DTC=y
CONFIG_OF=y
#
# Device Tree and Open Firmware support
#
CONFIG_PROC_DEVICETREE=y
# CONFIG_OF_SELFTEST is not set
CONFIG_OF_FLATTREE=y
CONFIG_OF_EARLY_FLATTREE=y
CONFIG_OF_ADDRESS=y
CONFIG_OF_IRQ=y
CONFIG_OF_NET=y
CONFIG_OF_MDIO=y
CONFIG_OF_MTD=y
# CONFIG_PARPORT is not set
CONFIG_BLK_DEV=y
# CONFIG_BLK_DEV_COW_COMMON is not set
CONFIG_BLK_DEV_LOOP=y
CONFIG_BLK_DEV_LOOP_MIN_COUNT=4
# CONFIG_BLK_DEV_CRYPTOLOOP is not set
# CONFIG_BLK_DEV_DRBD is not set
# CONFIG_BLK_DEV_NBD is not set
CONFIG_BLK_DEV_RAM=y
CONFIG_BLK_DEV_RAM_COUNT=4
CONFIG_BLK_DEV_RAM_SIZE=16384
# CONFIG_BLK_DEV_XIP is not set
# CONFIG_CDROM_PKTCDVD is not set
# CONFIG_ATA_OVER_ETH is not set
# CONFIG_MG_DISK is not set
# CONFIG_BLK_DEV_RBD is not set
#
# Misc devices
#
# CONFIG_SENSORS_LIS3LV02D is not set
# CONFIG_AD525X_DPOT is not set
# CONFIG_ATMEL_PWM is not set
# CONFIG_DUMMY_IRQ is not set
# CONFIG_ICS932S401 is not set
# CONFIG_ATMEL_SSC is not set
# CONFIG_ENCLOSURE_SERVICES is not set
# CONFIG_APDS9802ALS is not set
# CONFIG_ISL29003 is not set
# CONFIG_ISL29020 is not set
# CONFIG_SENSORS_TSL2550 is not set
# CONFIG_SENSORS_BH1780 is not set
# CONFIG_SENSORS_BH1770 is not set
# CONFIG_SENSORS_APDS990X is not set
# CONFIG_HMC6352 is not set
# CONFIG_DS1682 is not set
# CONFIG_TI_DAC7512 is not set
# CONFIG_BMP085_I2C is not set
# CONFIG_BMP085_SPI is not set
# CONFIG_USB_SWITCH_FSA9480 is not set
# CONFIG_LATTICE_ECP3_CONFIG is not set
# CONFIG_SRAM is not set
# CONFIG_CROSSBAR is not set
CONFIG_PWM_BUZZER=y
# CONFIG_C2PORT is not set
#
# EEPROM support
#
# CONFIG_EEPROM_AT24 is not set
# CONFIG_EEPROM_AT25 is not set
# CONFIG_EEPROM_LEGACY is not set
# CONFIG_EEPROM_MAX6875 is not set
CONFIG_EEPROM_93CX6=y
# CONFIG_EEPROM_93XX46 is not set
#
# Texas Instruments shared transport line discipline
#
CONFIG_TI_ST=y
# CONFIG_SENSORS_LIS3_SPI is not set
# CONFIG_SENSORS_LIS3_I2C is not set
#
# Altera FPGA firmware download module
#
# CONFIG_ALTERA_STAPL is not set
#
# SCSI device support
#
CONFIG_SCSI_MOD=y
# CONFIG_RAID_ATTRS is not set
CONFIG_SCSI=y
CONFIG_SCSI_DMA=y
# CONFIG_SCSI_TGT is not set
# CONFIG_SCSI_NETLINK is not set
CONFIG_SCSI_PROC_FS=y
#
# SCSI support type (disk, tape, CD-ROM)
#
CONFIG_BLK_DEV_SD=y
# CONFIG_CHR_DEV_ST is not set
# CONFIG_CHR_DEV_OSST is not set
# CONFIG_BLK_DEV_SR is not set
# CONFIG_CHR_DEV_SG is not set
# CONFIG_CHR_DEV_SCH is not set
# CONFIG_SCSI_MULTI_LUN is not set
# CONFIG_SCSI_CONSTANTS is not set
# CONFIG_SCSI_LOGGING is not set
# CONFIG_SCSI_SCAN_ASYNC is not set
#
# SCSI Transports
#
# CONFIG_SCSI_SPI_ATTRS is not set
# CONFIG_SCSI_FC_ATTRS is not set
# CONFIG_SCSI_ISCSI_ATTRS is not set
# CONFIG_SCSI_SAS_ATTRS is not set
# CONFIG_SCSI_SAS_LIBSAS is not set
# CONFIG_SCSI_SRP_ATTRS is not set
CONFIG_SCSI_LOWLEVEL=y
# CONFIG_ISCSI_TCP is not set
# CONFIG_ISCSI_BOOT_SYSFS is not set
# CONFIG_SCSI_UFSHCD is not set
# CONFIG_LIBFC is not set
# CONFIG_LIBFCOE is not set
# CONFIG_SCSI_DEBUG is not set
# CONFIG_SCSI_DH is not set
# CONFIG_SCSI_OSD_INITIATOR is not set
# CONFIG_ATA is not set
# CONFIG_MD is not set
# CONFIG_TARGET_CORE is not set
CONFIG_NETDEVICES=y
CONFIG_MII=y
CONFIG_NET_CORE=y
# CONFIG_BONDING is not set
# CONFIG_DUMMY is not set
# CONFIG_EQUALIZER is not set
# CONFIG_NET_TEAM is not set
# CONFIG_MACVLAN is not set
# CONFIG_VXLAN is not set
# CONFIG_NETCONSOLE is not set
# CONFIG_NETPOLL is not set
# CONFIG_NET_POLL_CONTROLLER is not set
CONFIG_TUN=y
# CONFIG_VETH is not set
# CONFIG_NLMON is not set
#
# CAIF transport drivers
#
#
# Distributed Switch Architecture drivers
#
# CONFIG_NET_DSA_MV88E6XXX is not set
# CONFIG_NET_DSA_MV88E6060 is not set
# CONFIG_NET_DSA_MV88E6XXX_NEED_PPU is not set
# CONFIG_NET_DSA_MV88E6131 is not set
# CONFIG_NET_DSA_MV88E6123_61_65 is not set
CONFIG_ETHERNET=y
# CONFIG_NET_VENDOR_ARC is not set
# CONFIG_NET_CADENCE is not set
# CONFIG_NET_VENDOR_BROADCOM is not set
# CONFIG_NET_CALXEDA_XGMAC is not set
# CONFIG_NET_VENDOR_CIRRUS is not set
# CONFIG_DM9000 is not set
# CONFIG_DNET is not set
# CONFIG_NET_VENDOR_FARADAY is not set
# CONFIG_NET_VENDOR_INTEL is not set
# CONFIG_NET_VENDOR_MARVELL is not set
# CONFIG_NET_VENDOR_MICREL is not set
# CONFIG_NET_VENDOR_MICROCHIP is not set
# CONFIG_NET_VENDOR_NATSEMI is not set
# CONFIG_ETHOC is not set
# CONFIG_SH_ETH is not set
# CONFIG_NET_VENDOR_SEEQ is not set
# CONFIG_NET_VENDOR_SMSC is not set
# CONFIG_NET_VENDOR_STMICRO is not set
CONFIG_NET_VENDOR_TI=y
CONFIG_TI_DAVINCI_EMAC=y
CONFIG_TI_DAVINCI_MDIO=y
CONFIG_TI_DAVINCI_CPDMA=y
CONFIG_TI_CPSW_PHY_SEL=y
CONFIG_TI_CPSW=y
CONFIG_TI_CPTS=y
# CONFIG_NET_VENDOR_VIA is not set
# CONFIG_NET_VENDOR_WIZNET is not set
CONFIG_PHYLIB=y
#
# MII PHY device drivers
#
# CONFIG_AT803X_PHY is not set
# CONFIG_AMD_PHY is not set
# CONFIG_MARVELL_PHY is not set
# CONFIG_DAVICOM_PHY is not set
# CONFIG_QSEMI_PHY is not set
# CONFIG_LXT_PHY is not set
# CONFIG_CICADA_PHY is not set
# CONFIG_VITESSE_PHY is not set
# CONFIG_SMSC_PHY is not set
CONFIG_DP83848_PHY=y
# CONFIG_BROADCOM_PHY is not set
# CONFIG_BCM87XX_PHY is not set
# CONFIG_ICPLUS_PHY is not set
# CONFIG_REALTEK_PHY is not set
# CONFIG_NATIONAL_PHY is not set
# CONFIG_STE10XP is not set
# CONFIG_LSI_ET1011C_PHY is not set
# CONFIG_MICREL_PHY is not set
# CONFIG_FIXED_PHY is not set
# CONFIG_MDIO_BITBANG is not set
# CONFIG_MDIO_BUS_MUX_GPIO is not set
# CONFIG_MDIO_BUS_MUX_MMIOREG is not set
# CONFIG_MICREL_KS8995MA is not set
# CONFIG_PPP is not set
# CONFIG_SLIP is not set
#
# USB Network Adapters
#
# CONFIG_USB_CATC is not set
# CONFIG_USB_KAWETH is not set
# CONFIG_USB_PEGASUS is not set
# CONFIG_USB_RTL8150 is not set
# CONFIG_USB_RTL8152 is not set
CONFIG_USB_USBNET=y
# CONFIG_USB_NET_AX8817X is not set
# CONFIG_USB_NET_AX88179_178A is not set
CONFIG_USB_NET_CDCETHER=y
CONFIG_USB_NET_CDC_EEM=y
CONFIG_USB_NET_CDC_NCM=y
CONFIG_USB_NET_CDC_MBIM=y
CONFIG_USB_NET_DM9601=y
CONFIG_USB_NET_SR9700=y
CONFIG_USB_NET_SMSC75XX=y
CONFIG_USB_NET_SMSC95XX=y
CONFIG_USB_NET_GL620A=y
CONFIG_USB_NET_NET1080=y
CONFIG_USB_NET_PLUSB=y
CONFIG_USB_NET_MCS7830=y
CONFIG_USB_NET_RNDIS_HOST=y
CONFIG_USB_NET_CDC_SUBSET=y
CONFIG_USB_ALI_M5632=y
CONFIG_USB_AN2720=y
CONFIG_USB_BELKIN=y
CONFIG_USB_ARMLINUX=y
CONFIG_USB_EPSON2888=y
CONFIG_USB_KC2190=y
CONFIG_USB_NET_ZAURUS=y
CONFIG_USB_NET_CX82310_ETH=y
CONFIG_USB_NET_KALMIA=y
CONFIG_USB_NET_QMI_WWAN=y
# CONFIG_USB_NET_INT51X1 is not set
# CONFIG_USB_IPHETH is not set
# CONFIG_USB_SIERRA_NET is not set
# CONFIG_USB_VL600 is not set
CONFIG_WLAN=y
# CONFIG_USB_ZD1201 is not set
# CONFIG_HOSTAP is not set
CONFIG_WL_TI=y
#
# Enable WiMAX (Networking options) to see the WiMAX drivers
#
# CONFIG_WAN is not set
# CONFIG_ISDN is not set
#
# Input device support
#
CONFIG_INPUT=y
# CONFIG_INPUT_FF_MEMLESS is not set
# CONFIG_INPUT_POLLDEV is not set
# CONFIG_INPUT_SPARSEKMAP is not set
# CONFIG_INPUT_MATRIXKMAP is not set
#
# Userland interfaces
#
# CONFIG_INPUT_MOUSEDEV is not set
# CONFIG_INPUT_JOYDEV is not set
CONFIG_INPUT_EVDEV=y
# CONFIG_INPUT_EVBUG is not set
#
# Input Device Drivers
#
CONFIG_INPUT_KEYBOARD=y
# CONFIG_KEYBOARD_ADP5588 is not set
# CONFIG_KEYBOARD_ADP5589 is not set
# CONFIG_KEYBOARD_ATKBD is not set
# CONFIG_KEYBOARD_QT1070 is not set
# CONFIG_KEYBOARD_QT2160 is not set
# CONFIG_KEYBOARD_LKKBD is not set
CONFIG_KEYBOARD_GPIO=y
# CONFIG_KEYBOARD_TCA6416 is not set
# CONFIG_KEYBOARD_TCA8418 is not set
# CONFIG_KEYBOARD_MATRIX is not set
# CONFIG_KEYBOARD_LM8323 is not set
# CONFIG_KEYBOARD_LM8333 is not set
# CONFIG_KEYBOARD_MAX7359 is not set
# CONFIG_KEYBOARD_MCS is not set
# CONFIG_KEYBOARD_MPR121 is not set
# CONFIG_KEYBOARD_NEWTON is not set
# CONFIG_KEYBOARD_OPENCORES is not set
# CONFIG_KEYBOARD_SAMSUNG is not set
# CONFIG_KEYBOARD_STOWAWAY is not set
# CONFIG_KEYBOARD_SUNKBD is not set
# CONFIG_KEYBOARD_OMAP4 is not set
# CONFIG_KEYBOARD_TWL4030 is not set
# CONFIG_KEYBOARD_XTKBD is not set
# CONFIG_INPUT_MOUSE is not set
# CONFIG_INPUT_JOYSTICK is not set
# CONFIG_INPUT_TABLET is not set
# CONFIG_INPUT_TOUCHSCREEN is not set
# CONFIG_INPUT_MISC is not set
#
# Hardware I/O ports
#
CONFIG_SERIO=y
# CONFIG_SERIO_SERPORT is not set
# CONFIG_SERIO_LIBPS2 is not set
# CONFIG_SERIO_RAW is not set
# CONFIG_SERIO_ALTERA_PS2 is not set
# CONFIG_SERIO_PS2MULT is not set
# CONFIG_SERIO_ARC_PS2 is not set
# CONFIG_SERIO_APBPS2 is not set
# CONFIG_SERIO_OLPC_APSP is not set
# CONFIG_GAMEPORT is not set
#
# Character devices
#
CONFIG_TTY=y
CONFIG_VT=y
CONFIG_CONSOLE_TRANSLATIONS=y
CONFIG_VT_CONSOLE=y
CONFIG_HW_CONSOLE=y
CONFIG_VT_HW_CONSOLE_BINDING=y
CONFIG_UNIX98_PTYS=y
# CONFIG_DEVPTS_MULTIPLE_INSTANCES is not set
# CONFIG_LEGACY_PTYS is not set
# CONFIG_SERIAL_NONSTANDARD is not set
# CONFIG_N_GSM is not set
# CONFIG_TRACE_SINK is not set
CONFIG_DEVKMEM=y
#
# Serial drivers
#
CONFIG_SERIAL_8250=y
CONFIG_SERIAL_8250_DEPRECATED_OPTIONS=y
CONFIG_SERIAL_8250_CONSOLE=y
CONFIG_SERIAL_8250_DMA=y
CONFIG_SERIAL_8250_NR_UARTS=4
CONFIG_SERIAL_8250_RUNTIME_UARTS=4
CONFIG_SERIAL_8250_EXTENDED=y
CONFIG_SERIAL_8250_MANY_PORTS=y
CONFIG_SERIAL_8250_SHARE_IRQ=y
CONFIG_SERIAL_8250_DETECT_IRQ=y
CONFIG_SERIAL_8250_RSA=y
# CONFIG_SERIAL_8250_DW is not set
# CONFIG_SERIAL_8250_EM is not set
#
# Non-8250 serial port support
#
# CONFIG_SERIAL_MAX3100 is not set
# CONFIG_SERIAL_MAX310X is not set
CONFIG_SERIAL_CORE=y
CONFIG_SERIAL_CORE_CONSOLE=y
# CONFIG_SERIAL_OF_PLATFORM is not set
CONFIG_SERIAL_OMAP=y
CONFIG_SERIAL_OMAP_CONSOLE=y
# CONFIG_SERIAL_SCCNXP is not set
# CONFIG_SERIAL_TIMBERDALE is not set
# CONFIG_SERIAL_ALTERA_JTAGUART is not set
# CONFIG_SERIAL_ALTERA_UART is not set
# CONFIG_SERIAL_IFX6X60 is not set
# CONFIG_SERIAL_XILINX_PS_UART is not set
# CONFIG_SERIAL_ARC is not set
# CONFIG_SERIAL_FSL_LPUART is not set
# CONFIG_SERIAL_ST_ASC is not set
# CONFIG_HVC_DCC is not set
# CONFIG_IPMI_HANDLER is not set
CONFIG_HW_RANDOM=y
# CONFIG_HW_RANDOM_TIMERIOMEM is not set
# CONFIG_HW_RANDOM_ATMEL is not set
CONFIG_HW_RANDOM_OMAP=y
# CONFIG_HW_RANDOM_EXYNOS is not set
# CONFIG_R3964 is not set
# CONFIG_RAW_DRIVER is not set
# CONFIG_TCG_TPM is not set
CONFIG_I2C=y
CONFIG_I2C_BOARDINFO=y
CONFIG_I2C_COMPAT=y
CONFIG_I2C_CHARDEV=y
# CONFIG_I2C_MUX is not set
CONFIG_I2C_HELPER_AUTO=y
#
# I2C Hardware Bus support
#
#
# I2C system bus drivers (mostly embedded / system-on-chip)
#
# CONFIG_I2C_CBUS_GPIO is not set
# CONFIG_I2C_DESIGNWARE_PLATFORM is not set
# CONFIG_I2C_GPIO is not set
# CONFIG_I2C_OCORES is not set
CONFIG_I2C_OMAP=y
# CONFIG_I2C_PCA_PLATFORM is not set
# CONFIG_I2C_PXA_PCI is not set
# CONFIG_I2C_SIMTEC is not set
# CONFIG_I2C_XILINX is not set
#
# External I2C/SMBus adapter drivers
#
# CONFIG_I2C_DIOLAN_U2C is not set
# CONFIG_I2C_PARPORT_LIGHT is not set
# CONFIG_I2C_TAOS_EVM is not set
# CONFIG_I2C_TINY_USB is not set
#
# Other I2C/SMBus bus drivers
#
# CONFIG_I2C_DEBUG_CORE is not set
# CONFIG_I2C_DEBUG_ALGO is not set
# CONFIG_I2C_DEBUG_BUS is not set
CONFIG_SPI=y
# CONFIG_SPI_DEBUG is not set
CONFIG_SPI_MASTER=y
#
# SPI Master Controller Drivers
#
# CONFIG_SPI_ALTERA is not set
# CONFIG_SPI_BITBANG is not set
# CONFIG_SPI_GPIO is not set
# CONFIG_SPI_FSL_SPI is not set
# CONFIG_SPI_FSL_DSPI is not set
# CONFIG_SPI_OC_TINY is not set
CONFIG_SPI_OMAP24XX=y
# CONFIG_SPI_TI_QSPI is not set
# CONFIG_SPI_PXA2XX_PCI is not set
# CONFIG_SPI_SC18IS602 is not set
# CONFIG_SPI_XCOMM is not set
# CONFIG_SPI_XILINX is not set
# CONFIG_SPI_DESIGNWARE is not set
#
# SPI Protocol Masters
#
# CONFIG_SPI_SPIDEV is not set
# CONFIG_SPI_TLE62X0 is not set
# CONFIG_HSI is not set
#
# PPS support
#
CONFIG_PPS=y
# CONFIG_PPS_DEBUG is not set
#
# PPS clients support
#
# CONFIG_PPS_CLIENT_KTIMER is not set
# CONFIG_PPS_CLIENT_LDISC is not set
# CONFIG_PPS_CLIENT_GPIO is not set
#
# PPS generators support
#
#
# PTP clock support
#
CONFIG_PTP_1588_CLOCK=y
#
# Enable PHYLIB and NETWORK_PHY_TIMESTAMPING to see the additional clocks.
#
CONFIG_PINCTRL=y
#
# Pin controllers
#
CONFIG_PINMUX=y
CONFIG_PINCONF=y
CONFIG_GENERIC_PINCONF=y
# CONFIG_DEBUG_PINCTRL is not set
CONFIG_PINCTRL_SINGLE=y
CONFIG_ARCH_HAVE_CUSTOM_GPIO_H=y
CONFIG_ARCH_REQUIRE_GPIOLIB=y
CONFIG_GPIO_DEVRES=y
CONFIG_GPIOLIB=y
CONFIG_OF_GPIO=y
# CONFIG_DEBUG_GPIO is not set
CONFIG_GPIO_SYSFS=y
#
# Memory mapped GPIO drivers:
#
# CONFIG_GPIO_GENERIC_PLATFORM is not set
# CONFIG_GPIO_EM is not set
# CONFIG_GPIO_RCAR is not set
# CONFIG_GPIO_TS5500 is not set
# CONFIG_GPIO_GRGPIO is not set
#
# I2C GPIO expanders:
#
# CONFIG_GPIO_MAX7300 is not set
# CONFIG_GPIO_MAX732X is not set
# CONFIG_GPIO_PCF857X is not set
# CONFIG_GPIO_SX150X is not set
# CONFIG_GPIO_TWL4030 is not set
# CONFIG_GPIO_ADP5588 is not set
# CONFIG_GPIO_ADNP is not set
#
# PCI GPIO expanders:
#
#
# SPI GPIO expanders:
#
# CONFIG_GPIO_MAX7301 is not set
# CONFIG_GPIO_MCP23S08 is not set
# CONFIG_GPIO_MC33880 is not set
# CONFIG_GPIO_74X164 is not set
#
# AC97 GPIO expanders:
#
#
# LPC GPIO expanders:
#
#
# MODULbus GPIO expanders:
#
# CONFIG_GPIO_TPS65910 is not set
#
# USB GPIO expanders:
#
# CONFIG_W1 is not set
CONFIG_POWER_SUPPLY=y
# CONFIG_POWER_SUPPLY_DEBUG is not set
# CONFIG_PDA_POWER is not set
# CONFIG_TEST_POWER is not set
# CONFIG_BATTERY_DS2780 is not set
# CONFIG_BATTERY_DS2781 is not set
# CONFIG_BATTERY_DS2782 is not set
# CONFIG_BATTERY_SBS is not set
# CONFIG_BATTERY_BQ27x00 is not set
# CONFIG_BATTERY_MAX17040 is not set
# CONFIG_BATTERY_MAX17042 is not set
# CONFIG_CHARGER_ISP1704 is not set
# CONFIG_CHARGER_MAX8903 is not set
# CONFIG_CHARGER_TWL4030 is not set
# CONFIG_CHARGER_LP8727 is not set
# CONFIG_CHARGER_GPIO is not set
# CONFIG_CHARGER_MANAGER is not set
# CONFIG_CHARGER_BQ2415X is not set
# CONFIG_CHARGER_BQ24190 is not set
# CONFIG_CHARGER_SMB347 is not set
# CONFIG_POWER_RESET is not set
# CONFIG_POWER_RESET_RESTART is not set
CONFIG_POWER_AVS=y
# CONFIG_HWMON is not set
# CONFIG_THERMAL is not set
CONFIG_WATCHDOG=y
CONFIG_WATCHDOG_CORE=y
# CONFIG_WATCHDOG_NOWAYOUT is not set
#
# Watchdog Device Drivers
#
# CONFIG_SOFT_WATCHDOG is not set
# CONFIG_DW_WATCHDOG is not set
CONFIG_OMAP_WATCHDOG=y
# CONFIG_TWL4030_WATCHDOG is not set
# CONFIG_MAX63XX_WATCHDOG is not set
# CONFIG_MEN_A21_WDT is not set
#
# USB-based Watchdog Cards
#
# CONFIG_USBPCWATCHDOG is not set
CONFIG_SSB_POSSIBLE=y
#
# Sonics Silicon Backplane
#
# CONFIG_SSB is not set
CONFIG_BCMA_POSSIBLE=y
#
# Broadcom specific AMBA
#
# CONFIG_BCMA is not set
#
# Multifunction device drivers
#
CONFIG_MFD_CORE=y
# CONFIG_MFD_AS3711 is not set
# CONFIG_PMIC_ADP5520 is not set
# CONFIG_MFD_AAT2870_CORE is not set
# CONFIG_MFD_CROS_EC is not set
# CONFIG_MFD_ASIC3 is not set
# CONFIG_PMIC_DA903X is not set
# CONFIG_MFD_DA9052_SPI is not set
# CONFIG_MFD_DA9052_I2C is not set
# CONFIG_MFD_DA9055 is not set
# CONFIG_MFD_DA9063 is not set
# CONFIG_MFD_MC13XXX_SPI is not set
# CONFIG_MFD_MC13XXX_I2C is not set
# CONFIG_HTC_EGPIO is not set
# CONFIG_HTC_PASIC3 is not set
# CONFIG_HTC_I2CPLD is not set
# CONFIG_MFD_KEMPLD is not set
# CONFIG_MFD_88PM800 is not set
# CONFIG_MFD_88PM805 is not set
# CONFIG_MFD_88PM860X is not set
# CONFIG_MFD_MAX77686 is not set
# CONFIG_MFD_MAX77693 is not set
# CONFIG_MFD_MAX8907 is not set
# CONFIG_MFD_MAX8925 is not set
# CONFIG_MFD_MAX8997 is not set
# CONFIG_MFD_MAX8998 is not set
# CONFIG_EZX_PCAP is not set
# CONFIG_MFD_VIPERBOARD is not set
# CONFIG_MFD_RETU is not set
# CONFIG_MFD_PCF50633 is not set
# CONFIG_MFD_RC5T583 is not set
# CONFIG_MFD_SEC_CORE is not set
# CONFIG_MFD_SI476X_CORE is not set
# CONFIG_MFD_SM501 is not set
# CONFIG_MFD_SMSC is not set
# CONFIG_ABX500_CORE is not set
# CONFIG_MFD_STMPE is not set
# CONFIG_MFD_SYSCON is not set
# CONFIG_MFD_TI_AM335X_TSCADC is not set
# CONFIG_MFD_LP8788 is not set
CONFIG_MFD_OMAP_USB_HOST=y
# CONFIG_MFD_PALMAS is not set
# CONFIG_TPS6105X is not set
# CONFIG_TPS65010 is not set
# CONFIG_TPS6507X is not set
# CONFIG_MFD_TPS65090 is not set
CONFIG_MFD_TPS65217=y
# CONFIG_MFD_TPS65218 is not set
# CONFIG_MFD_TPS6586X is not set
CONFIG_MFD_TPS65910=y
# CONFIG_MFD_TPS65912 is not set
# CONFIG_MFD_TPS65912_I2C is not set
# CONFIG_MFD_TPS65912_SPI is not set
# CONFIG_MFD_TPS80031 is not set
CONFIG_TWL4030_CORE=y
# CONFIG_TWL4030_MADC is not set
CONFIG_TWL4030_POWER=y
# CONFIG_MFD_TWL4030_AUDIO is not set
# CONFIG_TWL6040_CORE is not set
# CONFIG_MFD_WL1273_CORE is not set
# CONFIG_MFD_LM3533 is not set
# CONFIG_MFD_TC3589X is not set
# CONFIG_MFD_TMIO is not set
# CONFIG_MFD_T7L66XB is not set
# CONFIG_MFD_TC6387XB is not set
# CONFIG_MFD_TC6393XB is not set
# CONFIG_MFD_ARIZONA_I2C is not set
# CONFIG_MFD_ARIZONA_SPI is not set
# CONFIG_MFD_WM8400 is not set
# CONFIG_MFD_WM831X_I2C is not set
# CONFIG_MFD_WM831X_SPI is not set
# CONFIG_MFD_WM8350_I2C is not set
# CONFIG_MFD_WM8994 is not set
# CONFIG_VEXPRESS_CONFIG is not set
CONFIG_REGULATOR=y
# CONFIG_REGULATOR_DEBUG is not set
# CONFIG_REGULATOR_DUMMY is not set
CONFIG_REGULATOR_FIXED_VOLTAGE=y
# CONFIG_REGULATOR_VIRTUAL_CONSUMER is not set
# CONFIG_REGULATOR_USERSPACE_CONSUMER is not set
# CONFIG_REGULATOR_AD5398 is not set
# CONFIG_REGULATOR_DA9210 is not set
# CONFIG_REGULATOR_FAN53555 is not set
# CONFIG_REGULATOR_GPIO is not set
# CONFIG_REGULATOR_ISL6271A is not set
# CONFIG_REGULATOR_LP3971 is not set
# CONFIG_REGULATOR_LP3972 is not set
# CONFIG_REGULATOR_LP872X is not set
# CONFIG_REGULATOR_LP8755 is not set
# CONFIG_REGULATOR_MAX1586 is not set
# CONFIG_REGULATOR_MAX8649 is not set
# CONFIG_REGULATOR_MAX8660 is not set
# CONFIG_REGULATOR_MAX8952 is not set
# CONFIG_REGULATOR_MAX8973 is not set
# CONFIG_REGULATOR_PFUZE100 is not set
# CONFIG_REGULATOR_TI_ABB is not set
# CONFIG_REGULATOR_TPS51632 is not set
# CONFIG_REGULATOR_TPS62360 is not set
# CONFIG_REGULATOR_TPS65023 is not set
# CONFIG_REGULATOR_TPS6507X is not set
# CONFIG_REGULATOR_TPS65217 is not set
# CONFIG_REGULATOR_TPS6524X is not set
CONFIG_REGULATOR_TPS65910=y
# CONFIG_REGULATOR_TWL4030 is not set
# CONFIG_REGULATOR_TIAVSCLASS0 is not set
# CONFIG_MEDIA_SUPPORT is not set
#
# Graphics support
#
# CONFIG_DRM is not set
# CONFIG_VGASTATE is not set
# CONFIG_VIDEO_OUTPUT_CONTROL is not set
# CONFIG_FB is not set
# CONFIG_OMAP2_DSS is not set
# CONFIG_EXYNOS_VIDEO is not set
# CONFIG_BACKLIGHT_LCD_SUPPORT is not set
#
# Console display driver support
#
CONFIG_DUMMY_CONSOLE=y
# CONFIG_SOUND is not set
#
# HID support
#
CONFIG_HID=y
# CONFIG_HID_BATTERY_STRENGTH is not set
# CONFIG_HIDRAW is not set
# CONFIG_UHID is not set
CONFIG_HID_GENERIC=y
#
# Special HID drivers
#
CONFIG_HID_A4TECH=y
# CONFIG_HID_ACRUX is not set
CONFIG_HID_APPLE=y
# CONFIG_HID_APPLEIR is not set
# CONFIG_HID_AUREAL is not set
CONFIG_HID_BELKIN=y
CONFIG_HID_CHERRY=y
CONFIG_HID_CHICONY=y
CONFIG_HID_CYPRESS=y
# CONFIG_HID_DRAGONRISE is not set
# CONFIG_HID_EMS_FF is not set
# CONFIG_HID_ELECOM is not set
# CONFIG_HID_ELO is not set
CONFIG_HID_EZKEY=y
# CONFIG_HID_HOLTEK is not set
# CONFIG_HID_HUION is not set
# CONFIG_HID_KEYTOUCH is not set
# CONFIG_HID_KYE is not set
# CONFIG_HID_UCLOGIC is not set
# CONFIG_HID_WALTOP is not set
# CONFIG_HID_GYRATION is not set
# CONFIG_HID_ICADE is not set
# CONFIG_HID_TWINHAN is not set
CONFIG_HID_KENSINGTON=y
# CONFIG_HID_LCPOWER is not set
# CONFIG_HID_LENOVO_TPKBD is not set
CONFIG_HID_LOGITECH=y
# CONFIG_HID_LOGITECH_DJ is not set
# CONFIG_LOGITECH_FF is not set
# CONFIG_LOGIRUMBLEPAD2_FF is not set
# CONFIG_LOGIG940_FF is not set
# CONFIG_LOGIWHEELS_FF is not set
# CONFIG_HID_MAGICMOUSE is not set
CONFIG_HID_MICROSOFT=y
CONFIG_HID_MONTEREY=y
# CONFIG_HID_MULTITOUCH is not set
# CONFIG_HID_NTRIG is not set
# CONFIG_HID_ORTEK is not set
# CONFIG_HID_PANTHERLORD is not set
# CONFIG_HID_PETALYNX is not set
# CONFIG_HID_PICOLCD is not set
# CONFIG_HID_PRIMAX is not set
# CONFIG_HID_ROCCAT is not set
# CONFIG_HID_SAITEK is not set
# CONFIG_HID_SAMSUNG is not set
# CONFIG_HID_SONY is not set
# CONFIG_HID_SPEEDLINK is not set
# CONFIG_HID_STEELSERIES is not set
# CONFIG_HID_SUNPLUS is not set
# CONFIG_HID_GREENASIA is not set
# CONFIG_HID_SMARTJOYPLUS is not set
# CONFIG_HID_TIVO is not set
# CONFIG_HID_TOPSEED is not set
# CONFIG_HID_THINGM is not set
# CONFIG_HID_THRUSTMASTER is not set
# CONFIG_HID_WACOM is not set
# CONFIG_HID_WIIMOTE is not set
# CONFIG_HID_XINMO is not set
# CONFIG_HID_ZEROPLUS is not set
# CONFIG_HID_ZYDACRON is not set
# CONFIG_HID_SENSOR_HUB is not set
#
# USB HID support
#
CONFIG_USB_HID=y
# CONFIG_HID_PID is not set
# CONFIG_USB_HIDDEV is not set
#
# I2C HID support
#
# CONFIG_I2C_HID is not set
CONFIG_USB_OHCI_LITTLE_ENDIAN=y
CONFIG_USB_ARCH_HAS_EHCI=y
CONFIG_USB_SUPPORT=y
CONFIG_USB_COMMON=y
CONFIG_USB_ARCH_HAS_HCD=y
CONFIG_USB=y
CONFIG_USB_DEBUG=y
CONFIG_USB_ANNOUNCE_NEW_DEVICES=y
#
# Miscellaneous USB options
#
CONFIG_USB_DEFAULT_PERSIST=y
# CONFIG_USB_DYNAMIC_MINORS is not set
# CONFIG_USB_OTG is not set
CONFIG_USB_MON=y
# CONFIG_USB_WUSB_CBAF is not set
#
# USB Host Controller Drivers
#
# CONFIG_USB_C67X00_HCD is not set
# CONFIG_USB_XHCI_HCD is not set
CONFIG_USB_EHCI_HCD=y
CONFIG_USB_EHCI_ROOT_HUB_TT=y
CONFIG_USB_EHCI_TT_NEWSCHED=y
CONFIG_USB_EHCI_HCD_OMAP=y
CONFIG_USB_EHCI_HCD_PLATFORM=y
# CONFIG_USB_OXU210HP_HCD is not set
# CONFIG_USB_ISP116X_HCD is not set
# CONFIG_USB_ISP1760_HCD is not set
# CONFIG_USB_ISP1362_HCD is not set
# CONFIG_USB_FUSBH200_HCD is not set
# CONFIG_USB_FOTG210_HCD is not set
CONFIG_USB_OHCI_HCD=y
CONFIG_USB_OHCI_HCD_OMAP3=y
CONFIG_USB_OHCI_HCD_PLATFORM=y
# CONFIG_USB_SL811_HCD is not set
# CONFIG_USB_R8A66597_HCD is not set
# CONFIG_USB_HCD_TEST_MODE is not set
CONFIG_USB_MUSB_HDRC=y
CONFIG_USB_MUSB_HOST=y
# CONFIG_USB_MUSB_GADGET is not set
# CONFIG_USB_MUSB_DUAL_ROLE is not set
# CONFIG_USB_MUSB_TUSB6010 is not set
# CONFIG_USB_MUSB_OMAP2PLUS is not set
# CONFIG_USB_MUSB_AM35X is not set
CONFIG_USB_MUSB_DSPS=y
# CONFIG_USB_MUSB_UX500 is not set
CONFIG_USB_MUSB_AM335X_CHILD=y
CONFIG_USB_TI_CPPI41_DMA=y
# CONFIG_MUSB_PIO_ONLY is not set
# CONFIG_USB_RENESAS_USBHS is not set
#
# USB Device Class drivers
#
CONFIG_USB_ACM=y
# CONFIG_USB_PRINTER is not set
CONFIG_USB_WDM=y
# CONFIG_USB_TMC is not set
#
# NOTE: USB_STORAGE depends on SCSI but BLK_DEV_SD may
#
#
# also be needed; see USB_STORAGE Help for more info
#
CONFIG_USB_STORAGE=y
CONFIG_USB_STORAGE_DEBUG=y
# CONFIG_USB_STORAGE_REALTEK is not set
# CONFIG_USB_STORAGE_DATAFAB is not set
# CONFIG_USB_STORAGE_FREECOM is not set
# CONFIG_USB_STORAGE_ISD200 is not set
# CONFIG_USB_STORAGE_USBAT is not set
# CONFIG_USB_STORAGE_SDDR09 is not set
# CONFIG_USB_STORAGE_SDDR55 is not set
# CONFIG_USB_STORAGE_JUMPSHOT is not set
# CONFIG_USB_STORAGE_ALAUDA is not set
# CONFIG_USB_STORAGE_ONETOUCH is not set
# CONFIG_USB_STORAGE_KARMA is not set
# CONFIG_USB_STORAGE_CYPRESS_ATACB is not set
# CONFIG_USB_STORAGE_ENE_UB6250 is not set
#
# USB Imaging devices
#
# CONFIG_USB_MDC800 is not set
# CONFIG_USB_MICROTEK is not set
# CONFIG_USB_CHIPIDEA is not set
#
# USB port drivers
#
# CONFIG_USB_SERIAL is not set
#
# USB Miscellaneous drivers
#
# CONFIG_USB_EMI62 is not set
# CONFIG_USB_EMI26 is not set
# CONFIG_USB_ADUTUX is not set
# CONFIG_USB_SEVSEG is not set
# CONFIG_USB_RIO500 is not set
# CONFIG_USB_LEGOTOWER is not set
# CONFIG_USB_LCD is not set
# CONFIG_USB_LED is not set
# CONFIG_USB_CYPRESS_CY7C63 is not set
# CONFIG_USB_CYTHERM is not set
# CONFIG_USB_IDMOUSE is not set
# CONFIG_USB_FTDI_ELAN is not set
# CONFIG_USB_APPLEDISPLAY is not set
# CONFIG_USB_SISUSBVGA is not set
# CONFIG_USB_LD is not set
# CONFIG_USB_TRANCEVIBRATOR is not set
# CONFIG_USB_IOWARRIOR is not set
# CONFIG_USB_TEST is not set
# CONFIG_USB_EHSET_TEST_FIXTURE is not set
# CONFIG_USB_ISIGHTFW is not set
# CONFIG_USB_YUREX is not set
# CONFIG_USB_EZUSB_FX2 is not set
# CONFIG_USB_HSIC_USB3503 is not set
#
# USB Physical Layer drivers
#
CONFIG_USB_PHY=y
CONFIG_NOP_USB_XCEIV=y
CONFIG_AM335X_CONTROL_USB=y
CONFIG_AM335X_PHY_USB=y
# CONFIG_SAMSUNG_USB2PHY is not set
# CONFIG_SAMSUNG_USB3PHY is not set
# CONFIG_USB_GPIO_VBUS is not set
# CONFIG_USB_ISP1301 is not set
# CONFIG_USB_RCAR_PHY is not set
# CONFIG_USB_ULPI is not set
CONFIG_USB_GADGET=y
# CONFIG_USB_GADGET_DEBUG is not set
# CONFIG_USB_GADGET_DEBUG_FILES is not set
# CONFIG_USB_GADGET_DEBUG_FS is not set
CONFIG_USB_GADGET_VBUS_DRAW=500
CONFIG_USB_GADGET_STORAGE_NUM_BUFFERS=2
#
# USB Peripheral Controller
#
# CONFIG_USB_FUSB300 is not set
# CONFIG_USB_FOTG210_UDC is not set
# CONFIG_USB_R8A66597 is not set
# CONFIG_USB_PXA27X is not set
# CONFIG_USB_MV_UDC is not set
# CONFIG_USB_MV_U3D is not set
# CONFIG_USB_M66592 is not set
# CONFIG_USB_NET2272 is not set
# CONFIG_USB_DUMMY_HCD is not set
CONFIG_USB_LIBCOMPOSITE=y
CONFIG_USB_F_MASS_STORAGE=y
# CONFIG_USB_CONFIGFS is not set
# CONFIG_USB_ZERO is not set
# CONFIG_USB_ETH is not set
# CONFIG_USB_G_NCM is not set
# CONFIG_USB_GADGETFS is not set
# CONFIG_USB_FUNCTIONFS is not set
CONFIG_USB_MASS_STORAGE=y
# CONFIG_USB_G_SERIAL is not set
# CONFIG_USB_G_PRINTER is not set
# CONFIG_USB_CDC_COMPOSITE is not set
# CONFIG_USB_G_ACM_MS is not set
# CONFIG_USB_G_MULTI is not set
# CONFIG_USB_G_HID is not set
# CONFIG_USB_G_DBGP is not set
CONFIG_MMC=y
# CONFIG_MMC_DEBUG is not set
# CONFIG_MMC_UNSAFE_RESUME is not set
# CONFIG_MMC_CLKGATE is not set
#
# MMC/SD/SDIO Card Drivers
#
CONFIG_MMC_BLOCK=y
CONFIG_MMC_BLOCK_MINORS=8
CONFIG_MMC_BLOCK_BOUNCE=y
CONFIG_SDIO_UART=y
# CONFIG_MMC_TEST is not set
#
# MMC/SD/SDIO Host Controller Drivers
#
# CONFIG_MMC_SDHCI is not set
# CONFIG_MMC_SDHCI_PXAV3 is not set
# CONFIG_MMC_SDHCI_PXAV2 is not set
CONFIG_MMC_OMAP=y
CONFIG_MMC_OMAP_HS=y
# CONFIG_MMC_DW is not set
# CONFIG_MMC_VUB300 is not set
# CONFIG_MMC_USHC is not set
# CONFIG_MEMSTICK is not set
CONFIG_NEW_LEDS=y
CONFIG_LEDS_CLASS=y
#
# LED drivers
#
# CONFIG_LEDS_LM3530 is not set
# CONFIG_LEDS_LM3642 is not set
# CONFIG_LEDS_PCA9532 is not set
CONFIG_LEDS_GPIO=y
# CONFIG_LEDS_LP3944 is not set
# CONFIG_LEDS_LP5521 is not set
# CONFIG_LEDS_LP5523 is not set
# CONFIG_LEDS_LP5562 is not set
# CONFIG_LEDS_LP8501 is not set
# CONFIG_LEDS_PCA955X is not set
# CONFIG_LEDS_PCA963X is not set
# CONFIG_LEDS_DAC124S085 is not set
# CONFIG_LEDS_PWM is not set
# CONFIG_LEDS_REGULATOR is not set
# CONFIG_LEDS_BD2802 is not set
# CONFIG_LEDS_LT3593 is not set
# CONFIG_LEDS_TCA6507 is not set
# CONFIG_LEDS_LM355x is not set
# CONFIG_LEDS_OT200 is not set
# CONFIG_LEDS_BLINKM is not set
#
# LED Triggers
#
CONFIG_LEDS_TRIGGERS=y
CONFIG_LEDS_TRIGGER_TIMER=y
CONFIG_LEDS_TRIGGER_ONESHOT=y
CONFIG_LEDS_TRIGGER_HEARTBEAT=y
CONFIG_LEDS_TRIGGER_BACKLIGHT=y
CONFIG_LEDS_TRIGGER_CPU=y
CONFIG_LEDS_TRIGGER_GPIO=y
CONFIG_LEDS_TRIGGER_DEFAULT_ON=y
#
# iptables trigger is under Netfilter config (LED target)
#
# CONFIG_LEDS_TRIGGER_TRANSIENT is not set
# CONFIG_LEDS_TRIGGER_CAMERA is not set
# CONFIG_ACCESSIBILITY is not set
# CONFIG_EDAC is not set
CONFIG_RTC_LIB=y
CONFIG_RTC_CLASS=y
CONFIG_RTC_HCTOSYS=y
CONFIG_RTC_SYSTOHC=y
CONFIG_RTC_HCTOSYS_DEVICE="rtc1"
CONFIG_RTC_DEBUG=y
#
# RTC interfaces
#
CONFIG_RTC_INTF_SYSFS=y
CONFIG_RTC_INTF_PROC=y
CONFIG_RTC_INTF_DEV=y
# CONFIG_RTC_INTF_DEV_UIE_EMUL is not set
# CONFIG_RTC_DRV_TEST is not set
#
# I2C RTC drivers
#
CONFIG_RTC_DRV_DS1307=y
CONFIG_RTC_DRV_DS1374=y
# CONFIG_RTC_DRV_DS1672 is not set
# CONFIG_RTC_DRV_DS3232 is not set
# CONFIG_RTC_DRV_MAX6900 is not set
# CONFIG_RTC_DRV_RS5C372 is not set
# CONFIG_RTC_DRV_ISL1208 is not set
# CONFIG_RTC_DRV_ISL12022 is not set
# CONFIG_RTC_DRV_X1205 is not set
# CONFIG_RTC_DRV_PCF2127 is not set
# CONFIG_RTC_DRV_PCF8523 is not set
# CONFIG_RTC_DRV_PCF8563 is not set
# CONFIG_RTC_DRV_PCF8583 is not set
# CONFIG_RTC_DRV_M41T80 is not set
# CONFIG_RTC_DRV_BQ32K is not set
# CONFIG_RTC_DRV_TWL4030 is not set
# CONFIG_RTC_DRV_TPS65910 is not set
# CONFIG_RTC_DRV_S35390A is not set
# CONFIG_RTC_DRV_FM3130 is not set
# CONFIG_RTC_DRV_RX8581 is not set
# CONFIG_RTC_DRV_RX8025 is not set
# CONFIG_RTC_DRV_EM3027 is not set
# CONFIG_RTC_DRV_RV3029C2 is not set
#
# SPI RTC drivers
#
# CONFIG_RTC_DRV_M41T93 is not set
# CONFIG_RTC_DRV_M41T94 is not set
# CONFIG_RTC_DRV_DS1305 is not set
# CONFIG_RTC_DRV_DS1390 is not set
# CONFIG_RTC_DRV_MAX6902 is not set
# CONFIG_RTC_DRV_R9701 is not set
# CONFIG_RTC_DRV_RS5C348 is not set
# CONFIG_RTC_DRV_DS3234 is not set
# CONFIG_RTC_DRV_PCF2123 is not set
# CONFIG_RTC_DRV_RX4581 is not set
#
# Platform RTC drivers
#
# CONFIG_RTC_DRV_CMOS is not set
# CONFIG_RTC_DRV_DS1286 is not set
# CONFIG_RTC_DRV_DS1511 is not set
# CONFIG_RTC_DRV_DS1553 is not set
# CONFIG_RTC_DRV_DS1742 is not set
# CONFIG_RTC_DRV_STK17TA8 is not set
# CONFIG_RTC_DRV_M48T86 is not set
# CONFIG_RTC_DRV_M48T35 is not set
# CONFIG_RTC_DRV_M48T59 is not set
# CONFIG_RTC_DRV_MSM6242 is not set
# CONFIG_RTC_DRV_BQ4802 is not set
# CONFIG_RTC_DRV_RP5C01 is not set
# CONFIG_RTC_DRV_V3020 is not set
# CONFIG_RTC_DRV_DS2404 is not set
#
# on-CPU RTC drivers
#
CONFIG_RTC_DRV_OMAP=y
# CONFIG_RTC_DRV_SNVS is not set
# CONFIG_RTC_DRV_MOXART is not set
#
# HID Sensor RTC drivers
#
# CONFIG_RTC_DRV_HID_SENSOR_TIME is not set
CONFIG_DMADEVICES=y
# CONFIG_DMADEVICES_DEBUG is not set
#
# DMA Devices
#
# CONFIG_DW_DMAC_CORE is not set
# CONFIG_DW_DMAC is not set
# CONFIG_TIMB_DMA is not set
CONFIG_TI_EDMA=y
CONFIG_DMA_OMAP=y
CONFIG_TI_CPPI41=y
CONFIG_DMA_ENGINE=y
CONFIG_DMA_VIRTUAL_CHANNELS=y
CONFIG_DMA_OF=y
#
# DMA Clients
#
# CONFIG_ASYNC_TX_DMA is not set
# CONFIG_DMATEST is not set
# CONFIG_AUXDISPLAY is not set
# CONFIG_UIO is not set
# CONFIG_VIRT_DRIVERS is not set
#
# Virtio drivers
#
# CONFIG_VIRTIO_MMIO is not set
#
# Microsoft Hyper-V guest support
#
# CONFIG_STAGING is not set
CONFIG_CLKDEV_LOOKUP=y
CONFIG_HAVE_CLK_PREPARE=y
CONFIG_COMMON_CLK=y
#
# Common Clock Framework
#
CONFIG_COMMON_CLK_DEBUG=y
# CONFIG_COMMON_CLK_SI5351 is not set
#
# Hardware Spinlock drivers
#
# CONFIG_HWSPINLOCK_OMAP is not set
CONFIG_CLKSRC_OF=y
CONFIG_CLKSRC_MMIO=y
CONFIG_ARM_ARCH_TIMER=y
CONFIG_MAILBOX=y
CONFIG_OMAP_MBOX=y
CONFIG_OMAP2PLUS_MBOX=y
CONFIG_OMAP_MBOX_KFIFO_SIZE=256
# CONFIG_IOMMU_SUPPORT is not set
#
# Remoteproc drivers
#
# CONFIG_STE_MODEM_RPROC is not set
#
# Rpmsg drivers
#
# CONFIG_PM_DEVFREQ is not set
# CONFIG_EXTCON is not set
# CONFIG_MEMORY is not set
# CONFIG_IIO is not set
CONFIG_PWM=y
CONFIG_PWM_SYSFS=y
# CONFIG_PWM_PCA9685 is not set
CONFIG_PWM_TIECAP=y
CONFIG_PWM_TIEHRPWM=y
CONFIG_PWM_TIPWMSS=y
# CONFIG_PWM_TWL is not set
# CONFIG_PWM_TWL_LED is not set
CONFIG_IRQCHIP=y
CONFIG_ARM_GIC=y
# CONFIG_IPACK_BUS is not set
CONFIG_ARCH_HAS_RESET_CONTROLLER=y
CONFIG_RESET_CONTROLLER=y
CONFIG_RESET_TI=y
# CONFIG_FMC is not set
#
# PHY Subsystem
#
CONFIG_GENERIC_PHY=y
CONFIG_OMAP_CONTROL_PHY=y
CONFIG_OMAP_USB2=y
CONFIG_OMAP_PIPE3=y
#
# File systems
#
CONFIG_DCACHE_WORD_ACCESS=y
CONFIG_EXT2_FS=y
# CONFIG_EXT2_FS_XATTR is not set
# CONFIG_EXT2_FS_XIP is not set
CONFIG_EXT3_FS=y
CONFIG_EXT3_DEFAULTS_TO_ORDERED=y
# CONFIG_EXT3_FS_XATTR is not set
CONFIG_EXT4_FS=y
# CONFIG_EXT4_FS_POSIX_ACL is not set
# CONFIG_EXT4_FS_SECURITY is not set
# CONFIG_EXT4_DEBUG is not set
CONFIG_JBD=y
# CONFIG_JBD_DEBUG is not set
CONFIG_JBD2=y
# CONFIG_JBD2_DEBUG is not set
CONFIG_FS_MBCACHE=y
# CONFIG_REISERFS_FS is not set
# CONFIG_JFS_FS is not set
# CONFIG_XFS_FS is not set
# CONFIG_GFS2_FS is not set
# CONFIG_OCFS2_FS is not set
# CONFIG_BTRFS_FS is not set
# CONFIG_NILFS2_FS is not set
CONFIG_FS_POSIX_ACL=y
CONFIG_FILE_LOCKING=y
CONFIG_FSNOTIFY=y
CONFIG_DNOTIFY=y
CONFIG_INOTIFY_USER=y
# CONFIG_FANOTIFY is not set
# CONFIG_QUOTA is not set
# CONFIG_QUOTACTL is not set
# CONFIG_AUTOFS4_FS is not set
# CONFIG_FUSE_FS is not set
#
# Caches
#
# CONFIG_FSCACHE is not set
#
# CD-ROM/DVD Filesystems
#
# CONFIG_ISO9660_FS is not set
# CONFIG_UDF_FS is not set
#
# DOS/FAT/NT Filesystems
#
CONFIG_FAT_FS=y
CONFIG_MSDOS_FS=y
CONFIG_VFAT_FS=y
CONFIG_FAT_DEFAULT_CODEPAGE=437
CONFIG_FAT_DEFAULT_IOCHARSET="iso8859-1"
# CONFIG_NTFS_FS is not set
#
# Pseudo filesystems
#
CONFIG_PROC_FS=y
CONFIG_PROC_SYSCTL=y
CONFIG_PROC_PAGE_MONITOR=y
CONFIG_SYSFS=y
CONFIG_TMPFS=y
# CONFIG_TMPFS_POSIX_ACL is not set
# CONFIG_TMPFS_XATTR is not set
# CONFIG_HUGETLB_PAGE is not set
CONFIG_CONFIGFS_FS=y
CONFIG_MISC_FILESYSTEMS=y
# CONFIG_ADFS_FS is not set
# CONFIG_AFFS_FS is not set
# CONFIG_ECRYPT_FS is not set
# CONFIG_HFS_FS is not set
# CONFIG_HFSPLUS_FS is not set
# CONFIG_BEFS_FS is not set
# CONFIG_BFS_FS is not set
# CONFIG_EFS_FS is not set
# CONFIG_JFFS2_FS is not set
CONFIG_UBIFS_FS=y
# CONFIG_UBIFS_FS_ADVANCED_COMPR is not set
CONFIG_UBIFS_FS_LZO=y
CONFIG_UBIFS_FS_ZLIB=y
# CONFIG_LOGFS is not set
# CONFIG_CRAMFS is not set
# CONFIG_SQUASHFS is not set
# CONFIG_VXFS_FS is not set
# CONFIG_MINIX_FS is not set
# CONFIG_OMFS_FS is not set
# CONFIG_HPFS_FS is not set
# CONFIG_QNX4FS_FS is not set
# CONFIG_QNX6FS_FS is not set
# CONFIG_ROMFS_FS is not set
# CONFIG_PSTORE is not set
# CONFIG_SYSV_FS is not set
# CONFIG_UFS_FS is not set
# CONFIG_F2FS_FS is not set
CONFIG_NETWORK_FILESYSTEMS=y
CONFIG_NFS_FS=y
CONFIG_NFS_V2=y
CONFIG_NFS_V3=y
CONFIG_NFS_V3_ACL=y
CONFIG_NFS_V4=y
# CONFIG_NFS_SWAP is not set
# CONFIG_NFS_V4_1 is not set
CONFIG_ROOT_NFS=y
# CONFIG_NFS_USE_LEGACY_DNS is not set
CONFIG_NFS_USE_KERNEL_DNS=y
# CONFIG_NFSD is not set
CONFIG_LOCKD=y
CONFIG_LOCKD_V4=y
CONFIG_NFS_ACL_SUPPORT=y
CONFIG_NFS_COMMON=y
CONFIG_SUNRPC=y
CONFIG_SUNRPC_GSS=y
# CONFIG_SUNRPC_DEBUG is not set
# CONFIG_CEPH_FS is not set
# CONFIG_CIFS is not set
# CONFIG_NCP_FS is not set
# CONFIG_CODA_FS is not set
# CONFIG_AFS_FS is not set
CONFIG_NLS=y
CONFIG_NLS_DEFAULT="iso8859-1"
CONFIG_NLS_CODEPAGE_437=y
# CONFIG_NLS_CODEPAGE_737 is not set
# CONFIG_NLS_CODEPAGE_775 is not set
# CONFIG_NLS_CODEPAGE_850 is not set
# CONFIG_NLS_CODEPAGE_852 is not set
# CONFIG_NLS_CODEPAGE_855 is not set
# CONFIG_NLS_CODEPAGE_857 is not set
# CONFIG_NLS_CODEPAGE_860 is not set
# CONFIG_NLS_CODEPAGE_861 is not set
# CONFIG_NLS_CODEPAGE_862 is not set
# CONFIG_NLS_CODEPAGE_863 is not set
# CONFIG_NLS_CODEPAGE_864 is not set
# CONFIG_NLS_CODEPAGE_865 is not set
# CONFIG_NLS_CODEPAGE_866 is not set
# CONFIG_NLS_CODEPAGE_869 is not set
# CONFIG_NLS_CODEPAGE_936 is not set
# CONFIG_NLS_CODEPAGE_950 is not set
# CONFIG_NLS_CODEPAGE_932 is not set
# CONFIG_NLS_CODEPAGE_949 is not set
# CONFIG_NLS_CODEPAGE_874 is not set
# CONFIG_NLS_ISO8859_8 is not set
# CONFIG_NLS_CODEPAGE_1250 is not set
# CONFIG_NLS_CODEPAGE_1251 is not set
# CONFIG_NLS_ASCII is not set
CONFIG_NLS_ISO8859_1=y
# CONFIG_NLS_ISO8859_2 is not set
# CONFIG_NLS_ISO8859_3 is not set
# CONFIG_NLS_ISO8859_4 is not set
# CONFIG_NLS_ISO8859_5 is not set
# CONFIG_NLS_ISO8859_6 is not set
# CONFIG_NLS_ISO8859_7 is not set
# CONFIG_NLS_ISO8859_9 is not set
# CONFIG_NLS_ISO8859_13 is not set
# CONFIG_NLS_ISO8859_14 is not set
# CONFIG_NLS_ISO8859_15 is not set
# CONFIG_NLS_KOI8_R is not set
# CONFIG_NLS_KOI8_U is not set
# CONFIG_NLS_MAC_ROMAN is not set
# CONFIG_NLS_MAC_CELTIC is not set
# CONFIG_NLS_MAC_CENTEURO is not set
# CONFIG_NLS_MAC_CROATIAN is not set
# CONFIG_NLS_MAC_CYRILLIC is not set
# CONFIG_NLS_MAC_GAELIC is not set
# CONFIG_NLS_MAC_GREEK is not set
# CONFIG_NLS_MAC_ICELAND is not set
# CONFIG_NLS_MAC_INUIT is not set
# CONFIG_NLS_MAC_ROMANIAN is not set
# CONFIG_NLS_MAC_TURKISH is not set
# CONFIG_NLS_UTF8 is not set
# CONFIG_DLM is not set
#
# Kernel hacking
#
#
# printk and dmesg options
#
CONFIG_PRINTK_TIME=y
CONFIG_DEFAULT_MESSAGE_LOGLEVEL=7
# CONFIG_BOOT_PRINTK_DELAY is not set
# CONFIG_DYNAMIC_DEBUG is not set
#
# Compile-time checks and compiler options
#
# CONFIG_DEBUG_INFO is not set
CONFIG_ENABLE_WARN_DEPRECATED=y
CONFIG_ENABLE_MUST_CHECK=y
CONFIG_FRAME_WARN=1024
# CONFIG_STRIP_ASM_SYMS is not set
# CONFIG_READABLE_ASM is not set
# CONFIG_UNUSED_SYMBOLS is not set
CONFIG_DEBUG_FS=y
# CONFIG_HEADERS_CHECK is not set
# CONFIG_DEBUG_SECTION_MISMATCH is not set
# CONFIG_DEBUG_FORCE_WEAK_PER_CPU is not set
# CONFIG_MAGIC_SYSRQ is not set
CONFIG_DEBUG_KERNEL=y
#
# Memory Debugging
#
# CONFIG_DEBUG_PAGEALLOC is not set
# CONFIG_DEBUG_OBJECTS is not set
# CONFIG_DEBUG_SLAB is not set
CONFIG_HAVE_DEBUG_KMEMLEAK=y
# CONFIG_DEBUG_KMEMLEAK is not set
# CONFIG_DEBUG_STACK_USAGE is not set
# CONFIG_DEBUG_VM is not set
CONFIG_DEBUG_MEMORY_INIT=y
# CONFIG_DEBUG_HIGHMEM is not set
# CONFIG_DEBUG_SHIRQ is not set
#
# Debug Lockups and Hangs
#
# CONFIG_LOCKUP_DETECTOR is not set
# CONFIG_DETECT_HUNG_TASK is not set
CONFIG_PANIC_ON_OOPS=y
CONFIG_PANIC_ON_OOPS_VALUE=1
CONFIG_SCHED_DEBUG=y
# CONFIG_SCHEDSTATS is not set
# CONFIG_TIMER_STATS is not set
#
# Lock Debugging (spinlocks, mutexes, etc...)
#
# CONFIG_DEBUG_RT_MUTEXES is not set
# CONFIG_RT_MUTEX_TESTER is not set
# CONFIG_DEBUG_SPINLOCK is not set
# CONFIG_DEBUG_MUTEXES is not set
# CONFIG_DEBUG_WW_MUTEX_SLOWPATH is not set
# CONFIG_DEBUG_LOCK_ALLOC is not set
# CONFIG_PROVE_LOCKING is not set
# CONFIG_LOCK_STAT is not set
# CONFIG_DEBUG_ATOMIC_SLEEP is not set
# CONFIG_DEBUG_LOCKING_API_SELFTESTS is not set
# CONFIG_DEBUG_KOBJECT is not set
CONFIG_DEBUG_BUGVERBOSE=y
# CONFIG_DEBUG_WRITECOUNT is not set
# CONFIG_DEBUG_LIST is not set
# CONFIG_DEBUG_SG is not set
# CONFIG_DEBUG_NOTIFIERS is not set
# CONFIG_DEBUG_CREDENTIALS is not set
#
# RCU Debugging
#
# CONFIG_SPARSE_RCU_POINTER is not set
# CONFIG_RCU_TORTURE_TEST is not set
# CONFIG_RCU_TRACE is not set
# CONFIG_DEBUG_BLOCK_EXT_DEVT is not set
# CONFIG_NOTIFIER_ERROR_INJECTION is not set
# CONFIG_FAULT_INJECTION is not set
# CONFIG_LATENCYTOP is not set
CONFIG_HAVE_FUNCTION_TRACER=y
CONFIG_HAVE_FUNCTION_GRAPH_TRACER=y
CONFIG_HAVE_DYNAMIC_FTRACE=y
CONFIG_HAVE_FTRACE_MCOUNT_RECORD=y
CONFIG_HAVE_SYSCALL_TRACEPOINTS=y
CONFIG_HAVE_C_RECORDMCOUNT=y
CONFIG_TRACING_SUPPORT=y
# CONFIG_FTRACE is not set
#
# Runtime Testing
#
# CONFIG_LKDTM is not set
# CONFIG_TEST_LIST_SORT is not set
# CONFIG_BACKTRACE_SELF_TEST is not set
# CONFIG_RBTREE_TEST is not set
# CONFIG_ATOMIC64_SELFTEST is not set
# CONFIG_TEST_STRING_HELPERS is not set
# CONFIG_TEST_KSTRTOX is not set
# CONFIG_DMA_API_DEBUG is not set
# CONFIG_SAMPLES is not set
CONFIG_HAVE_ARCH_KGDB=y
# CONFIG_KGDB is not set
# CONFIG_STRICT_DEVMEM is not set
CONFIG_ARM_UNWIND=y
# CONFIG_DEBUG_USER is not set
# CONFIG_DEBUG_LL is not set
CONFIG_DEBUG_LL_INCLUDE="mach/debug-macro.S"
# CONFIG_DEBUG_UART_PL01X is not set
# CONFIG_DEBUG_UART_8250 is not set
CONFIG_UNCOMPRESS_INCLUDE="debug/uncompress.h"
# CONFIG_PID_IN_CONTEXTIDR is not set
#
# Security options
#
CONFIG_KEYS=y
# CONFIG_ENCRYPTED_KEYS is not set
# CONFIG_KEYS_DEBUG_PROC_KEYS is not set
# CONFIG_SECURITY_DMESG_RESTRICT is not set
CONFIG_SECURITY=y
# CONFIG_SECURITYFS is not set
# CONFIG_SECURITY_NETWORK is not set
# CONFIG_SECURITY_PATH is not set
# CONFIG_SECURITY_SMACK is not set
# CONFIG_SECURITY_TOMOYO is not set
# CONFIG_SECURITY_APPARMOR is not set
# CONFIG_SECURITY_YAMA is not set
# CONFIG_IMA is not set
# CONFIG_EVM is not set
CONFIG_DEFAULT_SECURITY_DAC=y
CONFIG_DEFAULT_SECURITY=""
CONFIG_CRYPTO=y
#
# Crypto core or helper
#
CONFIG_CRYPTO_ALGAPI=y
CONFIG_CRYPTO_ALGAPI2=y
CONFIG_CRYPTO_AEAD=y
CONFIG_CRYPTO_AEAD2=y
CONFIG_CRYPTO_BLKCIPHER=y
CONFIG_CRYPTO_BLKCIPHER2=y
CONFIG_CRYPTO_HASH=y
CONFIG_CRYPTO_HASH2=y
CONFIG_CRYPTO_RNG2=y
CONFIG_CRYPTO_PCOMP2=y
CONFIG_CRYPTO_MANAGER=y
CONFIG_CRYPTO_MANAGER2=y
# CONFIG_CRYPTO_USER is not set
CONFIG_CRYPTO_MANAGER_DISABLE_TESTS=y
# CONFIG_CRYPTO_GF128MUL is not set
# CONFIG_CRYPTO_NULL is not set
CONFIG_CRYPTO_WORKQUEUE=y
# CONFIG_CRYPTO_CRYPTD is not set
CONFIG_CRYPTO_AUTHENC=y
#
# Authenticated Encryption with Associated Data
#
# CONFIG_CRYPTO_CCM is not set
# CONFIG_CRYPTO_GCM is not set
# CONFIG_CRYPTO_SEQIV is not set
#
# Block modes
#
CONFIG_CRYPTO_CBC=y
# CONFIG_CRYPTO_CTR is not set
# CONFIG_CRYPTO_CTS is not set
CONFIG_CRYPTO_ECB=y
# CONFIG_CRYPTO_LRW is not set
# CONFIG_CRYPTO_PCBC is not set
# CONFIG_CRYPTO_XTS is not set
#
# Hash modes
#
# CONFIG_CRYPTO_CMAC is not set
CONFIG_CRYPTO_HMAC=y
# CONFIG_CRYPTO_XCBC is not set
# CONFIG_CRYPTO_VMAC is not set
#
# Digest
#
CONFIG_CRYPTO_CRC32C=y
# CONFIG_CRYPTO_CRC32 is not set
CONFIG_CRYPTO_CRCT10DIF=y
# CONFIG_CRYPTO_GHASH is not set
# CONFIG_CRYPTO_MD4 is not set
CONFIG_CRYPTO_MD5=y
CONFIG_CRYPTO_MICHAEL_MIC=y
# CONFIG_CRYPTO_RMD128 is not set
# CONFIG_CRYPTO_RMD160 is not set
# CONFIG_CRYPTO_RMD256 is not set
# CONFIG_CRYPTO_RMD320 is not set
CONFIG_CRYPTO_SHA1=y
# CONFIG_CRYPTO_SHA1_ARM is not set
CONFIG_CRYPTO_SHA256=y
CONFIG_CRYPTO_SHA512=y
# CONFIG_CRYPTO_TGR192 is not set
# CONFIG_CRYPTO_WP512 is not set
#
# Ciphers
#
CONFIG_CRYPTO_AES=y
CONFIG_CRYPTO_AES_ARM=y
# CONFIG_CRYPTO_ANUBIS is not set
CONFIG_CRYPTO_ARC4=y
# CONFIG_CRYPTO_BLOWFISH is not set
# CONFIG_CRYPTO_CAMELLIA is not set
# CONFIG_CRYPTO_CAST5 is not set
# CONFIG_CRYPTO_CAST6 is not set
CONFIG_CRYPTO_DES=y
# CONFIG_CRYPTO_FCRYPT is not set
# CONFIG_CRYPTO_KHAZAD is not set
# CONFIG_CRYPTO_SALSA20 is not set
# CONFIG_CRYPTO_SEED is not set
# CONFIG_CRYPTO_SERPENT is not set
# CONFIG_CRYPTO_TEA is not set
# CONFIG_CRYPTO_TWOFISH is not set
#
# Compression
#
CONFIG_CRYPTO_DEFLATE=y
# CONFIG_CRYPTO_ZLIB is not set
CONFIG_CRYPTO_LZO=y
# CONFIG_CRYPTO_LZ4 is not set
# CONFIG_CRYPTO_LZ4HC is not set
#
# Random Number Generation
#
# CONFIG_CRYPTO_ANSI_CPRNG is not set
# CONFIG_CRYPTO_USER_API_HASH is not set
# CONFIG_CRYPTO_USER_API_SKCIPHER is not set
CONFIG_CRYPTO_HW=y
CONFIG_CRYPTO_DEV_OMAP_SHAM=y
CONFIG_CRYPTO_DEV_OMAP_AES=y
CONFIG_CRYPTO_DEV_OMAP_DES=y
CONFIG_ASYMMETRIC_KEY_TYPE=y
CONFIG_ASYMMETRIC_PUBLIC_KEY_SUBTYPE=y
CONFIG_PUBLIC_KEY_ALGO_RSA=y
CONFIG_X509_CERTIFICATE_PARSER=y
# CONFIG_BINARY_PRINTF is not set
#
# Library routines
#
CONFIG_BITREVERSE=y
CONFIG_GENERIC_STRNCPY_FROM_USER=y
CONFIG_GENERIC_STRNLEN_USER=y
CONFIG_GENERIC_NET_UTILS=y
CONFIG_GENERIC_PCI_IOMAP=y
CONFIG_GENERIC_IO=y
CONFIG_CRC_CCITT=y
CONFIG_CRC16=y
CONFIG_CRC_T10DIF=y
CONFIG_CRC_ITU_T=y
CONFIG_CRC32=y
# CONFIG_CRC32_SELFTEST is not set
CONFIG_CRC32_SLICEBY8=y
# CONFIG_CRC32_SLICEBY4 is not set
# CONFIG_CRC32_SARWATE is not set
# CONFIG_CRC32_BIT is not set
CONFIG_CRC7=y
CONFIG_LIBCRC32C=y
# CONFIG_CRC8 is not set
CONFIG_ZLIB_INFLATE=y
CONFIG_ZLIB_DEFLATE=y
CONFIG_LZO_COMPRESS=y
CONFIG_LZO_DECOMPRESS=y
CONFIG_LZ4_DECOMPRESS=y
CONFIG_XZ_DEC=y
# CONFIG_XZ_DEC_X86 is not set
# CONFIG_XZ_DEC_POWERPC is not set
# CONFIG_XZ_DEC_IA64 is not set
CONFIG_XZ_DEC_ARM=y
CONFIG_XZ_DEC_ARMTHUMB=y
# CONFIG_XZ_DEC_SPARC is not set
CONFIG_XZ_DEC_BCJ=y
# CONFIG_XZ_DEC_TEST is not set
CONFIG_DECOMPRESS_GZIP=y
CONFIG_DECOMPRESS_BZIP2=y
CONFIG_DECOMPRESS_LZMA=y
CONFIG_DECOMPRESS_XZ=y
CONFIG_DECOMPRESS_LZO=y
CONFIG_DECOMPRESS_LZ4=y
CONFIG_BCH=y
CONFIG_HAS_IOMEM=y
CONFIG_HAS_IOPORT=y
CONFIG_HAS_DMA=y
CONFIG_DQL=y
CONFIG_NLATTR=y
CONFIG_ARCH_HAS_ATOMIC64_DEC_IF_POSITIVE=y
CONFIG_AVERAGE=y
CONFIG_CLZ_TAB=y
# CONFIG_CORDIC is not set
# CONFIG_DDR is not set
CONFIG_MPILIB=y
CONFIG_OID_REGISTRY=y
# CONFIG_VIRTUALIZATION is not set