Other Parts Discussed in Thread: OMAP-L138, OMAP-L137
For customer's board design, is it mandatory to pull-down the EMIFA upper address A[18:13] as below description in the EMIFA User's Guide P74? If yes, why is it unneccesary to pull-down the other address A[12:0] and A[23:19] as well? Or is it acceptable to pull-up the A[18:13]?
> The upper address inputs A[18:13] are provided by GPIO pins. The
> six GPIO pins are connected to the upper address bits of the flash
> memory and attached to pulldown resistors so that their value is 0
> six GPIO pins are connected to the upper address bits of the flash
> memory and attached to pulldown resistors so that their value is 0
> after reset and before configuring the pins as GPIO. This is necessary
> if the ROM bootloader is copying the secondary bootloader from theflash.
> if the ROM bootloader is copying the secondary bootloader from theflash.
Best Regards,
Tanaka