Hi.
I am using DM8148 with FPGA and other ASICs. And i dont want to use TPS659113 either. below are my queries
1. Is it possible to do external sequencing without that TPS659113
2.If it is possible then what is the sequence and what is the 1-1 delay to each supply
3. If i have some on board voltages like 3.3V,1.8V can it directly be used to DM8148 processor along with FPGA and other IC's
4.Is there any requirement to use separate regulators for DM8148 supplies
Thanks & Regards
Madhura