Other Parts Discussed in Thread: SYSBIOS
Dear all,
We are working on a project that we want to get rid of a old DSP platform and use the new one platform c6657.
We would like to replace the old DSP/BIOs with the new one that is included in TI/RTOS C6000_2_01_23 .
We must implement a functionality for communication between the DSP and MCSB.
In the previous implementation, this functionality was implemented using the SIO . But, this module does not exist in the current product.
We have two option:
The one is the Stream package that is supported by IPC 1.24. But this is not supported in the newest version of IPC. Is this correct?
The second one is the GIO. But it is referred that this module is deprecated in the newest bios_6_41_00_26.
What is your opinion . What is the preferable solution?
Also we notice that in SIO struct the first object is pointer to the device.
Both of GIO Stream object do not have something like this?
How can we access the Device object using GIO or SIO?
Best regards,
George