Hi,
I am creating a design with OMAP 353x using external memories and I need to have 512MB of RAM.
I have found 2GBit memory chip from Micron.
However, the internal structure of the chip is 128M x 16.
In the data sheet to the OMAP CPU (SPRUF98D–October 2009) is a table
(Table 11-63. SDRC Address Multiplexing Scheme Selection vs SDRAM
Configurations) with list of compatible memory configuration.
Unfortunately this one configuration (128x16) is not listed.
I am aware, that this type of memory is really new and therefore in
might not be listed in the mentioned table.
I need some kind of confirmation if the OMAP will work with these memory chips before I buy them and make a final deisng.
Brg,
Rado