Other Parts Discussed in Thread: TWL6030
Hi ,
I have Beagle Bone Black board planned to bring it up with linux by following the steps given in
but when I was configuring the kernel to beagle, it got following errors & warning can anyone conform why these error are coming.
here is the log of configuartion
sainath@sainath-Veriton-Series:~/BBB/kernel/kernel$ make ARCH=arm beaglebone_defconfig
HOSTCC scripts/basic/fixdep
HOSTCC scripts/kconfig/conf.o
SHIPPED scripts/kconfig/zconf.tab.c
SHIPPED scripts/kconfig/zconf.lex.c
SHIPPED scripts/kconfig/zconf.hash.c
HOSTCC scripts/kconfig/zconf.tab.o
HOSTLD scripts/kconfig/conf
drivers/video/Kconfig:60:error: recursive dependency detected!
drivers/video/Kconfig:60: symbol FB is selected by DRM_KMS_HELPER
drivers/gpu/drm/Kconfig:28: symbol DRM_KMS_HELPER is selected by DRM_TILCDC
drivers/gpu/drm/tilcdc/Kconfig:1: symbol DRM_TILCDC depends on BACKLIGHT_LCD_SUPPORT
drivers/video/backlight/Kconfig:5: symbol BACKLIGHT_LCD_SUPPORT is selected by FB_BACKLIGHT
drivers/video/Kconfig:247: symbol FB_BACKLIGHT is selected by PMAC_BACKLIGHT
drivers/macintosh/Kconfig:134: symbol PMAC_BACKLIGHT depends on FB
warning: (USB_MUSB_HDRC) selects TWL6030_USB which has unmet direct dependencies (USB_SUPPORT && (USB || USB_GADGET) && TWL4030_CORE && OMAP_USB2 && USB_MUSB_OMAP2PLUS)
warning: (DVB_USB_PCTV452E) selects TTPCI_EEPROM which has unmet direct dependencies (MEDIA_SUPPORT && MEDIA_PCI_SUPPORT && MEDIA_DIGITAL_TV_SUPPORT && I2C)
warning: (USB_MUSB_HDRC) selects TWL6030_USB which has unmet direct dependencies (USB_SUPPORT && (USB || USB_GADGET) && TWL4030_CORE && OMAP_USB2 && USB_MUSB_OMAP2PLUS)
warning: (DVB_USB_PCTV452E) selects TTPCI_EEPROM which has unmet direct dependencies (MEDIA_SUPPORT && MEDIA_PCI_SUPPORT && MEDIA_DIGITAL_TV_SUPPORT && I2C)
#
# configuration written to .config
Can anyone help me out why those warnings & error are coming.
Regards,
sainath