This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Vision SDK boot log

Hello,

We are using the Vision SDK (2.5).

We have found a problem where some of the Vps_printf() put in boot code of DSP / EVE are not seen in the boot log on UART console.

    Explanation:

We are using Prebuiilt binary provided by Vision SDK (2.5)

After the image is loaded in memory by boot loader, each core starts its execution ​one after the another. In Vision SDK code, almost on

all cores the first prints is the Firmware build time and date and then the next print is CPU Frequency related print.

         [IPU1-0]      3.634765 s:  ***** IPU1_0 Firmware build time 14:06:08 Oct 21 2014

        [IPU1-0]      3.634887 s:  *** SYSTEM: CPU Frequency <ORG = 212800000 Hz>, <NEW = 212800000 Hz>

 

These prints are captured in the boot log for IPU1-0, IPU1-1, HOST, but not captured for DSP1, DSP2, EVE1, EVE2, EVE3, EVE4 as seen in the boot log attached.

Though these prints are seen in some boot logs, but it is consistently missed for DSP1 & DSP2 cores.

We would like to understand if this issue is already known? And is there a solution to avoid such thing from happening?

Find the Log below:

Log:

 Vayu SBL Boot

AVS class-0 has been completed already
DPLL configuration completed

PRCM clock domain force wake-up completed

PRCM module enable completed

TI tda2xx evm pad configuration completed

DDR3 configuration completed

AppImage download begins

WARNING: Device Id Doesnot match

MPU CPU0 image load completed

IPU1 CPU0 image load completed

IPU1 CPU1 image load completed

DSP1 image load completed

DSP2 image load completed

EVE1 image load completed

EVE2 image load completed

EVE3 image load completed

EVE4 image load completed

SBL boot completed succesfully 

**************SBL Boot-up clock cycles*******************

PMCCNTR counts once every 64 clock cycles. To get actual CPU cycle multiple by 64

soc prcm init clock cycles - 184637

ddr3 init clock cycles - 35876

appImage load clock cycles - 37321279

slavecore bring-up clock cycles - 13983

sbl total boot-up clock cycles - 37760681

*****************************************************************

Jumping to MPU CPU0 Application...

[IPU1-0]      3.634765 s:  ***** IPU1_0 Firmware build time 14:06:08 Oct 21 2014

[IPU1-0]      3.634887 s:  *** SYSTEM: CPU Frequency <ORG = 212800000 Hz>, <NEW = 212800000 Hz>

[IPU1-0]      3.694122 s:  SYSTEM: System Common Init in progress !!!

[IPU1-0]      3.694305 s:  SYSTEM: IPC init in progress !!!

[IPU1-0]      3.694366 s:  SYSTEM: Attaching to [IPU1-1] ...

[IPU1-0]      3.694976 s:  SYSTEM: Attaching to [IPU1-1] ... SUCCESS !!!

[IPU1-0]      3.695953 s:  SYSTEM: Attaching to [DSP1] ... SUCCESS !!!

[IPU1-0]      3.696960 s:  SYSTEM: Attaching to [DSP2] ... SUCCESS !!!

[IPU1-0]      3.697937 s:  SYSTEM: Attaching to [EVE1] ... SUCCESS !!!

[IPU1-0]      3.698974 s:  SYSTEM: Attaching to [EVE2] ... SUCCESS !!!

[IPU1-0]      3.699951 s:  SYSTEM: Attaching to [EVE3] ... SUCCESS !!!

[IPU1-0]      3.700958 s:  SYSTEM: Attaching to [EVE4] ... SUCCESS !!!

[IPU1-0]      3.701995 s:  SYSTEM: Attaching to [HOST] ... SUCCESS !!!

[IPU1-0]      3.702209 s:  SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_0] ...

[IPU1-0]      3.702636 s:  SYSTEM: Creating MsgQ [IPU1-0_MSGQ] ...

[IPU1-0]      3.702819 s:  SYSTEM: Creating MsgQ [IPU1-0_ACK_MSGQ] ...

[IPU1-0]      3.704986 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...

[IPU1-0]      3.705139 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...

[IPU1-0]      3.705261 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...

[IPU1-0]      3.705352 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...

[IPU1-0]      3.705474 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...

[IPU1-0]      3.705596 s:  SYSTEM: Notify register to [EVE3] line 0, event 15...

[IPU1-0]      3.705718 s:  SYSTEM: Notify register to [EVE4] line 0, event 15...

[IPU1-0]      3.705841 s:  SYSTEM: Notify register to [HOST] line 0, event 15...

[IPU1-0]      3.706054 s:  SYSTEM: IPC init DONE !!!

[IPU1-0]      3.707336 s:  UTILS: MEM: Shared Region 0: Base = 0xa0000000 Length = 0x00d00000 (13 MB)

[IPU1-0] 3.707519 s: UTILS: MEM: Shared Region 1: Base = 0x86000000 Length = 0x10000000 (256 MB)

[IPU1-0]      3.707763 s:  UTILS: MEM: Shared Region 2: Base = 0x40400000 Length = 0x00100000 (1 MB)

[IPU1-0]      3.710021 s:  SYSTEM: System Common Init Done !!!

[IPU1-0]      3.710113 s:  SYSTEM: System Init in progress !!!

[IPU1-0]      3.710144 s:  SYSTEM: BSP Common Init in progress !!!

[IPU1-0]      3.710266 s:  SYSTEM: BSP Common Init Done !!!

[IPU1-0]      3.710327 s:  SYSTEM: BSP Platform Init in progress !!!

[IPU1-0]      3.710479 s:  SYSTEM: BSP Platform Init Done !!!

[IPU1-0]      3.710540 s:  SYSTEM: FVID2 Init in progress !!!

[IPU1-0]      3.710632 s:  SYSTEM: FVID2 Init Done !!!

[IPU1-0]      3.710662 s:  SYSTEM: VPS Init in progress !!!

[IPU1-0]      3.724029 s:  SYSTEM: VPS Init Done !!!

[IPU1-0]      3.724090 s:  SYSTEM: FVID2 Drivers Version: FVID_02_01_00_01

[IPU1-0]      3.789794 s:  UTILS: DMA: HWI Create for INT34 !!!

[IPU1-0]      3.872558 s:  SYSTEM: Initializing Links !!!

[IPU1-0]      3.872619 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024

[IPU1-0]      3.872711 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 262144 B (256 KB), Free size = 246608 B (240 KB)

[IPU1-0]      3.872863 s:  SYSTEM: Heap = SR2_OCMC             @ 0x40400000, Total size = 1048448 B (1023 KB), Free size = 1048448 B (1023 KB)

[IPU1-0]      3.873016 s:  SYSTEM: Heap = SR1_FRAME_BUF_DDR    @ 0x86000000, Total size = 268435328 B (255 MB), Free size = 264125312 B (251 MB)

[IPU1-0]      3.873199 s:  SYSTEM: Heap = SR0_DDR              @ 0xa0000000, Total size = 13628032 B (12 MB), Free size = 9152512 B (8 MB)

[IPU1-0]      3.958404 s:  SYSTEM: Initializing Links ... DONE !!!

[IPU1-0]      4.032165 s:  BOARD: Board Init in progress !!!

[IPU1-0]      4.032287 s:  BOARD: Board Init Done !!!

[IPU1-0]      4.033386 s:

[IPU1-0]      4.033416 s:  FVID2 Version         : [FVID_02_01_00_01]

[IPU1-0]      4.033477 s:  BSP Version           : [BSP_01_01_05_15]

[IPU1-0]      4.033538 s:  Platform              : [EVM]

[IPU1-0]      4.033569 s:  SOC                   : [TDA2XX]

[IPU1-0]      4.033630 s:  SOC Revision          : [ES1.1]

[IPU1-0]      4.033660 s:  Board Detected        : [Vision]

[IPU1-0]      4.039550 s:  Base Board Revision   : [REV B]

[IPU1-0]      4.039611 s:  Daughter Card Revision: [REV A]

[IPU1-0]      4.039642 s: 

[IPU1-1]      3.635070 s:  ***** IPU1_1 Firmware build time 13:53:39 Oct 21 2014

[IPU1-1]      3.635192 s:  *** SYSTEM: CPU Frequency <ORG = 212800000 Hz>, <NEW = 212800000 Hz>

[IPU1-1]      3.705963 s:  SYSTEM: System Common Init in progress !!!

[IPU1-1]      3.706176 s:  SYSTEM: IPC init in progress !!!

[IPU1-1]      3.706329 s:  SYSTEM: Attaching to [IPU1-0] ...

[IPU1-1]      3.707275 s:  SYSTEM: Attaching to [IPU1-0] ... SUCCESS !!!

[IPU1-1]      3.708282 s:  SYSTEM: Attaching to [DSP1] ... SUCCESS !!!

[IPU1-1]      3.709259 s:  SYSTEM: Attaching to [DSP2] ... SUCCESS !!!

[IPU1-1]      3.710296 s:  SYSTEM: Attaching to [EVE1] ... SUCCESS !!!

[IPU1-1]      3.711303 s:  SYSTEM: Attaching to [EVE2] ... SUCCESS !!!

[IPU1-1]      3.712310 s:  SYSTEM: Attaching to [EVE3] ... SUCCESS !!!

[IPU1-1]      3.713287 s:  SYSTEM: Attaching to [EVE4] ... SUCCESS !!!

[IPU1-1]      3.714355 s:  SYSTEM: Attaching to [HOST] ... SUCCESS !!!

[IPU1-1]      3.714569 s:  SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_1] ...

[IPU1-1]      3.715423 s:  SYSTEM: Creating MsgQ [IPU1-1_MSGQ] ...

[IPU1-1]      3.715606 s:  SYSTEM: Creating MsgQ [IPU1-1_ACK_MSGQ] ...

[IPU1-1]      3.717803 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...

[IPU1-1]      3.717987 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...

[IPU1-1]      3.718109 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...

[IPU1-1]      3.718231 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...

[IPU1-1]      3.718414 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...

[IPU1-1]      3.718597 s:  SYSTEM: Notify register to [EVE3] line 0, event 15...

[IPU1-1]      3.718719 s:  SYSTEM: Notify register to [EVE4] line 0, event 15...

[IPU1-1]      3.718811 s:  SYSTEM: Notify register to [HOST] line 0, event 15...

[IPU1-1]      3.718933 s:  SYSTEM: IPC init DONE !!!

[IPU1-1]      3.959655 s:  UTILS: MEM: Shared Region 0: Base = 0xa0000000 Length = 0x00d00000 (13 MB)

[IPU1-1]      3.959930 s:  UTILS: MEM: Shared Region 1: Base = 0x86000000 Length = 0x10000000 (256 MB)

[IPU1-1]      3.960235 s:  UTILS: MEM: Shared Region 2: Base = 0x40400000 Length = 0x00100000 (1 MB)

[IPU1-1]      3.962707 s:  SYSTEM: System Common Init Done !!!

[IPU1-1]      3.962799 s:  SYSTEM: System IPU1_1 Init in progress !!!

[IPU1-1]      3.963378 s:  UTILS: DMA: HWI Create for INT25 !!!

[IPU1-1]      3.963531 s:  SYSTEM: Initializing IPU1_1 Links !!!

[IPU1-1]      3.963592 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024

[IPU1-1]      3.963684 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 262144 B (256 KB), Free size = 227696 B (222 KB)

[IPU1-1]      4.019714 s:  SYSTEM: Initializing IPU1_1 Links ... DONE !!!

[IPU1-1]      4.019805 s:  SYSTEM: System IPU1_1 Init Done !!!

[HOST  ]      3.679687 s:  ***** A15_0 Firmware build time 14:04:44 Oct 21 2014

[HOST  ]      3.679718 s:  *** SYSTEM: CPU Frequency <ORG = 588000000 Hz>, <NEW = 750000000 Hz>

[HOST  ]      3.694244 s:  SYSTEM: System Common Init in progress !!!

[HOST  ]      3.694274 s:  SYSTEM: IPC init in progress !!!

[HOST  ]      3.694274 s:  SYSTEM: Attaching to [IPU1-0] ...

[HOST  ]      3.695251 s:  SYSTEM: Attaching to [IPU1-0] ... SUCCESS !!!

[HOST  ]      3.696228 s:  SYSTEM: Attaching to [IPU1-1] ... SUCCESS !!!

[HOST  ]      3.697235 s:  SYSTEM: Attaching to [DSP1] ... SUCCESS !!!

[HOST  ]      3.698242 s:  SYSTEM: Attaching to [DSP2] ... SUCCESS !!!

[HOST  ]      3.699249 s:  SYSTEM: Attaching to [EVE1] ... SUCCESS !!!

[HOST  ]      3.700225 s:  SYSTEM: Attaching to [EVE2] ... SUCCESS !!!

[HOST  ]      3.701232 s:  SYSTEM: Attaching to [EVE3] ... SUCCESS !!!

[HOST  ]      3.702239 s:  SYSTEM: Attaching to [EVE4] ... SUCCESS !!!

[HOST  ]      3.702270 s:  SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_2] ...

[HOST  ]      3.702301 s:  SYSTEM: Creating MsgQ [HOST_MSGQ] ...

[HOST  ]      3.702331 s:  SYSTEM: Creating MsgQ [HOST_ACK_MSGQ] ...

[HOST  ]      3.702392 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...

[HOST  ]      3.702423 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...

[HOST  ]      3.702423 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...

[HOST  ]      3.702453 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...

[HOST  ]      3.702453 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...

[HOST  ]      3.702484 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...

[HOST  ]      3.702484 s:  SYSTEM: Notify register to [EVE3] line 0, event 15...

[HOST  ]      3.702514 s:  SYSTEM: Notify register to [EVE4] line 0, event 15...

[HOST  ]      3.702514 s:  SYSTEM: IPC init DONE !!!

[HOST  ]      3.958953 s:  UTILS: MEM: Shared Region 0: Base = 0xa0000000 Length = 0x00d00000 (13 MB)

[HOST  ]      3.958984 s:  UTILS: MEM: Shared Region 1: Base = 0x86000000 Length = 0x10000000 (256 MB)

[HOST  ]      3.959014 s:  UTILS: MEM: Shared Region 2: Base = 0x40400000 Length = 0x00100000 (1 MB)

[HOST  ]      3.959075 s:  SYSTEM: System Common Init Done !!!

[HOST  ]      3.959106 s:  SYSTEM: System A15 Init in progress !!!

[HOST  ]      3.959320 s:  UTILS: DMA: HWI Create for INT66 !!!

[HOST  ]      3.959320 s:  SYSTEM: Initializing A15 Links !!!

[HOST  ]      3.959350 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024

[HOST  ]      3.959350 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 262144 B (256 KB), Free size = 249856 B (244 KB)

[HOST  ]      3.960754 s:  SYSTEM: Initializing A15 Links ... DONE !!!

[HOST  ]      3.960784 s:  SYSTEM: System A15 Init Done !!!

[DSP1  ]      3.698242 s:  SYSTEM: System Common Init in progress !!!

[DSP1  ]      3.698272 s:  SYSTEM: IPC init in progress !!!

[DSP1  ]      3.698303 s:  SYSTEM: Attaching to [IPU1-0] ...

[DSP1  ]      3.699096 s:  SYSTEM: Attaching to [IPU1-0] ... SUCCESS !!!

[DSP1  ]      3.699920 s:  SYSTEM: Attaching to [IPU1-1] ... SUCCESS !!!

[DSP1  ]      3.700744 s:  SYSTEM: Attaching to [DSP2] ... SUCCESS !!!

[DSP1  ]      3.701599 s:  SYSTEM: Attaching to [EVE1] ... SUCCESS !!!

[DSP1  ]      3.702423 s:  SYSTEM: Attaching to [EVE2] ... SUCCESS !!!

[DSP1  ]      3.703277 s:  SYSTEM: Attaching to [EVE3] ... SUCCESS !!!

[DSP1  ]      3.704101 s:  SYSTEM: Attaching to [EVE4] ... SUCCESS !!!

[DSP1  ]      3.704956 s:  SYSTEM: Attaching to [HOST] ... SUCCESS !!!

[DSP1  ]      3.704986 s:  SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_3] ...

[DSP1  ]      3.705139 s:  SYSTEM: Creating MsgQ [DSP1_MSGQ] ...

[DSP1  ]      3.705169 s:  SYSTEM: Creating MsgQ [DSP1_ACK_MSGQ] ...

[DSP1  ]      3.705322 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...

[DSP1  ]      3.705383 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...

[DSP1  ]      3.705413 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...

[DSP1  ]      3.705444 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...

[DSP1  ]      3.705474 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...

[DSP1  ]      3.705474 s:  SYSTEM: Notify register to [EVE3] line 0, event 15...

[DSP1  ]      3.705505 s:  SYSTEM: Notify register to [EVE4] line 0, event 15...

[DSP1  ]      3.705535 s:  SYSTEM: Notify register to [HOST] line 0, event 15...

[DSP1  ]      3.705566 s:  SYSTEM: IPC init DONE !!!

[DSP1  ]      3.958831 s:  UTILS: MEM: Shared Region 0: Base = 0xa0000000 Length = 0x00d00000 (13 MB)

[DSP1  ]      3.958892 s:  UTILS: MEM: Shared Region 1: Base = 0x86000000 Length = 0x10000000 (256 MB)

[DSP1  ]      3.958953 s:  UTILS: MEM: Shared Region 2: Base = 0x40400000 Length = 0x00100000 (1 MB)

[DSP1  ]      3.959136 s:  SYSTEM: System Common Init Done !!!

[DSP1  ]      3.959167 s:  SYSTEM: System DSP Init in progress !!!

[DSP1  ]      3.959381 s:  SYSTEM: Initializing DSP Links !!!

[DSP1  ]      3.959411 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024

[DSP1  ]      3.959442 s:  SYSTEM: Heap = LOCAL_L2             @ 0x00800000, Total size = 196608 B (192 KB), Free size = 196608 B (192 KB)

[DSP1  ]      3.959472 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 32768 B (32 KB), Free size = 21904 B (21 KB)

[DSP1  ]      3.965454 s:  SYSTEM: Initializing DSP Links ... DONE !!!

[DSP1  ]      3.965484 s:  SYSTEM: System DSP Init Done !!!

[DSP2  ]      3.699890 s:  SYSTEM: System Common Init in progress !!!

[DSP2  ]      3.699920 s:  SYSTEM: IPC init in progress !!!

[DSP2  ]      3.699951 s:  SYSTEM: Attaching to [IPU1-0] ...

[DSP2  ]      3.700744 s:  SYSTEM: Attaching to [IPU1-0] ... SUCCESS !!!

[DSP2  ]      3.701568 s:  SYSTEM: Attaching to [IPU1-1] ... SUCCESS !!!

[DSP2  ]      3.702392 s:  SYSTEM: Attaching to [DSP1] ... SUCCESS !!!

[DSP2  ]      3.703247 s:  SYSTEM: Attaching to [EVE1] ... SUCCESS !!!

[DSP2  ]      3.704071 s:  SYSTEM: Attaching to [EVE2] ... SUCCESS !!!

[DSP2  ]      3.704925 s:  SYSTEM: Attaching to [EVE3] ... SUCCESS !!!

[DSP2  ]      3.705749 s:  SYSTEM: Attaching to [EVE4] ... SUCCESS !!!

[DSP2  ]      3.706604 s:  SYSTEM: Attaching to [HOST] ... SUCCESS !!!

[DSP2  ]      3.706634 s:  SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_4] ...

[DSP2  ]      3.706817 s:  SYSTEM: Creating MsgQ [DSP2_MSGQ] ...

[DSP2  ]      3.706848 s:  SYSTEM: Creating MsgQ [DSP2_ACK_MSGQ] ...

[DSP2  ]      3.707031 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...

[DSP2  ]      3.707092 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...

[DSP2  ]      3.707122 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...

[DSP2  ]      3.707153 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...

[DSP2  ]      3.707183 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...

[DSP2  ]      3.707214 s:  SYSTEM: Notify register to [EVE3] line 0, event 15...

[DSP2  ]      3.707214 s:  SYSTEM: Notify register to [EVE4] line 0, event 15...

[DSP2  ]      3.707244 s:  SYSTEM: Notify register to [HOST] line 0, event 15...

[DSP2  ]      3.707275 s:  SYSTEM: IPC init DONE !!!

[DSP2  ]      3.958831 s:  UTILS: MEM: Shared Region 0: Base = 0xa0000000 Length = 0x00d00000 (13 MB)

[DSP2  ]      3.958892 s:  UTILS: MEM: Shared Region 1: Base = 0x86000000 Length = 0x10000000 (256 MB)

[DSP2  ]      3.958953 s:  UTILS: MEM: Shared Region 2: Base = 0x40400000 Length = 0x00100000 (1 MB)

[DSP2  ]      3.959136 s:  SYSTEM: System Common Init Done !!!

[DSP2  ]      3.959167 s:  SYSTEM: System DSP Init in progress !!!

[DSP2  ]      3.959381 s:  SYSTEM: Initializing DSP Links !!!

[DSP2  ]      3.959411 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024

[DSP2  ]      3.959442 s:  SYSTEM: Heap = LOCAL_L2             @ 0x00800000, Total size = 196608 B (192 KB), Free size = 196608 B (192 KB)

[DSP2  ]      3.959472 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 32768 B (32 KB), Free size = 21904 B (21 KB)

[DSP2  ]      3.965087 s:  SYSTEM: Initializing DSP Links ... DONE !!!

[DSP2  ]      3.965118 s:  SYSTEM: System DSP Init Done !!!

[EVE1  ]      3.707153 s:  SYSTEM: System Common Init in progress !!!

[EVE1  ]      3.707977 s:  SYSTEM: IPC init in progress !!!

[EVE1  ]      3.708618 s:  SYSTEM: Attaching to [IPU1-0] ...

[EVE1  ]      3.717834 s:  SYSTEM: Attaching to [IPU1-0] ... SUCCESS !!!

[EVE1  ]      3.727905 s:  SYSTEM: Attaching to [IPU1-1] ... SUCCESS !!!

[EVE1  ]      3.737915 s:  SYSTEM: Attaching to [DSP1] ... SUCCESS !!!

[EVE1  ]      3.747924 s:  SYSTEM: Attaching to [DSP2] ... SUCCESS !!!

[EVE1  ]      3.757934 s:  SYSTEM: Attaching to [EVE2] ... SUCCESS !!!

[EVE1  ]      3.767944 s:  SYSTEM: Attaching to [EVE3] ... SUCCESS !!!

[EVE1  ]      3.777954 s:  SYSTEM: Attaching to [EVE4] ... SUCCESS !!!

[EVE1  ]      3.787963 s:  SYSTEM: Attaching to [HOST] ... SUCCESS !!!

[EVE1  ]      3.789337 s:  SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_5] ...

[EVE1  ]      3.791564 s:  SYSTEM: Creating MsgQ [EVE1_MSGQ] ...

[EVE1  ]      3.792724 s:  SYSTEM: Creating MsgQ [EVE1_ACK_MSGQ] ...

[EVE1  ]      3.797210 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...

[EVE1  ]      3.798370 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...

[EVE1  ]      3.799468 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...

[EVE1  ]      3.800506 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...

[EVE1  ]      3.801574 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...

[EVE1  ]      3.802642 s:  SYSTEM: Notify register to [EVE3] line 0, event 15...

[EVE1  ]      3.803710 s:  SYSTEM: Notify register to [EVE4] line 0, event 15...

[EVE1  ]      3.804779 s:  SYSTEM: Notify register to [HOST] line 0, event 15...

[EVE1  ]      3.805816 s:  SYSTEM: IPC init DONE !!!

[EVE1  ]      3.969512 s:  UTILS: MEM: Shared Region 0: Base = 0xa0000000 Length = 0x00d00000 (13 MB)

[EVE1  ]      3.971252 s:  UTILS: MEM: Shared Region 1: Base = 0x86000000 Length = 0x10000000 (256 MB)

[EVE1  ]      3.973266 s:  UTILS: MEM: Shared Region 2: Base = 0x40400000 Length = 0x00100000 (1 MB)

[EVE1  ]      3.977569 s:  SYSTEM: System Common Init Done !!!

[EVE1  ]      3.978332 s:  SYSTEM: System EVE Init in progress !!!

[EVE1  ]      3.979827 s:  UTILS: DMA: HWI Create for INT8 !!!

[EVE1  ]      3.980865 s:  SYSTEM: Initializing EVE Links !!!

[EVE1  ]      3.981567 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024

[EVE1  ]      3.982604 s:  SYSTEM: Heap = LOCAL_L2             @ 0x40020000, Total size = 25600 B (25 KB), Free size = 25600 B (25 KB)

[EVE1  ]      3.984649 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 16384 B (16 KB), Free size = 5416 B (5 KB)

[EVE1  ]      4.030578 s:  SYSTEM: Initializing EVE Links ... DONE !!!

[EVE1  ]      4.031219 s:  SYSTEM: System EVE Init Done !!!

[EVE2  ]      3.710906 s:  SYSTEM: System Common Init in progress !!!

[EVE2  ]      3.711730 s:  SYSTEM: IPC init in progress !!!

[EVE2  ]      3.712371 s:  SYSTEM: Attaching to [IPU1-0] ...

[EVE2  ]      3.718261 s:  SYSTEM: Attaching to [IPU1-0] ... SUCCESS !!!

[EVE2  ]      3.728302 s:  SYSTEM: Attaching to [IPU1-1] ... SUCCESS !!!

[EVE2  ]      3.738311 s:  SYSTEM: Attaching to [DSP1] ... SUCCESS !!!

[EVE2  ]      3.748291 s:  SYSTEM: Attaching to [DSP2] ... SUCCESS !!!

[EVE2  ]      3.758300 s:  SYSTEM: Attaching to [EVE1] ... SUCCESS !!!

[EVE2  ]      3.768310 s:  SYSTEM: Attaching to [EVE3] ... SUCCESS !!!

[EVE2  ]      3.778320 s:  SYSTEM: Attaching to [EVE4] ... SUCCESS !!!

[EVE2  ]      3.788330 s:  SYSTEM: Attaching to [HOST] ... SUCCESS !!!

[EVE2  ]      3.789428 s:  SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_6] ...

[EVE2  ]      3.791625 s:  SYSTEM: Creating MsgQ [EVE2_MSGQ] ...

[EVE2  ]      3.792816 s:  SYSTEM: Creating MsgQ [EVE2_ACK_MSGQ] ...

[EVE2  ]      3.797393 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...

[EVE2  ]      3.798553 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...

[EVE2  ]      3.799652 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...

[EVE2  ]      3.800689 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...

[EVE2  ]      3.801757 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...

[EVE2  ]      3.802825 s:  SYSTEM: Notify register to [EVE3] line 0, event 15...

[EVE2  ]      3.803894 s:  SYSTEM: Notify register to [EVE4] line 0, event 15...

[EVE2  ]      3.804962 s:  SYSTEM: Notify register to [HOST] line 0, event 15...

[EVE2  ]      3.806030 s:  SYSTEM: IPC init DONE !!!

[EVE2  ]      3.969146 s:  UTILS: MEM: Shared Region 0: Base = 0xa0000000 Length = 0x00d00000 (13 MB)

[EVE2  ]      3.970855 s:  UTILS: MEM: Shared Region 1: Base = 0x86000000 Length = 0x10000000 (256 MB)

[EVE2  ]      3.972900 s:  UTILS: MEM: Shared Region 2: Base = 0x40400000 Length = 0x00100000 (1 MB)

[EVE2  ]      3.977142 s:  SYSTEM: System Common Init Done !!!

[EVE2  ]      3.977844 s:  SYSTEM: System EVE Init in progress !!!

[EVE2  ]      3.979370 s:  UTILS: DMA: HWI Create for INT8 !!!

[EVE2  ]      3.980438 s:  SYSTEM: Initializing EVE Links !!!

[EVE2  ]      3.981140 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024

[EVE2  ]      3.982177 s:  SYSTEM: Heap = LOCAL_L2             @ 0x40020000, Total size = 25600 B (25 KB), Free size = 25600 B (25 KB)

[EVE2  ]      3.984252 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 16384 B (16 KB), Free size = 5416 B (5 KB)

[EVE2  ]      4.029968 s:  SYSTEM: Initializing EVE Links ... DONE !!!

[EVE2  ]      4.030639 s:  SYSTEM: System EVE Init Done !!!

[EVE3  ]      3.715515 s:  SYSTEM: System Common Init in progress !!!

[EVE3  ]      3.716461 s:  SYSTEM: IPC init in progress !!!

[EVE3  ]      3.717163 s:  SYSTEM: Attaching to [IPU1-0] ...

[EVE3  ]      3.718139 s:  SYSTEM: Attaching to [IPU1-0] ... SUCCESS !!!

[EVE3  ]      3.728179 s:  SYSTEM: Attaching to [IPU1-1] ... SUCCESS !!!

[EVE3  ]      3.738189 s:  SYSTEM: Attaching to [DSP1] ... SUCCESS !!!

[EVE3  ]      3.748199 s:  SYSTEM: Attaching to [DSP2] ... SUCCESS !!!

[EVE3  ]      3.758209 s:  SYSTEM: Attaching to [EVE1] ... SUCCESS !!!

[EVE3  ]      3.768218 s:  SYSTEM: Attaching to [EVE2] ... SUCCESS !!!

[EVE3  ]      3.778228 s:  SYSTEM: Attaching to [EVE4] ... SUCCESS !!!

[EVE3  ]      3.788208 s:  SYSTEM: Attaching to [HOST] ... SUCCESS !!!

[EVE3  ]      3.789550 s:  SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_7] ...

[EVE3  ]      3.791717 s:  SYSTEM: Creating MsgQ [EVE3_MSGQ] ...

[EVE3  ]      3.792877 s:  SYSTEM: Creating MsgQ [EVE3_ACK_MSGQ] ...

[EVE3  ]      3.797363 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...

[EVE3  ]      3.798522 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...

[EVE3  ]      3.799621 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...

[EVE3  ]      3.800659 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...

[EVE3  ]      3.801727 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...

[EVE3  ]      3.802795 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...

[EVE3  ]      3.803863 s:  SYSTEM: Notify register to [EVE4] line 0, event 15...

[EVE3  ]      3.804901 s:  SYSTEM: Notify register to [HOST] line 0, event 15...

[EVE3  ]      3.805969 s:  SYSTEM: IPC init DONE !!!

[EVE3  ]      3.969512 s:  UTILS: MEM: Shared Region 0: Base = 0xa0000000 Length = 0x00d00000 (13 MB)

[EVE3  ]      3.971221 s:  UTILS: MEM: Shared Region 1: Base = 0x86000000 Length = 0x10000000 (256 MB)

[EVE3  ]      3.973236 s:  UTILS: MEM: Shared Region 2: Base = 0x40400000 Length = 0x00100000 (1 MB)

[EVE3  ]      3.977508 s:  SYSTEM: System Common Init Done !!!

[EVE3  ]      3.978240 s:  SYSTEM: System EVE Init in progress !!!

[EVE3  ]      3.979766 s:  UTILS: DMA: HWI Create for INT8 !!!

[EVE3  ]      3.980804 s:  SYSTEM: Initializing EVE Links !!!

[EVE3  ]      3.981475 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024

[EVE3  ]      3.982513 s:  SYSTEM: Heap = LOCAL_L2             @ 0x40020000, Total size = 25600 B (25 KB), Free size = 25600 B (25 KB)

[EVE3  ]      3.984558 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 16384 B (16 KB), Free size = 5416 B (5 KB)

[EVE3  ]      4.030273 s:  SYSTEM: Initializing EVE Links ... DONE !!!

[EVE3  ]      4.030914 s:  SYSTEM: System EVE Init Done !!!

[EVE4  ]      3.715454 s:  SYSTEM: System Common Init in progress !!!

[EVE4  ]      3.716369 s:  SYSTEM: IPC init in progress !!!

[EVE4  ]      3.717041 s:  SYSTEM: Attaching to [IPU1-0] ...

[EVE4  ]      3.718261 s:  SYSTEM: Attaching to [IPU1-0] ... SUCCESS !!!

[EVE4  ]      3.728302 s:  SYSTEM: Attaching to [IPU1-1] ... SUCCESS !!!

[EVE4  ]      3.738281 s:  SYSTEM: Attaching to [DSP1] ... SUCCESS !!!

[EVE4  ]      3.748291 s:  SYSTEM: Attaching to [DSP2] ... SUCCESS !!!

[EVE4  ]      3.758300 s:  SYSTEM: Attaching to [EVE1] ... SUCCESS !!!

[EVE4  ]      3.768310 s:  SYSTEM: Attaching to [EVE2] ... SUCCESS !!!

[EVE4  ]      3.778320 s:  SYSTEM: Attaching to [EVE3] ... SUCCESS !!!

[EVE4  ]      3.788330 s:  SYSTEM: Attaching to [HOST] ... SUCCESS !!!

[EVE4  ]      3.789428 s:  SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_8] ...

[EVE4  ]      3.791595 s:  SYSTEM: Creating MsgQ [EVE4_MSGQ] ...

[EVE4  ]      3.792785 s:  SYSTEM: Creating MsgQ [EVE4_ACK_MSGQ] ...

[EVE4  ]      3.797363 s:  SYSTEM: Notify register to [IPU1-0] line 0, event 15...

[EVE4  ]      3.798522 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...

[EVE4  ]      3.799621 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...

[EVE4  ]      3.800659 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...

[EVE4  ]      3.801727 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...

[EVE4  ]      3.802795 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...

[EVE4  ]      3.803863 s:  SYSTEM: Notify register to [EVE3] line 0, event 15...

[EVE4  ]      3.804931 s:  SYSTEM: Notify register to [HOST] line 0, event 15...

[EVE4  ]      3.805969 s:  SYSTEM: IPC init DONE !!!

[EVE4  ]      3.969146 s:  UTILS: MEM: Shared Region 0: Base = 0xa0000000 Length = 0x00d00000 (13 MB)

[EVE4  ]      3.970855 s:  UTILS: MEM: Shared Region 1: Base = 0x86000000 Length = 0x10000000 (256 MB)

[EVE4  ]      3.972900 s:  UTILS: MEM: Shared Region 2: Base = 0x40400000 Length = 0x00100000 (1 MB)

[EVE4  ]      3.977142 s:  SYSTEM: System Common Init Done !!!

[EVE4  ]      3.977813 s:  SYSTEM: System EVE Init in progress !!!

[EVE4  ]      3.979370 s:  UTILS: DMA: HWI Create for INT8 !!!

[EVE4  ]      3.980438 s:  SYSTEM: Initializing EVE Links !!!

[EVE4  ]      3.981109 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024

[EVE4  ]      3.982147 s:  SYSTEM: Heap = LOCAL_L2             @ 0x40020000, Total size = 25600 B (25 KB), Free size = 25600 B (25 KB)

[EVE4  ]      3.984191 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 16384 B (16 KB), Free size = 5416 B (5 KB)

[EVE4  ]      4.029815 s:  SYSTEM: Initializing EVE Links ... DONE !!!

[EVE4  ]      4.030456 s:  SYSTEM: System EVE Init Done !!!

[IPU1-0]      5.041473 s:  QSPI Init Started

[IPU1-0]      5.041625 s:  MID - 1

[IPU1-0]      5.041656 s:  DID - 18

[IPU1-0]      5.041839 s:  QSPI Init Completed Sucessfully

[IPU1-0]      5.041900 s:  DMM_PEG_PRIO_4 (0x4e000630) = 0x44444440

[IPU1-0]      5.042022 s:  SYSTEM: Opening MsgQ [IPU1-1_MSGQ] ...

[IPU1-0]      5.043304 s: 

[IPU1-0]      5.043365 s:  Current System Settings,

[IPU1-0]      5.043426 s:  ========================

[IPU1-0]      5.043457 s:  Display Type   : HDMI 1920x1080 @ 60fps

[IPU1-0]      5.043518 s:  Capture Source : Sensor OV10635 1280x720  @ 30fps

[IPU1-0]      5.043548 s:  My IP address  : 0.0.0.0

[IPU1-0]      5.043609 s: 

[IPU1-0]      5.043640 s:  ============

[IPU1-0]      5.043670 s:  Usecase Menu

[IPU1-0]      5.043731 s:  ============

[IPU1-0]      5.043762 s:

[IPU1-0] 

[IPU1-0]  Single Camera Use-cases,

[IPU1-0]  ------------------------

[IPU1-0]  1: 1CH VIP  capture + Display

[IPU1-0]  2: 1CH VIP  capture + Alg Frame Copy (DSP1)     + Display

[IPU1-0]  3: 1CH VIP  capture + Alg Frame Copy (EVE1)     + Display

[IPU1-0]  4: 1CH VIP  capture + Alg Frame Copy (A15)      + Display

[IPU1-0]  5: 1CH VIP  capture + Edge Detect (EVE1)        + Display

[IPU1-0]  6: 1CH VIP  capture + Dense Optical Flow (EVEx) + HDMI Display

[IPU1-0]  7: 1CH VIP  capture + Pedestrain Detect (EVE1 + DSP1) + Display

[IPU1-0]  8: 1Ch VIP  capture + Sparse Optical Flow (EVE1) + Display

[IPU1-0]  9: 1CH VIP  capture + Alg Subframe Copy (EVE1) + Display

[IPU1-0] 

[IPU1-0]  Multi-Camera LVDS Use-cases,

[IPU1-0]  ----------------------------

[IPU1-0]  a: 4CH LVDS VIP Capture + VPE + Sync + Alg DMA SW Mosaic (IPU1-0) + Display

[IPU1-0]  b: 5CH LVDS VIP Capture + Surround View (DSPx) + Edge Detect (EVE1) + HDMI Display

[IPU1-0]  c: 5CH LVDS VIP Capture + Surround View (DSPx) + DOF (EVE1) + HDMI Display

[IPU1-0] 

[IPU1-0]  AVB RX Use-cases,

[IPU1-0]  -----------------

[IPU1-0]  d: 4CH AVB Capture + Decode + VPE + Sync + Alg DMA SW Mosaic (IPU1-0) + Display

[IPU1-0]  e: 5CH AVB Capture + Surround View (DSPx) + Edge Detect (EVE1) + HDMI Display

[IPU1-0] 

[IPU1-0]  Dual Display Use-cases,

[IPU1-0]  -----------------------

[IPU1-0]  f: 1CH VIP  capture + Edge Detect (EVE1) + Dual Display

[IPU1-0] 

[IPU1-0]  s: System Settings

[IPU1-0] 

[IPU1-0]  x: Exit

[IPU1-0] 

[IPU1-0]  Enter Choice:

[IPU1-0] 

 

 

Please provide some info. on this.

 

Regards,

Swapnil Nagare

  • Hello Swapnil,

    I note you that - Remote log feature with ability to print logs from all CPUs to UART controlled by IPU1-0

    Remote log client task (on IPU1-0 only): This task looks at the shared remote log buffer and outputs any strings to UART terminal. Normally during run-time prints are not done hence this task does not appear in the task load log.

    I checked if these log messages are disabled for EVEs and DSPs modules. However these messages are enabled.
    For example, you can see in vision_sdk/src/main_app/tda2xx/eve1/src/ main_eve1.c

    /* This should the first call for initializing the remote debug server
    */
    RemoteLog_init();
    Vps_printf(" ***** EVE1 Firmware build time %s %s \n",
    __TIME__,__DATE__);

    I will forward your questions to Vision SDK experts.

    Best regards,
    Yanko
  • Hello Swapnil,

    I got the confirmation about your question.

    In conclusion, this is a limitation of Vision SDK, This is because it’s CORTEX M4 who set the RemoteLog_init(), so any prints before this point is getting missed. All prints after this point will get printed correctly though.

    Best regards,

    Yanko

  • Hello Yanko,

    Thanks for the reply.

    One quick question.Can we avoid this scenario by adding a start up delay for the DSP Core so that M4 gets initialized and we could get the prints?

    Will this work?

     

    Thanks,

    Swapnil Nagare

     

  • Hello Swapnil,

    I assume that it won't work. Because, adding a start up delay for DSP core is in contradiction with Jacinto's initialization sequence.

    However, you can test this idea.

    Best regards,
    Yanko