This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138 Support

I am trying to test the L138 EVM and ran into a few problems.  I ordered the experimenter’s kit and a 6.4” VGA display kit.  Both arrived and I was able to install the ARM tools, boot from FLASH and boot from TFTP/NFS.  When I try to connect the display I find no documentation that connects the display module to the experimenter’s board.  I read through schematics to see how the connector should be installed and tried it.  The board did not fry, it came up looking like u-boot was driving QVGA to my VGA screen.  As the kernel boots it changes video settings and loses sync…

LogicPD said this was a good question for TI…what have you got for me?  How do I set up my video modes to get this display to work?  Can I use fbset, bootargs or something else to set this up?