Hi All,
I am using IPNC_RDK_3.8 with DM8127 based custom board. Currently, I am running "low power TRI_STREAM usecase". With this usecase, I am able to get encoded frames.
[m3video] ==================== EncLink_PrintDetails ====================
[m3video] 56043: HDVICP-ID:0
[m3video] totalAcquire2wait in msec: 830
[m3video] totalWait2Isr in msec: 12955
[m3video] totalIsr2Done in msec: 82
[m3video] totalWait2Done in msec: 13037
[m3video] totalDone2Release in msec: 0
[m3video] totalAcquire2Release in msec: 14127
[m3video] totalAcq2acqDelay in msec: 36252
[m3video] totalElapsedTime in msec: 50354
[m3video] numAccessCnt: 3261
[m3video] IVA-FPS : 65
[m3video]
[m3video] *** ENCODE Statistics ***
[m3video]
[m3video] Elasped Time : 49 secs
[m3video]
[m3video]
[m3video] CH | In Recv In Skip In User Out Latency
[m3video] Num | FPS FPS Skip FPS FPS Min / Max
[m3video] --------------------------------------------
[m3video] 0 | 30 0 0 30.20 13 / 17
[m3video] 1 | 30 0 0 30.39 11 / 20
[m3video] 2 | 30 0 25 5.08 20 / 24
[m3video]
[m3video] Multi Channel Encode Average Submit Batch Size
[m3video] Max Submit Batch Size : 24
[m3video] IVAHD_0 Average Batch Size : 1
[m3video] IVAHD_0 Max achieved Batch Size : 1
[m3video] ==============================================================
But my streaming is not working. When wis-streamer starts, it gives following error,
Error: Memory return Invalid, from function share_memory_init in file ./network/live/appro/wis-streamer.cpp.
Due to this error, wis-streamer is not starting.
I have not changed any default initialization. Still I am getting invalid memory pointer.
I am using following Boot arguments.
console=ttyO0,115200n8 rootdelay=2 mem=80M vram=4M root=/dev/nfs notifyk.vpssm3_sva=0xBFD00000 nfsroot=10.103.0.117:/home/krinali/Gen3Zooter/Source_Package/Current/Source/ipnc_rdk/target/filesys,nolock rw ip=dhcp cmemk.phys_start=0x85000000 cmemk.phys_end=0x89000000 cmemk.allowOverlap=1 earlyprintk
please suggest some solution to resolve this issue.
Thanks,
Krinali Shah