Other Parts Discussed in Thread: PMP
After uImage was loaded,problems occured in the process of file-system booting,the message-lags are like this:
Waiting for root device /dev/mmcblk0p2...
mmc0: new high speed SDHC card at address e624
mmcblk0: mmc0:e624 SD08G 7.40 GiB (ro)
mmcblk0: p1 p2 p3
VFS: Cannot open root device "mmcblk0p2" or unknown-block(179,2)
Please append a correct "root=" boot option; here are the available partitions:
1f00 64 mtdblock0 (driver?)
1f02 64 mtdblock2 (driver?)
1f04 2432 mtdblock4 (driver?)
1f05 128 mtdblock5 (driver?)
1f06 4352 mtdblock6 (driver?)
1f07 204928 mtdblock7 (driver?)
1f08 50304 mtdblock8 (driver?)
b300 7761920 mmcblk0 driver: mmcblk
b301 40131 mmcblk0p1 00000000-0000-0000-0000-000000000mmcblk0p1
b302 883575 mmcblk0p2 00000000-0000-0000-0000-000000000mmcblk0p2
b303 6835657 mmcblk0p3 00000000-0000-0000-0000-000000000mmcblk0p3
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)
Backtrace:
[<c0043b44>] (dump_backtrace+0x0/0x110) from [<c0353b74>] (dump_stack+0x18/0x1c)
r7:cc812000 r6:00000000 r5:c002b71c r4:c04b98d0
[<c0353b5c>] (dump_stack+0x0/0x1c) from [<c0353bd8>] (panic+0x60/0x17c)
[<c0353b78>] (panic+0x0/0x17c) from [<c0009254>] (mount_block_root+0x1e0/0x220)
r3:00000000 r2:00000000 r1:cc82bf58 r0:c040632c
[<c0009074>] (mount_block_root+0x0/0x220) from [<c0009340>] (mount_root+0xac/0xcc)
[<c0009294>] (mount_root+0x0/0xcc) from [<c00094d0>] (prepare_namespace+0x170/0x1d4)
r4:c04b9264
[<c0009360>] (prepare_namespace+0x0/0x1d4) from [<c0008784>] (kernel_init+0x114/0x154)
r5:c0008670 r4:c04b9200
[<c0008670>] (kernel_init+0x0/0x154) from [<c0063ae0>] (do_exit+0x0/0x5e4)
r5:c0008670 r4:00000000
My software environments are based on Vmware and Ubuntu linux, and the dm8168-board parameters are set as following:
verify=yes
ethact=DaVinci EMAC
baudrate=115200
filesize=240B20
netmask=255.255.255.0
gatewayip=192.168.1.1
ipaddr=192.168.1.100
nfsserver=192.168.1.108
serverip=192.168.1.108
hostname=zb205-desktop
ethaddr=00:0C:29:4A:95:8B
nfsvers=nfs3
bootargs=console=ttyO2,115200n8 rootwait root=/dev/mmcblk0p2 rw mem=256M earlyprink vram=50M ti816xfb.vram=0:16M,1:16M,2:6M ip=off noinitrd
bootcmd=mmc init 0;fatload mmc 0 0x81000000 uImage;bootm 0x81000000
stdin=serial
stdout=serial
stderr=serial
ver=U-Boot 2010.06 (Jun 01 2011 - 12:30:57)
I checked my setenv, but can't figured out what's wrong with that ,or does there any problems that I haven't noticed yet?
Please help me out these! Thanks a lot !