Hi ,
I want to set static ip to our ti8148evm board.But I'm not sure how to set.
Is it in the \etc\network\interfaces ?
Would you tell me how to do ?
Thank you very much.
BR
Bob
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Bob,
bob lee said:But I find sometimes the ip in linux is not the ip I have set.
Make sure your boot arguments are not overwriting your static ip setings.
BR
Pavel
Hi Pavel,
I just want to know if we can set the static ip in arago-base-tisdk-image-dm814x-evm.
I have set the ipaddr in the uboot,but the ip in linux isn't same as in uboot.
Is it related to the udhcpc?If so ,how to disable it in arago-base-tisdk-image-dm814x-evm?
BR
Bob
yes,
you may try like this,
vi /etc/network/interfaces
#Wired or wireless interfaces
auto eth0
#iface eth0 inet dhcp
# pre-up /bin/grep -v -e "ip=[0-9]\+\.[0-9]\+\.[0-9]\+\.[0-9]\+" /proc/cm
iface eth0 inet static
address 192.168.254.184
netmask 255.255.255.0
gateway 192.168.254.1
auto eth1
#iface eth1 inet dhcp
iface eth1 inet static
address 192.168.253.183
netmask 255.255.255.0
gateway 192.168.253.1
Bob,
bob lee said:I just want to know if we can set the static ip in arago-base-tisdk-image-dm814x-evm.
I have set the ipaddr in the uboot,but the ip in linux isn't same as in uboot.
Is it related to the udhcpc?If so ,how to disable it in arago-base-tisdk-image-dm814x-evm?
When I set static ip in u-boot and boot arguments, this static ip is not changed nor in linux kernel neither in root filesystem, and I end up with this static up unchanged.
TI8148_EVM#setenv ipaddr 172.20.0.127
TI8148_EVM#setenv bootargs 'console=ttyO0,115200n8 root=/dev/nfs nfsroot=172.20.1.195:/home/users/pbotev/targetfs,nolock rw mem=364M@0x80000000 mem=320M@0x9FC00000 vmalloc=500M notifyk.vpssm3_sva=0xBF900000 ip=172.20.0.127 noinitrd'
Starting kernel ...
Kernel command line: console=ttyO0,115200n8 root=/dev/nfs nfsroot=172.20.1.195:/home/users/pbotev/targetfs,nolock rw mem=364M@0x80000000 mem=320M@0x9FC00000 vmalloc=500M notifyk.vpssm3_sva=0xBF900000 ip=172.20.0.127 noinitrd
IP-Config: Guessing netmask 255.255.0.0
IP-Config: Complete:
device=eth0, addr=172.20.0.127, mask=255.255.0.0, gw=255.255.255.255,
host=172.20.0.127, domain=, nis-domain=(none),
bootserver=255.255.255.255, rootserver=172.20.1.195, rootpath=
dm814x-evm login: root
root@dm814x-evm:~# ifconfig
eth0 Link encap:Ethernet HWaddr 90:D7:EB:D5:13:96
inet addr:172.20.0.127 Bcast:172.20.255.255 Mask:255.255.0.0
UP BROADCAST RUNNING ALLMULTI MULTICAST MTU:1500 Metric:1
RX packets:44373 errors:0 dropped:212 overruns:0 frame:0
TX packets:25775 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:58319021 (55.6 MiB) TX bytes:2514040 (2.3 MiB)
Interrupt:40
Regards,
Pavel
Hi Pavel,
I have set static ip in interfaces ,but it always shows the message as below before login linux.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dm814x-evm ttyO0
Arago 2011.09 dm814x-evm ttyO0
dm814x-evm login: PHY: 0:01 - Link is Up - 100/Full
PHY: 0:02 - Link is Up - 0/Half
PHY: 0:02 - Link is Down
Do you tell me how to change the code to disable it to show the message as below?
PHY: 0:01 - Link is Up - 100/FullPHY: 0:02 - Link is Up - 0/Half
PHY: 0:02 - Link is Down
Thank you
BR
Bob
Bob,
bob lee said:Do you tell me how to change the code to disable it to show the message as below?
PHY: 0:01 - Link is Up - 100/FullPHY: 0:02 - Link is Up - 0/Half
PHY: 0:02 - Link is Down
I think these messages come from the linux kernel, not from the root filesystem. Could you please provide me all your steps in u-boot and all the boot log (not just part of it)?
BR
Pavel
Hi Pavel,
Here is the boot up message.
U-Boot 2010.06 (Jun 06 2014 - 11:54:38)
TI8148-GP rev 3.0
ARM clk: 600MHz
DDR clk: 400MHz
DRAM: 2 GiB
NAND: HW ECC BCH8 Selected
256 MiB
*** Warning - bad CRC or NAND, using default environment
The 2nd stage U-Boot will now be auto-loaded
Please do not interrupt the countdown till TI8148_EVM prompt if 2nd stage is already flashed
Net: <ethaddr> not set. Reading from E-fuse
Detected MACID:84:7e:40:e9:c9:36
cpsw
Hit any key to stop autoboot: 0
NAND read: device 0 offset 0x20000, size 0x40000
262144 bytes read: OK
## Starting application at 0x81000000 ...
U-Boot 2010.06 (Jun 06 2014 - 11:55:10)
TI8148-GP rev 3.0
ARM clk: 600MHz
DDR clk: 400MHz
I2C: ready
DRAM: 2 GiB
NAND: HW ECC BCH8 Selected
256 MiB
MMC: OMAP SD/MMC: 0
.:;rrr;;.
,5#@@@@#####@@@@@@#2,
,A@@@hi;;;r5;;;;r;rrSG@@@A,
r@@#i;:;s222hG;rrsrrrrrr;ri#@@r
:@@hr:r;SG3ssrr2r;rrsrsrsrsrr;rh@@:
B@H;;rr;3Hs;rrr;sr;;rrsrsrsrsrsr;;H@B
@@s:rrs;5#;;rrrr;r#@H:;;rrsrsrsrsrr:s@@
@@;;srs&X#9;r;r;;,2@@@rrr:;;rrsrsrsrr;;@@
@@;;rrsrrs@MB#@@@@@###@@@@@@#rsrsrsrsrr;;@@
G@r;rrsrsr;#X;SX25Ss#@@#M@#9H9rrsrsrsrsrs;r@G
@9:srsrsrs;2@;:;;:.X@@@@@H::;rrsrsrsrsrsrr:3@
X@;rrsrsrsrr;XAi;;:&@@#@Bs:rrsrsrsrsrsrsrsrr;@X
@#;rsrsrsrsrr;r2ir@@@###::rrsrsrsrsrsrsrsrsr:@@
@A:rrsrsrsrr;:2@29@@M@@@;:;rrrrsrsrsrsrsrsrs;H@
@&;rsrsrsrr;A@@@@@@###@@@s::;:;;rrsrsrsrsrsr;G@
@#:rrsrsrsr;G@5Hr25@@@#@@@#9XG9s:rrrrsrsrsrs:#@
M@;rsrsrsrs;r@&#;::S@@@@@@@M@@@@Grr:;rsrsrsr;@#
:@s;rsrsrsrr:M#Msrr;;&#@@@@@@@@@@H@@5;rsrsr;s@,
@@:rrsrsrsr;S@rrrsr;:;r3MH@@#@M5,S@@irrsrr:@@
@A:rrsrsrsrrrrrsrsrrr;::;@##@r:;rH@h;srr:H@
;@9:rrsrsrsrrrsrsrsrsr;,S@Hi@i:;s;MX;rr:h@;
r@B:rrrrsrsrsrsrsrr;;sA@#i,i@h;r;S5;r:H@r
,@@r;rrrsrsrsrsrr;2BM3r:;r:G@:rrr;;r@@,
B@Mr;rrrrsrsrsr@@S;;;rrr:5M;rr;rM@H
.@@@i;;rrrrsrs2i;rrrrr;r@M:;i@@@.
.A@@#5r;;;r;;;rrr;r:r#AsM@@H.
;&@@@@MhXS5i5SX9B@@@@G;
:ihM#@@@@@##hs,
Net: Detected MACID:84:7e:40:e9:c9:36
cpsw
Hit any key to stop autoboot: 0
NAND read: device 0 offset 0x280000, size 0x600000
Skipping bad block 0x00280000
Skipping bad block 0x002a0000
Skipping bad block 0x002c0000
Skipping bad block 0x002e0000
Skipping bad block 0x00300000
Skipping bad block 0x00320000
Skipping bad block 0x00340000
Skipping bad block 0x00360000
Skipping bad block 0x00420000
Skipping bad block 0x004c0000
Skipping bad block 0x005a0000
6291456 bytes read: OK
NAND read: device 0 offset 0x880000, size 0x1400000
20971520 bytes read: OK
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Linux-2.6.37+
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2749100 Bytes = 2.6 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37+ (boblee@javenshen-desktop) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #98 Tue Jan 27 15:09:33 CST 2015
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8148evm
bootconsole [earlycon0] enabled
reserved size = 52428800 at 0x0
FB: Reserving 52428800 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8148 3.0
SRAM: Mapped pa 0x402f1000 to va 0xfe400000 size: 0xf000
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 52224
Kernel command line: mem=256M console=ttyO0,115200n8 earlyprintk root=/dev/ram rw initrd=0x82000000,32MB
PID hash table entries: 1024 (order: 0, 4096 bytes)
Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
Memory: 206MB = 206MB total
Memory: 170024k/170024k available, 92120k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xd0800000 - 0xf8000000 ( 632 MB)
lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.init : 0xc0008000 - 0xc003c000 ( 208 kB)
.text : 0xc003c000 - 0xc0532000 (5080 kB)
.data : 0xc0532000 - 0xc057a7c0 ( 290 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:375
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQ368
Trying to install interrupt handler for IRQ369
Trying to install interrupt handler for IRQ370
Trying to install interrupt handler for IRQ371
Trying to install interrupt handler for IRQ372
Trying to install interrupt handler for IRQ373
Trying to install interrupt handler for IRQ374
Trying to install type control for IRQ375
Trying to set irq flags for IRQ375
OMAP clockevent source: GPTIMER1 at 20000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 598.01 BogoMIPS (lpj=2990080)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
omap_voltage_early_init: voltage driver support not added
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!
omap_voltage_add_dev: VDD specified does not exist!
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
omap_mux_init: Add partition: #1: core, flags: 4
NOR: Can't request GPMC CS
_omap_mux_get_by_name: Could not find signal gpio1_08_mux1
_omap_mux_get_by_name: Could not find signal gpio1_10_mux1
Debugfs: Only enabling/disabling deep sleep and wakeup timer is supported now
registered ti81xx_vpss device
registered ti81xx_vidout device
registered ti81xx_fb device
registered ti81xx_vin device
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
USBSS revision 4ea2080b
registerd cppi-dma Intr @ IRQ 17
Cppi41 Init Done
omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
tps65910 1-002d: read from reg 3f failed
tps65910 1-002d: read from reg 1e failed
set_machine_constraints: failed to enable VRTC
tps65910 1-002d: failed to register tps65910-pmic regulator
tps65910-pmic: probe of tps65910-pmic failed with error -121
tps65910 1-002d: No interrupt support, no core IRQ
omap_i2c omap_i2c.3: bus 3 rev4.0 at 400 kHz
omap_i2c omap_i2c.4: bus 4 rev4.0 at 100 kHz
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
musb-hdrc: version 6.0, host, debug=0
musb-hdrc musb-hdrc.0: dma type: dma-cppi41
MUSB controller-0 revision 4ea20800
musb-hdrc musb-hdrc.0: MUSB HDRC host driver
musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 2.6.37+ musb-hcd
usb usb1: SerialNumber: musb-hdrc.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb-hdrc musb-hdrc.0: USB Host mode controller at d081e000 using DMA, IRQ 18
musb-hdrc musb-hdrc.1: dma type: dma-cppi41
MUSB controller-1 revision 4ea20800
musb-hdrc musb-hdrc.1: MUSB HDRC host driver
musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: MUSB HDRC host driver
usb usb2: Manufacturer: Linux 2.6.37+ musb-hcd
usb usb2: SerialNumber: musb-hdrc.1
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
musb-hdrc musb-hdrc.1: USB Host mode controller at d0828800 using DMA, IRQ 19
NET: Registered protocol family 2
IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (no cpio magic); looks like an initrd
Freeing initrd memory: 32768K
NetWinder Floating Point Emulator V0.97 (double precision)
PMU: registered new PMU device of type 0
omap-iommu omap-iommu.0: ducati registered
omap-iommu omap-iommu.1: sys registered
JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
msgmni has been set to 396
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
console [ttyO0] enabled, bootconsole disabled
console [ttyO0] enabled, bootconsole disabled
omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
brd: module loaded
loop: module loaded
ahci ahci.0: forcing PORTS_IMPL to 0x1
ahci ahci.0: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc apst
scsi0 : ahci_platform
ata1: SATA max UDMA/133 irq_stat 0x00400040, connection status changed irq 16
omap2-nand driver initializing
NAND device: Manufacturer ID: 0xec, Chip ID: 0xda (Samsung )
Creating 7 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000020000 : "U-Boot-min"
0x000000020000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x000000880000 : "Kernel"
0x000000880000-0x000001c80000 : "ramdisk"
0x000001c80000-0x000004480000 : "yaffs2"
0x000004480000-0x000010000000 : "Reserved"
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffff9
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver RTL821x Gigabit Ethernet
davinci_mdio davinci_mdio.0: phy[2]: device 0:02, driver RTL821x Gigabit Ethernet
CAN device driver interface
CAN bus driver for Bosch D_CAN controller 1.0
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver dm9601
usbcore: registered new interface driver cdc_acm
cdc_acm: v0.26:USB Abstract Control Model driver for USB modems and ISDN adapters
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mice: PS/2 mouse device common for all mice
qt602240_ts 1-004a: __qt602240_read_reg: i2c transfer failed
qt602240_ts: probe of 1-004a failed with error -5
rtc-ds1307 1-0068: rtc core: registered ds3231 as rtc0
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc1
i2c /dev entries driver
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.0.0)
lm75 1-004f: hwmon0: sensor 'lm75'
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usbcore: registered new interface driver snd-usb-audio
asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
asoc: HDMI-DAI-CODEC <-> hdmi-dai mapping ok
ALSA device list:
#0: TI81XX EVM
IPVS: Registered protocols ()
IPVS: Connection hash table configured (size=4096, memory=32Kbytes)
IPVS: ipvs loaded.
TCP cubic registered
NET: Registered protocol family 17
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Registering the dns_resolver key type
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
Power Management for TI81XX.
Detected MACID=84:7e:40:e9:c9:36
rtc-ds1307 1-0068: setting system clock to 2015-01-27 14:59:09 UTC (1422370749)
ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)
ata1.15: Port Multiplier 1.2, 0x197b:0x3202 r0, 2 ports, feat 0x5/0xf
ata1.00: hard resetting link
ata1.00: SATA link up 1.5 Gbps (SStatus 113 SControl 320)
ata1.01: hard resetting link
ata1.01: SATA link down (SStatus 0 SControl 320)
ata1.00: ATA-8: Shinedisk mSATA 8G, 20130816, max UDMA/133
ata1.00: 15650208 sectors, multi 0: LBA
ata1.00: configured for UDMA/133
ata1: EH complete
scsi 0:0:0:0: Direct-Access ATA Shinedisk mSATA 2013 PQ: 0 ANSI: 5
sd 0:0:0:0: Attached scsi generic sg0 type 0
sd 0:0:0:0: [sda] 15650208 512-byte logical blocks: (8.01 GB/7.46 GiB)
sd 0:0:0:0: [sda] Write Protect is off
sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA
sda: sda1
sd 0:0:0:0: [sda] Attached SCSI disk
RAMDISK: gzip image found at block 0
VFS: Mounted root (ext2 filesystem) on device 1:0.
devtmpfs: mounted
Freeing init memory: 208K
INIT: version 2.86 booting
yaffs: dev is 32505861 name is "mtdblock5" rw
yaffs: passed flags ""
yaffs: dev is 32505862 name is "mtdblock6" rw
yaffs: passed flags ""
Please wait: booting...
Error opening /dev/fb0: No such file or directory
Starting udev
WARNING: -e needs -E or -F
udevd (86): /proc/86/oom_adj is deprecated, please use /proc/86/oom_score_adj instead.
FAT: invalid media value (0xb9)
VFS: Can't find a valid FAT filesystem on dev sda.
yaffs: dev is 8388608 name is "sda" rw
yaffs: passed flags ""
yaffs: dev is 8388608 name is "sda" rw
yaffs: passed flags ""
EXT2-fs (sda1): warning: mounting unchecked fs, running e2fsck is recommended
Remounting root file system...
Caching udev devnodes
ALSA: Restoring mixer settings...
No state is present for card EVM
Found hardware: "" "" "" "" ""
Hardware is initialized using a generic method
No state is present for card EVM
Configuring e2fsprogs.
update-alternatives: Error: cannot register alternative chattr to /usr/bin/chattr since it is already registered to /bin/chattr
update-alternatives: Linking //sbin/uuidd to uuidd.util-linux-ng
Configuring update-modules.
Configuring dbus.
Adding system startup for /etc/init.d/dbus-1.
Configuring network interfaces...
CPSW phy found : id is : 0x1cc912
CPSW phy found : id is : 0x1cc912
ifconfig: SIOCGIFFLAGS: No such device
ifconfig: SIOCSIFADDR: No such device
route: SIOCADDRT: No such device
done.
Setting up IP spoofing protection: rp_filter.
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting telnet daemon.
Starting syslogd/klogd: done
Starting thttpd.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dm814x-evm ttyO0
Arago 2011.09 dm814x-evm ttyO0
dm814x-evm login: PHY: 0:01 - Link is Up - 100/Full
PHY: 0:02 - Link is Up - 0/Half
PHY: 0:02 - Link is Down
BR
Bob
Hi Pavel,
U-Boot 2010.06 (Jun 06 2014 - 11:54:38)
TI8148-GP rev 3.0
ARM clk: 600MHz
DDR clk: 400MHz
DRAM: 2 GiB
NAND: HW ECC BCH8 Selected
256 MiB
*** Warning - bad CRC or NAND, using default environment
The 2nd stage U-Boot will now be auto-loaded
Please do not interrupt the countdown till TI8148_EVM prompt if 2nd stage is already flashed
Net: <ethaddr> not set. Reading from E-fuse
Detected MACID:84:7e:40:e9:c9:36
cpsw
Hit any key to stop autoboot: 0
NAND read: device 0 offset 0x20000, size 0x40000
262144 bytes read: OK
## Starting application at 0x81000000 ...
U-Boot 2010.06 (Jun 06 2014 - 11:55:10)
TI8148-GP rev 3.0
ARM clk: 600MHz
DDR clk: 400MHz
I2C: ready
DRAM: 2 GiB
NAND: HW ECC BCH8 Selected
256 MiB
MMC: OMAP SD/MMC: 0
.:;rrr;;.
,5#@@@@#####@@@@@@#2,
,A@@@hi;;;r5;;;;r;rrSG@@@A,
r@@#i;:;s222hG;rrsrrrrrr;ri#@@r
:@@hr:r;SG3ssrr2r;rrsrsrsrsrr;rh@@:
B@H;;rr;3Hs;rrr;sr;;rrsrsrsrsrsr;;H@B
@@s:rrs;5#;;rrrr;r#@H:;;rrsrsrsrsrr:s@@
@@;;srs&X#9;r;r;;,2@@@rrr:;;rrsrsrsrr;;@@
@@;;rrsrrs@MB#@@@@@###@@@@@@#rsrsrsrsrr;;@@
G@r;rrsrsr;#X;SX25Ss#@@#M@#9H9rrsrsrsrsrs;r@G
@9:srsrsrs;2@;:;;:.X@@@@@H::;rrsrsrsrsrsrr:3@
X@;rrsrsrsrr;XAi;;:&@@#@Bs:rrsrsrsrsrsrsrsrr;@X
@#;rsrsrsrsrr;r2ir@@@###::rrsrsrsrsrsrsrsrsr:@@
@A:rrsrsrsrr;:2@29@@M@@@;:;rrrrsrsrsrsrsrsrs;H@
@&;rsrsrsrr;A@@@@@@###@@@s::;:;;rrsrsrsrsrsr;G@
@#:rrsrsrsr;G@5Hr25@@@#@@@#9XG9s:rrrrsrsrsrs:#@
M@;rsrsrsrs;r@&#;::S@@@@@@@M@@@@Grr:;rsrsrsr;@#
:@s;rsrsrsrr:M#Msrr;;&#@@@@@@@@@@H@@5;rsrsr;s@,
@@:rrsrsrsr;S@rrrsr;:;r3MH@@#@M5,S@@irrsrr:@@
@A:rrsrsrsrrrrrsrsrrr;::;@##@r:;rH@h;srr:H@
;@9:rrsrsrsrrrsrsrsrsr;,S@Hi@i:;s;MX;rr:h@;
r@B:rrrrsrsrsrsrsrr;;sA@#i,i@h;r;S5;r:H@r
,@@r;rrrsrsrsrsrr;2BM3r:;r:G@:rrr;;r@@,
B@Mr;rrrrsrsrsr@@S;;;rrr:5M;rr;rM@H
.@@@i;;rrrrsrs2i;rrrrr;r@M:;i@@@.
.A@@#5r;;;r;;;rrr;r:r#AsM@@H.
;&@@@@MhXS5i5SX9B@@@@G;
:ihM#@@@@@##hs,
Net: Detected MACID:84:7e:40:e9:c9:36
cpsw
Hit any key to stop autoboot: 0
NAND read: device 0 offset 0x280000, size 0x600000
Skipping bad block 0x00280000
Skipping bad block 0x002a0000
Skipping bad block 0x002c0000
Skipping bad block 0x002e0000
Skipping bad block 0x00300000
Skipping bad block 0x00320000
Skipping bad block 0x00340000
Skipping bad block 0x00360000
Skipping bad block 0x00420000
Skipping bad block 0x004c0000
Skipping bad block 0x005a0000
6291456 bytes read: OK
NAND read: device 0 offset 0x880000, size 0x1400000
20971520 bytes read: OK
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Linux-2.6.37+
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2749100 Bytes = 2.6 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37+ (boblee@javenshen-desktop) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #98 Tue Jan 27 15:09:33 CST 2015
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8148evm
bootconsole [earlycon0] enabled
reserved size = 52428800 at 0x0
FB: Reserving 52428800 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8148 3.0
SRAM: Mapped pa 0x402f1000 to va 0xfe400000 size: 0xf000
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 52224
Kernel command line: mem=256M console=ttyO0,115200n8 earlyprintk root=/dev/ram rw initrd=0x82000000,32MB
PID hash table entries: 1024 (order: 0, 4096 bytes)
Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
Memory: 206MB = 206MB total
Memory: 170024k/170024k available, 92120k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xd0800000 - 0xf8000000 ( 632 MB)
lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.init : 0xc0008000 - 0xc003c000 ( 208 kB)
.text : 0xc003c000 - 0xc0532000 (5080 kB)
.data : 0xc0532000 - 0xc057a7c0 ( 290 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:375
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQ368
Trying to install interrupt handler for IRQ369
Trying to install interrupt handler for IRQ370
Trying to install interrupt handler for IRQ371
Trying to install interrupt handler for IRQ372
Trying to install interrupt handler for IRQ373
Trying to install interrupt handler for IRQ374
Trying to install type control for IRQ375
Trying to set irq flags for IRQ375
OMAP clockevent source: GPTIMER1 at 20000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 598.01 BogoMIPS (lpj=2990080)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
omap_voltage_early_init: voltage driver support not added
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!
omap_voltage_add_dev: VDD specified does not exist!
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
omap_mux_init: Add partition: #1: core, flags: 4
NOR: Can't request GPMC CS
_omap_mux_get_by_name: Could not find signal gpio1_08_mux1
_omap_mux_get_by_name: Could not find signal gpio1_10_mux1
Debugfs: Only enabling/disabling deep sleep and wakeup timer is supported now
registered ti81xx_vpss device
registered ti81xx_vidout device
registered ti81xx_fb device
registered ti81xx_vin device
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
USBSS revision 4ea2080b
registerd cppi-dma Intr @ IRQ 17
Cppi41 Init Done
omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
tps65910 1-002d: read from reg 3f failed
tps65910 1-002d: read from reg 1e failed
set_machine_constraints: failed to enable VRTC
tps65910 1-002d: failed to register tps65910-pmic regulator
tps65910-pmic: probe of tps65910-pmic failed with error -121
tps65910 1-002d: No interrupt support, no core IRQ
omap_i2c omap_i2c.3: bus 3 rev4.0 at 400 kHz
omap_i2c omap_i2c.4: bus 4 rev4.0 at 100 kHz
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
musb-hdrc: version 6.0, host, debug=0
musb-hdrc musb-hdrc.0: dma type: dma-cppi41
MUSB controller-0 revision 4ea20800
musb-hdrc musb-hdrc.0: MUSB HDRC host driver
musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 2.6.37+ musb-hcd
usb usb1: SerialNumber: musb-hdrc.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb-hdrc musb-hdrc.0: USB Host mode controller at d081e000 using DMA, IRQ 18
musb-hdrc musb-hdrc.1: dma type: dma-cppi41
MUSB controller-1 revision 4ea20800
musb-hdrc musb-hdrc.1: MUSB HDRC host driver
musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: MUSB HDRC host driver
usb usb2: Manufacturer: Linux 2.6.37+ musb-hcd
usb usb2: SerialNumber: musb-hdrc.1
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
musb-hdrc musb-hdrc.1: USB Host mode controller at d0828800 using DMA, IRQ 19
NET: Registered protocol family 2
IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (no cpio magic); looks like an initrd
Freeing initrd memory: 32768K
NetWinder Floating Point Emulator V0.97 (double precision)
PMU: registered new PMU device of type 0
omap-iommu omap-iommu.0: ducati registered
omap-iommu omap-iommu.1: sys registered
JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
msgmni has been set to 396
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
console [ttyO0] enabled, bootconsole disabled
console [ttyO0] enabled, bootconsole disabled
omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
brd: module loaded
loop: module loaded
ahci ahci.0: forcing PORTS_IMPL to 0x1
ahci ahci.0: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc apst
scsi0 : ahci_platform
ata1: SATA max UDMA/133 irq_stat 0x00400040, connection status changed irq 16
omap2-nand driver initializing
NAND device: Manufacturer ID: 0xec, Chip ID: 0xda (Samsung )
Creating 7 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000020000 : "U-Boot-min"
0x000000020000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x000000880000 : "Kernel"
0x000000880000-0x000001c80000 : "ramdisk"
0x000001c80000-0x000004480000 : "yaffs2"
0x000004480000-0x000010000000 : "Reserved"
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffff9
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver RTL821x Gigabit Ethernet
davinci_mdio davinci_mdio.0: phy[2]: device 0:02, driver RTL821x Gigabit Ethernet
CAN device driver interface
CAN bus driver for Bosch D_CAN controller 1.0
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver dm9601
usbcore: registered new interface driver cdc_acm
cdc_acm: v0.26:USB Abstract Control Model driver for USB modems and ISDN adapters
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mice: PS/2 mouse device common for all mice
qt602240_ts 1-004a: __qt602240_read_reg: i2c transfer failed
qt602240_ts: probe of 1-004a failed with error -5
rtc-ds1307 1-0068: rtc core: registered ds3231 as rtc0
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc1
i2c /dev entries driver
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.0.0)
lm75 1-004f: hwmon0: sensor 'lm75'
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usbcore: registered new interface driver snd-usb-audio
asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
asoc: HDMI-DAI-CODEC <-> hdmi-dai mapping ok
ALSA device list:
#0: TI81XX EVM
IPVS: Registered protocols ()
IPVS: Connection hash table configured (size=4096, memory=32Kbytes)
IPVS: ipvs loaded.
TCP cubic registered
NET: Registered protocol family 17
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Registering the dns_resolver key type
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
Power Management for TI81XX.
Detected MACID=84:7e:40:e9:c9:36
rtc-ds1307 1-0068: setting system clock to 2015-01-27 14:59:09 UTC (1422370749)
ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)
ata1.15: Port Multiplier 1.2, 0x197b:0x3202 r0, 2 ports, feat 0x5/0xf
ata1.00: hard resetting link
ata1.00: SATA link up 1.5 Gbps (SStatus 113 SControl 320)
ata1.01: hard resetting link
ata1.01: SATA link down (SStatus 0 SControl 320)
ata1.00: ATA-8: Shinedisk mSATA 8G, 20130816, max UDMA/133
ata1.00: 15650208 sectors, multi 0: LBA
ata1.00: configured for UDMA/133
ata1: EH complete
scsi 0:0:0:0: Direct-Access ATA Shinedisk mSATA 2013 PQ: 0 ANSI: 5
sd 0:0:0:0: Attached scsi generic sg0 type 0
sd 0:0:0:0: [sda] 15650208 512-byte logical blocks: (8.01 GB/7.46 GiB)
sd 0:0:0:0: [sda] Write Protect is off
sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA
sda: sda1
sd 0:0:0:0: [sda] Attached SCSI disk
RAMDISK: gzip image found at block 0
VFS: Mounted root (ext2 filesystem) on device 1:0.
devtmpfs: mounted
Freeing init memory: 208K
INIT: version 2.86 booting
yaffs: dev is 32505861 name is "mtdblock5" rw
yaffs: passed flags ""
yaffs: dev is 32505862 name is "mtdblock6" rw
yaffs: passed flags ""
Please wait: booting...
Error opening /dev/fb0: No such file or directory
Starting udev
WARNING: -e needs -E or -F
udevd (86): /proc/86/oom_adj is deprecated, please use /proc/86/oom_score_adj instead.
FAT: invalid media value (0xb9)
VFS: Can't find a valid FAT filesystem on dev sda.
yaffs: dev is 8388608 name is "sda" rw
yaffs: passed flags ""
yaffs: dev is 8388608 name is "sda" rw
yaffs: passed flags ""
EXT2-fs (sda1): warning: mounting unchecked fs, running e2fsck is recommended
Remounting root file system...
Caching udev devnodes
ALSA: Restoring mixer settings...
No state is present for card EVM
Found hardware: "" "" "" "" ""
Hardware is initialized using a generic method
No state is present for card EVM
Configuring e2fsprogs.
update-alternatives: Error: cannot register alternative chattr to /usr/bin/chattr since it is already registered to /bin/chattr
update-alternatives: Linking //sbin/uuidd to uuidd.util-linux-ng
Configuring update-modules.
Configuring dbus.
Adding system startup for /etc/init.d/dbus-1.
Configuring network interfaces...
CPSW phy found : id is : 0x1cc912
CPSW phy found : id is : 0x1cc912
ifconfig: SIOCGIFFLAGS: No such device
ifconfig: SIOCSIFADDR: No such device
route: SIOCADDRT: No such device
done.
Setting up IP spoofing protection: rp_filter.
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting telnet daemon.
Starting syslogd/klogd: done
Starting thttpd.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dm814x-evm ttyO0
Arago 2011.09 dm814x-evm ttyO0
dm814x-evm login: PHY: 0:01 - Link is Up - 100/Full
PHY: 0:02 - Link is Up - 0/Half
PHY: 0:02 - Link is Down
Bob,
Your log ends here:
bob lee said:asoc: HDMI-DAI-CODEC <-> hdmi-dai mapping ok
ALSA device list:
#0: TI81XX EVM
Is this just part of the boot log or it hangs here?
bob lee said:Kernel command line: mem=256M console=ttyO0,115200n8 earlyprintk root=/dev/ram rw initrd=0x82000000,32MB
I see you are not using NFS but RAM. You are not using nor static IP neither dynamic IP (DHCP). I think you mess up your boot settings in NAND.
BR
Pavel
IPVS: Registered protocols ()
IPVS: Connection hash table configured (size=4096, memory=32Kbytes)
IPVS: ipvs loaded.
TCP cubic registered
NET: Registered protocol family 17
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Registering the dns_resolver key type
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
Power Management for TI81XX.
Detected MACID=84:7e:40:e9:c9:36
rtc-ds1307 1-0068: setting system clock to 2015-01-27 17:56:27 UTC (1422381387)
ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)
ata1.15: Port Multiplier 1.2, 0x197b:0x3202 r0, 2 ports, feat 0x5/0xf
ata1.00: hard resetting link
ata1.00: SATA link up 1.5 Gbps (SStatus 113 SControl 320)
ata1.01: hard resetting link
ata1.01: SATA link down (SStatus 0 SControl 320)
ata1.00: ATA-8: Shinedisk mSATA 8G, 20130816, max UDMA/133
ata1.00: 15650208 sectors, multi 0: LBA
ata1.00: configured for UDMA/133
ata1: EH complete
scsi 0:0:0:0: Direct-Access ATA Shinedisk mSATA 2013 PQ: 0 ANSI: 5
sd 0:0:0:0: Attached scsi generic sg0 type 0
sd 0:0:0:0: [sda] 15650208 512-byte logical blocks: (8.01 GB/7.46 GiB)
sd 0:0:0:0: [sda] Write Protect is off
sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA
sda: sda1
sd 0:0:0:0: [sda] Attached SCSI disk
RAMDISK: gzip image found at block 0
VFS: Mounted root (ext2 filesystem) on device 1:0.
devtmpfs: mounted
Freeing init memory: 208K
INIT: version 2.86 booting
yaffs: dev is 32505861 name is "mtdblock5" rw
yaffs: passed flags ""
yaffs: dev is 32505862 name is "mtdblock6" rw
yaffs: passed flags ""
Please wait: booting...
Error opening /dev/fb0: No such file or directory
Starting udev
WARNING: -e needs -E or -F
udevd (86): /proc/86/oom_adj is deprecated, please use /proc/86/oom_score_adj instead.
FAT: invalid media value (0xb9)
VFS: Can't find a valid FAT filesystem on dev sda.
yaffs: dev is 8388608 name is "sda" rw
yaffs: passed flags ""
yaffs: dev is 8388608 name is "sda" rw
yaffs: passed flags ""
EXT2-fs (sda1): warning: mounting unchecked fs, running e2fsck is recommended
Remounting root file system...
Caching udev devnodes
ALSA: Restoring mixer settings...
No state is present for card EVM
Found hardware: "" "" "" "" ""
Hardware is initialized using a generic method
No state is present for card EVM
Configuring e2fsprogs.
update-alternatives: Error: cannot register alternative chattr to /usr/bin/chattr since it is already registered to /bin/chattr
update-alternatives: Linking //sbin/uuidd to uuidd.util-linux-ng
Configuring update-modules.
Configuring dbus.
Adding system startup for /etc/init.d/dbus-1.
Configuring network interfaces...
CPSW phy found : id is : 0x1cc912
CPSW phy found : id is : 0x1cc912
ifconfig: SIOCGIFFLAGS: No such device
ifconfig: SIOCSIFADDR: No such device
route: SIOCADDRT: No such device
done.
Setting up IP spoofing protection: rp_filter.
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting telnet daemon.
Starting syslogd/klogd: done
Starting thttpd.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dm814x-evm ttyO0
Arago 2011.09 dm814x-evm ttyO0
dm814x-evm login: PHY: 0:01 - Link is Up - 100/Full
PHY: 0:02 - Link is Up - 0/Half
PHY: 0:02 - Link is Down
IPVS: Registered protocols ()
IPVS: Connection hash table configured (size=4096, memory=32Kbytes)
IPVS: ipvs loaded.
TCP cubic registered
NET: Registered protocol family 17
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Registering the dns_resolver key type
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
Power Management for TI81XX.
Detected MACID=84:7e:40:e9:c9:36
rtc-ds1307 1-0068: setting system clock to 2015-01-27 18:05:42 UTC (1422381942)
ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)
ata1.15: Port Multiplier 1.2, 0x197b:0x3202 r0, 2 ports, feat 0x5/0xf
ata1.00: hard resetting link
ata1.00: SATA link up 1.5 Gbps (SStatus 113 SControl 320)
ata1.01: hard resetting link
ata1.01: SATA link down (SStatus 0 SControl 320)
ata1.00: ATA-8: Shinedisk mSATA 8G, 20130816, max UDMA/133
ata1.00: 15650208 sectors, multi 0: LBA
ata1.00: configured for UDMA/133
ata1: EH complete
scsi 0:0:0:0: Direct-Access ATA Shinedisk mSATA 2013 PQ: 0 ANSI: 5
sd 0:0:0:0: Attached scsi generic sg0 type 0
sd 0:0:0:0: [sda] 15650208 512-byte logical blocks: (8.01 GB/7.46 GiB)
sd 0:0:0:0: [sda] Write Protect is off
sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA
sda: sda1
sd 0:0:0:0: [sda] Attached SCSI disk
RAMDISK: gzip image found at block 0
VFS: Mounted root (ext2 filesystem) on device 1:0.
devtmpfs: mounted
Freeing init memory: 208K
INIT: version 2.86 booting
yaffs: dev is 32505861 name is "mtdblock5" rw
yaffs: passed flags ""
yaffs: dev is 32505862 name is "mtdblock6" rw
yaffs: passed flags ""
Please wait: booting...
Error opening /dev/fb0: No such file or directory
Starting udev
WARNING: -e needs -E or -F
udevd (86): /proc/86/oom_adj is deprecated, please use /proc/86/oom_score_adj instead.
FAT: invalid media value (0xb9)
VFS: Can't find a valid FAT filesystem on dev sda.
yaffs: dev is 8388608 name is "sda" rw
yaffs: passed flags ""
yaffs: dev is 8388608 name is "sda" rw
yaffs: passed flags ""
EXT2-fs (sda1): warning: mounting unchecked fs, running e2fsck is recommended
Remounting root file system...
Caching udev devnodes
ALSA: Restoring mixer settings...
No state is present for card EVM
Found hardware: "" "" "" "" ""
Hardware is initialized using a generic method
No state is present for card EVM
Configuring e2fsprogs.
update-alternatives: Error: cannot register alternative chattr to /usr/bin/chattr since it is already registered to /bin/chattr
update-alternatives: Linking //sbin/uuidd to uuidd.util-linux-ng
Configuring update-modules.
Configuring dbus.
Adding system startup for /etc/init.d/dbus-1.
Configuring network interfaces...
CPSW phy found : id is : 0x1cc912
CPSW phy found : id is : 0x1cc912
ifconfig: SIOCGIFFLAGS: No such device
ifconfig: SIOCSIFADDR: No such device
route: SIOCADDRT: No such device
done.
Setting up IP spoofing protection: rp_filter.
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting telnet daemon.
Starting syslogd/klogd: done
Starting thttpd.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dm814x-evm ttyO0
Arago 2011.09 dm814x-evm ttyO0
dm814x-evm login: PHY: 0:01 - Link is Up - 100/Full
PHY: 0:02 - Link is Up - 0/Half
PHY: 0:02 - Link is Down
Hi Pavel,
I have pasted the other part message,but it shows as below.
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
If the administrator has configured this forum to support email notifications you will receive an email when your post is either approved or denied (if you have emails enabled in your profile).
Return to the DM814x and AM387x Processors Forum forum
BR
Bob
Bob,
bob lee said:RAMDISK: gzip image found at block 0
VFS: Mounted root (ext2 filesystem) on device 1:0.
devtmpfs: mounted
Freeing init memory: 208K
INIT: version 2.86 booting
yaffs: dev is 32505861 name is "mtdblock5" rw
yaffs: passed flags ""
yaffs: dev is 32505862 name is "mtdblock6" rw
yaffs: passed flags ""
I see you are using yaffs, not NFS with static/dynamic ip. But this e2e thread was opened with question regarding static ip. Could you please provide all your remaining questions regarding static ip usage?
BR
Pavel
Hi Pavel,
I only mount two blocks for yaffs.
I only want to set the ip to static ip in ramdisk.gz.Then I do , but it shows the message as below before login.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dm814x-evm ttyO0
Arago 2011.09 dm814x-evm ttyO0
dm814x-evm login: PHY: 0:01 - Link is Up - 100/Full
PHY: 0:02 - Link is Up - 0/Half
PHY: 0:02 - Link is Down
But I think it should be as this.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dm814x-evm ttyO0
Arago 2011.09 dm814x-evm ttyO0
dm814x-evm login:
BR
Bob
Bob,
bob lee said:I only want to set the ip to static ip in ramdisk.gz.
The static ip is set in u-boot and linux kernel. I do not think the static ip can be set in root fs (ramdisk.gz).
bob lee said:dm814x-evm login: PHY: 0:01 - Link is Up - 100/Full
PHY: 0:02 - Link is Up - 0/Half
PHY: 0:02 - Link is Down
I think your ethernet cable connection is not stable, see the blow e2e threads:


BR
Pavel