I am trying to get Graphics SDK 's sgx driver work on my ubuntu ARM 12.04.
with linux-2.6.37-psp04.01.00.06.patch4.; ezsdk_dm814x-evm_5_03_01_15 ; graphics-sdk_4.04.00.02
the ubuntu arm 12.04 rootfs work fine without the ti81xxfb driver before this, I run a QT program with my lvds LCD.
Today ,I rebulid the kernel and the sgx driver, and run make install in graphics-sdk_4.04.00.02 dir to install the km and sdk to my rootfs
I use the 38xx-demo to install the sgx dirver module and sdk,and disable the origin x in the script , and reboot.
After reboot , the vpss ti81xxfb cmem syslink was loaded( vpssis load with vram=0:48m,1:1M,2:1M)
Then I try to run /etc/init.d/rc.pvr ,it print out some error messages and hang there .
With lsmod ,the drm and pvrsrvkm module was loaded at this point.
What can I do to fix this problem?
below is the dmesg output:
--------------------------------------------------------------------------------------------------------------------
[ 2.060000] CPSW phy found : id is : 0x4dd074
[ 2.070000] PHY 0:01 not found
[ 3.080000] IP-Config: Complete:
[ 3.080000] device=eth0, addr=192.168.1.169, mask=255.255.0.0, gw=192.168.1.49,
[ 3.090000] host=192.168.1.169, domain=, nis-domain=(none),
[ 3.090000] bootserver=192.168.1.49, rootserver=192.168.1.49, rootpath=
[ 5.060000] PHY: 0:00 - Link is Up - 100/Full
[ 5.170000] VFS: Mounted root (nfs filesystem) on device 0:14.
[ 5.170000] devtmpfs: mounted
[ 5.180000] Freeing init memory: 176K
[ 6.930000] SysLink version : 2.00.05.85
[ 6.930000] SysLink module created on Date:Apr 24 2013 Time:15:38:22
[ 7.110000] <30>udevd[136]: starting version 175
[ 14.670000] init: failsafe main process (319) killed by TERM signal
[ 15.210000] init: udev-fallback-graphics main process (370) terminated with status 1
[ 17.160000] CMEMK module: built on Apr 24 2013 at 15:38:17
[ 17.160000] Reference Linux version 2.6.37
[ 17.160000] File /opt/d500/ti-ezsdk_dm814x-evm_5_03_01_15/component-sources/linuxutils_3_21_00_04/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c
[ 17.160000] CMEM Range Overlaps Kernel Physical - allowing overlap
[ 17.160000] CMEM phys_start (0x96000000) overlaps kernel (0x80000000 -> 0xa3a00000)
[ 17.160000] allocated heap buffer 0xe1000000 of size 0x2000000
[ 17.160000] heap fallback enabled - will try heap if pool buffer is not available
[ 17.160000] cmemk initialized
[ 17.200000] SDMAK module: built on Apr 24 2013 at 15:44:38
[ 17.200000] Reference Linux version 2.6.37
[ 17.200000] EDMAK Debug: rfxtiling registered major = 250
[ 17.240000] init: firmware-dm814x-fb main process (111) terminated with status 1
[ 85.400000] [drm] Initialized drm 1.1.0 20060810
[ 85.450000] [drm] Initialized pvrsrvkm 1.6.4117 Wed January 21 PST 2015 for SGX on minor 0
[ 85.650000] Unhandled fault: external abort on non-linefetch (0x1008) at 0xde9c0014
[ 85.660000] Internal error: : 1008 [#1]
[ 85.660000] last sysfs file: /sys/devices/SGX/drm/card0/uevent
[ 85.660000] Modules linked in: pvrsrvkm drm rfxtiling cmemk ti81xxfb vpss syslink
[ 85.660000] CPU: 0 Not tainted (2.6.37 #1)
[ 85.660000] PC is at OSReadHWReg+0xc/0x18 [pvrsrvkm]
[ 85.660000] LR is at SysCreateVersionString+0x30/0x8c [pvrsrvkm]
[ 85.660000] pc : [<bf1c30bc>] lr : [<bf1ce244>] psr: a0000013
[ 85.660000] sp : d4c0bd48 ip : d4c0bd58 fp : d4c0bd54
[ 85.660000] r10: bf1d4318 r9 : bf1c47dc r8 : 00000042
[ 85.660000] r7 : d5227000 r6 : 00000000 r5 : de9c0000 r4 : bf1d4c2c
[ 85.660000] r3 : 00000012 r2 : 00000000 r1 : 00000014 r0 : de9c0000
[ 85.660000] Flags: NzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
[ 85.660000] Control: 10c5387d Table: 94c00019 DAC: 00000015
[ 85.660000] Process pvrsrvinit (pid: 775, stack limit = 0xd4c0a2e8)
[ 85.660000] Stack: (0xd4c0bd48 to 0xd4c0c000)
[ 85.660000] bd40: d4c0bd74 d4c0bd58 bf1ce244 bf1c30bc 00000002 bf1d4c2c
[ 85.660000] bd60: bf1d4c2c bf1d4ba4 d4c0bd94 d4c0bd78 bf1ce314 bf1ce220 bf1d4c2c d5227000
[ 85.660000] bd80: d5226000 d5227000 d4c0bdac d4c0bd98 bf1bc7bc bf1ce2ac 00000000 d5227000
[ 85.660000] bda0: d4c0bdcc d4c0bdb0 bf1ca0ac bf1bc7a8 d5226000 d4c0be48 d5179140 d5227000
[ 85.660000] bdc0: d4c0bdf4 d4c0bdd0 bf1c8f38 bf1ca064 c01c6742 d4c0be48 00000307 d5208b00
[ 85.660000] bde0: 401c6440 bf1c47dc d4c0be1c d4c0bdf8 bf1c48fc bf1c8e68 c0b47960 d5179140
[ 85.660000] be00: 0000001c d4c0be48 0000001c d5208b00 d4c0bef4 d4c0be20 bf184180 bf1c47e8
[ 85.660000] be20: 00000307 401c6440 00000040 0000e200 00000001 d4c0be40 c009d4ac bef7b434
[ 85.660000] be40: d4c27400 d4c27420 00000042 0000001c bef7b468 00000008 bef7b460 00000008
[ 85.660000] be60: 00000001 c009b514 00000000 40a4e000 40a4e000 40a4dfff c0528894 c0528894
[ 85.660000] be80: d4c0bea4 d4c0be90 c009d7a8 c009d5dc d4c01028 40a4e000 d4c0becc d4c0bea8
[ 85.660000] bea0: c00aec74 c009d778 000037ee 00000000 00000000 40a4d000 bef5a000 c0528894
[ 85.660000] bec0: d4c0bf04 d4c0bed0 c00aed30 00000000 d5208b80 00000003 00000003 bef7b434
[ 85.660000] bee0: d4c0a000 00000000 d4c0bf04 d4c0bef8 c00cc0ec bf183eec d4c0bf74 d4c0bf08
[ 85.660000] bf00: c00cc7fc c00cc0d0 d4c5f688 00000000 d4c5f688 d5213b00 d4c0bf3c d4c0bf28
[ 85.660000] bf20: c00b08d4 c00bbe54 d4c5f688 d4c2c900 d4c0bf84 d4c0bf40 c00b18f0 c00b087c
[ 85.660000] bf40: 40a4e000 00000002 d4c0bf6c 00000000 bef7b434 401c6440 00000003 d5208b80
[ 85.660000] bf60: d4c0a000 00000000 d4c0bfa4 d4c0bf78 c00cc894 c00cc308 d4c0bfa4 00000000
[ 85.660000] bf80: c00b1968 00000001 bef7b434 401c6440 00000036 c003ef48 00000000 d4c0bfa8
[ 85.660000] bfa0: c003eda0 c00cc848 00000001 bef7b434 00000003 401c6440 bef7b434 0000001c
[ 85.660000] bfc0: 00000001 bef7b434 401c6440 00000036 00000000 00000000 40096000 00000000
[ 85.660000] bfe0: 400604cc bef7b40c 40052968 401bf85c 20000010 00000003 95ffe021 95ffe421
[ 85.660000] Backtrace:
[ 85.660000] [<bf1c30b0>] (OSReadHWReg+0x0/0x18 [pvrsrvkm]) from [<bf1ce244>] (SysCreateVersionString+0x30/0x8c [pvrsrvkm])
[ 85.660000] [<bf1ce214>] (SysCreateVersionString+0x0/0x8c [pvrsrvkm]) from [<bf1ce314>] (SysFinalise+0x74/0x94 [pvrsrvkm])
[ 85.660000] r5:bf1d4ba4 r4:bf1d4c2c
[ 85.660000] [<bf1ce2a0>] (SysFinalise+0x0/0x94 [pvrsrvkm]) from [<bf1bc7bc>] (PVRSRVFinaliseSystem+0x20/0x58 [pvrsrvkm])
[ 85.660000] r7:d5227000 r6:d5226000 r5:d5227000 r4:bf1d4c2c
[ 85.660000] [<bf1bc79c>] (PVRSRVFinaliseSystem+0x0/0x58 [pvrsrvkm]) from [<bf1ca0ac>] (PVRSRVInitSrvDisconnectBW+0x54/0x84 [pvrsrvkm])
[ 85.660000] r5:d5227000 r4:00000000
[ 85.660000] [<bf1ca058>] (PVRSRVInitSrvDisconnectBW+0x0/0x84 [pvrsrvkm]) from [<bf1c8f38>] (BridgedDispatchKM+0xdc/0x134 [pvrsrvkm])
[ 85.660000] r7:d5227000 r6:d5179140 r5:d4c0be48 r4:d5226000
[ 85.660000] [<bf1c8e5c>] (BridgedDispatchKM+0x0/0x134 [pvrsrvkm]) from [<bf1c48fc>] (PVRSRV_BridgeDispatchKM+0x120/0x150 [pvrsrvkm])
[ 85.660000] r9:bf1c47dc r8:401c6440 r7:d5208b00 r6:00000307 r5:d4c0be48
[ 85.660000] r4:c01c6742
[ 85.660000] [<bf1c47dc>] (PVRSRV_BridgeDispatchKM+0x0/0x150 [pvrsrvkm]) from [<bf184180>] (drm_ioctl+0x2a0/0x3a0 [drm])
[ 85.660000] r7:d5208b00 r6:0000001c r5:d4c0be48 r4:0000001c
[ 85.660000] [<bf183ee0>] (drm_ioctl+0x0/0x3a0 [drm]) from [<c00cc0ec>] (vfs_ioctl+0x28/0x44)
[ 85.660000] [<c00cc0c4>] (vfs_ioctl+0x0/0x44) from [<c00cc7fc>] (do_vfs_ioctl+0x500/0x540)
[ 85.660000] [<c00cc2fc>] (do_vfs_ioctl+0x0/0x540) from [<c00cc894>] (sys_ioctl+0x58/0x7c)
[ 85.660000] [<c00cc83c>] (sys_ioctl+0x0/0x7c) from [<c003eda0>] (ret_fast_syscall+0x0/0x30)
[ 85.660000] r8:c003ef48 r7:00000036 r6:401c6440 r5:bef7b434 r4:00000001
[ 85.660000] Code: e89da800 e1a0c00d e92dd800 e24cb004 (e7900001)
[ 86.110000] ---[ end trace f508dcc167c706ab ]---
[ 86.120000] [drm:drm_release] *ERROR* Device busy: 1