This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 EVM please help

Hello!

I have DM365 EVM; SDK 2_10_01_18; psp 02_10_00_14

bootargs=mem=116M console=ttyS0,115200n8 noninitrd rw ip=dhcp root=/dev/nfs nfsroot=192.168.0.200:/home/magbob/workdir/filesys,nolock video=divincifb:vid0=OFF:v
id1=OFF:osd0=720x576x16,4050K:osd1=720x576x16,4050K dm365_imp.oper_mode=0 davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=ntsc davinci_capture.device_type=1

Connected input (J13) camera Sony KPC-EX20.

I run ./video_loopback

Encode demo started.
davinci_resizer davinci_resizer.2: RSZ_G_CONFIG:0:1:108
davinci_previewer davinci_previewer.2: ipipe_set_preview_config

davinci_previewer davinci_previewer.2: ipipe_set_preview_config

vpfe ccdc capture vpfe ccdc capture.1: IMP chained

preview is endvpfe ccdc capture vpfe ccdc capture.1: Resizer present

MUX: initialized GPIO40
DavinciDisplay DavinciDisplay.1: Before finishing with S_FMT:
layer.pix_fmt.bytesperline = 1280,
 layer.pix_fmt.width = 1280,
 layer.pix_fmt.height = 720,
 layer.pix_fmt.sizeimage =1843200
DavinciDisplay DavinciDisplay.1: pixfmt->width = 1280,
 layer->layer_info.config.line_length= 1280
i2c_adapter i2c-0: tvp514x_setinput:lost lock]
i2c_adapter i2c-0: tvp514x: no input connected
vpfe ccdc capture vpfe ccdc capture.1: vpfe_get_std_info: Error in set std in de
coder
vpfe ccdc capture vpfe ccdc capture.1: Error in initializing channel
DavinciDisplay DavinciDisplay.1: streaming not started in layer id = 0
Error: [capture.c] Cannot open /dev/video0 (Invalid argument)

init capture is end
Error: [display.c] (pre) putDisplayBuffer() failed
cleanup_display: VIDIOC_STREAMOFF: Invalid argument

help me please, why not see input composite?