Hi,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Hi Baptiste,
What is the sampling rate you want to achieve? Isn't it possible to do this with standard McSPI peripheral? I don't think there are ready examples of doing this with PRU.
Hi Biser,
Thanks for your help. I would like to achieve a minimum sampling rate of 1 MSPS, and if possible in a "real-time" way, i.e. the time between two samples should always be the same.
Is it possible with standard McSPI peripheral? If so, it would make things easier I think. Do you have a link to relevant online resources to get me started?
Many thanks
Baptiste
The McSPI can go up to 48MHz clock, however I don't think that what you want to achieve will be possible under Linux. You might want to check the Starterware package, which is an OS-less environment: http://processors.wiki.ti.com/index.php/StarterWare