This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HyperLink pair/lane swap configuration



SPRABC1 "SerDes Implementation Guide for Keystone I Devices" p.16 says:

- HyperLink lanes can be swapped to simplify routing.  The differential pairing must be maintained.

- P and N connections for a single differential pair can be inverted to simplify routing.

I don't see anything in SPRUGW8C "HyperLink for Keystone Devices User Guide" about lane swapping.

To invert a HyperLink pair, the registers in SPRUGW8C Sec 3.4.3 - 3.4.4 include an INVPAIR bit for each Tx/Rx register, but the description says "This field is set automatically by the HyperLink module" as if the setting is configured elsewhere.

Questions:

1. How is HyperLink lane swapping configured?

2. How is HyperLink pair inversion configured?