This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

No Display in Display device on DM355EVM



Hi All

I am using DM355EVM from spectrum digital. When I am running the demo on that board ,I did not get any error message on terminal.But i could not see anything on

Display device which is connected to TVOUT on the board.

/decode -v data/videos/mpeg4ts_part1.mpeg4 -t 20

Demo started...

I did not get any error.But no display in display device.

 

For displaying png image on device

./interface

Demo is running level 0

I did not get any error.But no display in display device.

 

Dvsdk version is  dvsdk_DM355_setuplinux_1_30_00_23.bin

bootargs console=ttyS0,115200n8   noinitrd rw ip=dhcp root=/dev/nfs  nfsroot=$(nfshost):$(rootpath),nolock mem=116M

Does any changes need in boot arguments?

 

thanks and regards

Tamil