This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dra7xx-evm I2C2 Config error



Hello All,


I am using DRA7xx-EVM HW .

processors.wiki.ti.com/.../DRA7xx_GLSDK_Software_Developers_Guide

I was trying to configure I2C2 pins on my target  to run VIP application demos and it fails every-time.

root@dra7xx-evm:~# devmem2 0x4847C010 w 0x4
/dev/mem opened.
Memory mapped at address 0xb6f38[   55.742431] Unhandled fault: imprecise external abort (0x1406) at 0x00000000
000.
Bus error

Can anyone help to resolve this ?

Thanks,

Kanagarajan

  • Hello Kanagarajan,

    It seems that your I2C2 module is not enabled.

    Check the following registers and apply the proposed settings.

    L4PER power state
    0x4AE0 7400 - PM_L4PER_PWRSTCTRL[1:0] POWERSTATE - 0x3: ON State

    0x4A00 9700 - CM_L4PER_CLKSTCTRL[1:0] CLKTRCTRL - 0x2: SW_WKUP
    Controls the clock state transition of the L4PER clock domain.

    0x4A00 97A8 - CM_L4PER_I2C2_CLKCTRL[1:0] MODULEMODE - 0x2 Module is explicitly enabled.

    After PRCM configuration for I2C2 module please check I2C2 Pad configuration in Control Module:

    CTRL_CORE_PAD_I2C2_SDA  -  0x4A00 3808
    CTRL_CORE_PAD_I2C2_SCL  -  0x4A00 380C

    After this global configurations settings, you should write in I2C2 registers - I2C_SYSC


    Best regards,

    Yanko

  • Hello Yanko,

    After checking the ctrl pad register ,what would be settings for the I2C_SYSC register of I2C2 module ? 

    Thanks,

    Kanagarajan

  • Hello Kanagarajan,

    Check the values in following fields:
    I2C_SYSC[9:8] CLKACTIVITY 0x3: Both clocks must be kept active
    I2C_SYSC[4:3] IDLEMODE 0x1 No Idle mode
    I2C_SYSC[1] SRST - 0x0: Normal mode
    I2C_SYSC[0] AUTOIDLE - 0x0: Auto Idle mechanism is disabled

    Could you confirm that your are already able to write in 0x4847C010?

    Best regards,
    Yanko
  • Hello Yanko,

    I have explicitly enabled module mode in 0x4A00 97A8 - CM_L4PER_I2C2_CLKCTRL register (value 0x30002).
    And still I am unable to write in 0x4847C010 , please find the log from the target.

    May I know which register is mapped to 0x4847C010 ?


    root@dra7xx-evm:~#
    root@dra7xx-evm:~#
    root@dra7xx-evm:~# devmem2 0x4A009700
    /dev/mem opened.
    Memory mapped at address 0xb6fc4000.
    Read at address 0x4A009700 (0xb6fc4700): 0x01209103
    root@dra7xx-evm:~# devmem2 0x4A0097A8
    /dev/mem opened.
    Memory mapped at address 0xb6fad000.
    Read at address 0x4A0097A8 (0xb6fad7a8): 0x00030000
    root@dra7xx-evm:~# devmem2 0x4A0097A8 w 0x00030002
    /dev/mem opened.
    Memory mapped at address 0xb6f3d000.
    Read at address 0x4A0097A8 (0xb6f3d7a8): 0x00030000
    Write at address 0x4A0097A8 (0xb6f3d7a8): 0x00030002, readback 0x00030002
    root@dra7xx-evm:~# devmem2 0x4A003808
    /dev/mem opened.
    Memory mapped at address 0xb6f87000.
    Read at address 0x4A003808 (0xb6f87808): 0x00060000
    root@dra7xx-evm:~# devmem2 0x4A00380C
    /dev/mem opened.
    Memory mapped at address 0xb6fb8000.
    Read at address 0x4A00380C (0xb6fb880c): 0x00060000
    root@dra7xx-evm:~# devmem2 0x4847C010 w 0x4
    /dev/mem opened.
    Memory mapped at address 0xb6fee[ 165.109161] Unhandled fault: imprecise external abort (0x1406) at 0x00000000
    000.
    Bus error

    Thanks,
    Kanagarajan
  • Hello Kanagarajan,

    If you read   0x4A00 97A8 - CM_L4PER_I2C2_CLKCTRL register value 0x30002.  

    17:16 -  0x3: Module is disabled and cannot be accessed

    1:0 MODULEMODE - 0x2: Module is explicitly enabled.

    With this value you cannot access I2C2 module.To access I2C2 module please set - CM_L4PER_CLKSTCTRL[1:0] CLKTRCTRL - 0x2: SW_WKUP

    However, you are unable to write in 0x4847C010, because this register belong to McASP8 module. This address corresponds to MCASP_PFUNC register.


    Best regards,

    Yanko

  • Hello Yanko,

    In order to effect the changes of register write 0x4A00 97A8 with 0x2: Module is explicitly enabled - I tried to modify the register directly within the init of i2c driver it crashes , seems memory is not mapped .
    is there a specific way to access the core register in kernel during start-up ?

    I have gone through the board specific init for I2C2 controller the module mode is enabled by default using the struct definitions dra7xx_i2c2_hwmod -> .modulemode = MODULEMODE_SWCTRL, but it seems to be not working ,after startup when i read the register values , it uses the default reset values of the register would find the value of the register as 0x 0x00030000. Also i am not sure how to set 16:17 bits to enable the module using the struct dra7xx_i2c2_hwmod , is there any flags available ?

    Thanks,
    Kanagarajan
  • Hello Kanagarajan,

    I see that you use GLSDK SW release. See my steps for enabling I2C2 module by using omapconf tool:

    root@dra7xx-evm:~# omapconf read 0x4A0097A8

    00030000

    root@dra7xx-evm:~# omapconf set bit 0x4A0097A8 1

    @0x4A0097A8: 0x00030000 ==> 0x00030002

    root@dra7xx-evm:~# omapconf read 0x4AE07400

    000F0105

    root@dra7xx-evm:~# omapconf set bit 0x4AE07400 1

    @0x4AE07400: 0x000F0105 ==> 0x000F0107

    root@dra7xx-evm:~# omapconf read 0x4A009700

    01229103

    root@dra7xx-evm:~# omapconf clear bit 0x4A009700 0

    @0x4A009700: 0x01229103 ==> 0x01229102

    root@dra7xx-evm:~# omapconf read 0x4A0097A8

    00000002

    After this configuration I can access I2C2 module's registers:

    root@dra7xx-evm:~# omapconf read 0x48072000  - I2C_REVNB_LO
    0000080C

    root@dra7xx-evm:~# omapconf read 0x48072004  - I2C_REVNB_HI
    00005040

    Bits 16:17 cannot be set. Those bits are read only. 

    Could you explain what modifications are applied in your kernel?


    Best regards,

    Yanko

  • Hello Yanko,

    In my kernel modifications , just tried to read the register values from kernel using readl function using the memory  address of 0x4A0097A8 and it crashes due to invalid memory mapping.

    I2C1 module is enabled during the kernel startup itself could find in the log  below and why it fails to do the same for I2C2 ?

    root@dra7xx-evm:~# omapconf dump 0x4A0097A0 0x4A0097A8
    |----------------------------|
    | Address (hex) | Data (hex) |
    |----------------------------|
    | 0x4A0097A0    | 0x00020002 | // I2C1
    | 0x4A0097A4    | 0x00000000 |
    | 0x4A0097A8    | 0x00030000 | // I2C2
    |----------------------------|

    I tried your configuration on my target , please find the log :

    root@dra7xx-evm:~#  omapconf read 0x4A0097A8

    00030000

    omapconf: powerdm_deinit(): cpu not supported!!!

    omapconf: clockdm_deinit(): cpu not supported!!!

    root@dra7xx-evm:~#  omapconf set bit 0x4A0097A8 1

    @0x4A0097A8: 0x00030000 ==> 0x00030002

    omapconf: powerdm_deinit(): cpu not supported!!!

    omapconf: clockdm_deinit(): cpu not supported!!!

    root@dra7xx-evm:~# omapconf read 0x4AE07400

    000F0107

    omapconf: powerdm_deinit(): cpu not supported!!!

    omapconf: clockdm_deinit(): cpu not supported!!!

    root@dra7xx-evm:~#

    root@dra7xx-evm:~# omapconf set bit 0x4AE07400 1

    @0x4AE07400: 0x000F0107 ==> 0x000F0107

    omapconf: powerdm_deinit(): cpu not supported!!!

    omapconf: clockdm_deinit(): cpu not supported!!!

    root@dra7xx-evm:~# omapconf read 0x4A009700                                                                                          

    01209103

    omapconf: powerdm_deinit(): cpu not supported!!!

    omapconf: clockdm_deinit(): cpu not supported!!!

    root@dra7xx-evm:~# omapconf clear bit 0x4A009700 0

    @0x4A009700: 0x01209103 ==> 0x01209102

    omapconf: powerdm_deinit(): cpu not supported!!!

    omapconf: clockdm_deinit(): cpu not supported!!!

    root@dra7xx-evm:~# omapconf read 0x4A0097A8

    00020002

    omapconf: powerdm_deinit(): cpu not supported!!!

    omapconf: clockdm_deinit(): cpu not supported!!!

    root@dra7xx-evm:~# omapconf read 0x48072000

    0000080C

    omapconf: powerdm_deinit(): cpu not supported!!!

    omapconf: clockdm_deinit(): cpu not supported!!!

    root@dra7xx-evm:~# omapconf read 0x48072004

    00005040

    omapconf: powerdm_deinit(): cpu not supported!!!

    omapconf: clockdm_deinit(): cpu not supported!!!

    May I know how these changes can be done in the kernel build to enable I2C2 ?


    I am testing VIP/VPE applications on GLSDK 6.04 release.

    But I don't understand the beahviour in my target , could you explain  if I2C2 module is not enabled , then how could the LVDS cameras works in my target when running vip applications dmabuftest & v4l2capturedisplay, eventhough all cameras doesn't probe successfully it manages to register video driver for atleast 1 or 2 cameras in random.In the Dra7xx developers guide it has mentioned that it should be able to probe i2c2 slave for all the LVDS  cameras connected.

    During the kernel startup some of the i2c config messages , are these for i2c-1 ?

    [    2.492279] i2c /dev entries driver
    [    2.498504] i2c 1-0031: Writing addr = 14, data = f4
    [    2.503936] i2c 1-0031: Writing addr = 15, data = f6
    [    2.509368] i2c 1-0031: Writing addr = 16, data = f8
    [    2.514770] i2c 1-0031: Writing addr = 17, data = fa
    [    2.520141] i2c 1-0031: Writing addr = 18, data = fc
    [    2.525543] i2c 1-0031: Writing addr = 19, data = fe
    [    2.531921] i2c_expander 1-0027: Writing addr = 0, data = 0
    [    2.537963] i2c_expander 1-0027: Writing addr = c, data = 0
    [    2.543975] i2c_expander 1-0027: Writing addr = 12, data = 63
    [    2.550201] i2c_expander 1-0027: Writing addr = 12, data = e3
    [    2.556427] i2c_expander 1-0027: Writing addr = 1, data = 0
    [    2.562469] i2c_expander 1-0027: Writing addr = d, data = 0
    [    2.568511] i2c_expander 1-0027: Writing addr = 13, data = 63
    [    2.574707] i2c_expander 1-0027: Writing addr = 13, data = e3
    [    2.581939] i2c_expander 1-0027: i2c expander initialized
    [    2.587738] i2c 1-0031: Writing addr = 14, data = f4
    [    2.593109] i2c 1-0031: Writing addr = 15, data = f6
    [    2.598480] i2c 1-0031: Writing addr = 16, data = f8
    [    2.603881] i2c 1-0031: Writing addr = 17, data = fa
    [    2.609283] i2c 1-0031: Writing addr = 18, data = fc
    [    2.614654] i2c 1-0031: Writing addr = 19, data = fe
    [    2.621063] i2c_expander 1-0021: Writing addr = 0, data = 0
    [    2.627105] i2c_expander 1-0021: Writing addr = c, data = 0
    [    2.633148] i2c_expander 1-0021: Writing addr = 12, data = 63
    [    2.639373] i2c_expander 1-0021: Writing addr = 12, data = e3
    [    2.645568] i2c_expander 1-0021: Writing addr = 1, data = 0
    [    2.651611] i2c_expander 1-0021: Writing addr = d, data = 0
    [    2.657653] i2c_expander 1-0021: Writing addr = 13, data = 63
    [    2.663879] i2c_expander 1-0021: Writing addr = 13, data = e3
    [    2.671051] i2c_expander 1-0021: i2c expander initialized
    [    2.676849] i2c 1-0031: Writing addr = 14, data = f4
    [    2.682250] i2c 1-0031: Writing addr = 15, data = f6
    [    2.687652] i2c 1-0031: Writing addr = 16, data = f8
    [    2.693023] i2c 1-0031: Writing addr = 17, data = fa
    [    2.698425] i2c 1-0031: Writing addr = 18, data = fc
    [    2.703826] i2c 1-0031: Writing addr = 19, data = fe
    [    2.710205] i2c_expander 1-0025: Writing addr = 0, data = 0
    [    2.716247] i2c_expander 1-0025: Writing addr = c, data = 0
    [    2.722290] i2c_expander 1-0025: Writing addr = 12, data = 63
    [    2.728515] i2c_expander 1-0025: Writing addr = 12, data = e3
    [    2.734741] i2c_expander 1-0025: Writing addr = 1, data = 0
    [    2.740783] i2c_expander 1-0025: Writing addr = d, data = 0
    [    2.746795] i2c_expander 1-0025: Writing addr = 13, data = 63
    [    2.753021] i2c_expander 1-0025: Writing addr = 13, data = e3
    [    2.760223] i2c_expander 1-0025: i2c expander initialized

    Thanks,

    Kanagarajan

  • Hello Kanagarajan,

    I2C2 module in your configuration is 0x2: Module is in Idle mode (only OCP part). It is functional if using separate functional clock.

    I2C2 module has: L4PER_L3_GICLK  - Interface clock

                                         PER_96M_GFCLK - Functional clock

    It seems that L3 GICLK is not enabled in your configuration

    /* i2c2 */

    static struct omap_hwmod dra7xx_i2c2_hwmod = {

    .name = "i2c2",

    .class = &dra7xx_i2c_hwmod_class,

    .clkdm_name = "l4per_clkdm",

    .flags = HWMOD_16BIT_REG | HWMOD_SET_DEFAULT_CLOCKACT,

    .prcm = {

    .omap4 = {

    .clkctrl_offs = DRA7XX_CM_L4PER_I2C2_CLKCTRL_OFFSET,

    .context_offs = DRA7XX_RM_L4PER_I2C2_CONTEXT_OFFSET,

    .modulemode   = MODULEMODE_SWCTRL,

    },

    },

    .dev_attr = &i2c_dev_attr,

    };

    #Q: I2C1 module is enabled during the kernel startup itself could find in the log  below and why it fails to do the same for I2C2 ?

    It seems that your problem is caused by conflict between I2C2 module and other module in DRA7xx EVM.

    Please run following commands to enable I2C2:

    target# devmem2 0x4a003808 w 0x60000
    target# devmem2 0x4a00380C w 0x60000
    target# devmem2 0x4847C010 w 0x4
    target# devmem2 0x4847C014 w 0x0
    
    Best regards,
    Yanko