Other Parts Discussed in Thread: TMS320C6748, OMAPL138, SYSBIOS
Hi,
I downloaded the software for TMS320C6748 SYS/BIOS Software Development Kit (SDK). I then created a new project in CCS for IO_Stream example for OMAPL137 (not for DSP core but just for ARM 9 - single core). At the moment I just want to test the UART functionality of OMAPL137. I then selected all the RTSC options available. When I build this project it fails with the following 2 errors:
1. fatal error #1965: cannot open source file "C:/...../Debug/configPkg/package/cfg/stream_pe9.h"
2. can't find the library 'lib/ti.targets.arm.rtsarm.ae9' specified by pakage ti.targets.arm.rtsarm. It was'nt found along the path '.....'.
Is there something that I am missing here. I just want to build a UART example.