Hello.
I've seen this problem raised in relation to many other processors:
And here is the Wiki guide:
processors.wiki.ti.com/.../Accessing_c_int00
But I still can't make any progress.
I need to place somehow the entry point of the ARM code at the address 0x40200000, but I don't know what I should add to the linker command file.
I understand I should follow this syntax:
boot > 0x1234
{
-l rts55.lib<boot.obj>(.text)
}
but I don't know what library (instead of "rts55.lib") I'm supposed to use that would contain "boot.obj" and correspond to Cortex-A8.
Thank you very much in advance.