I imported a CCS V3.1 project in CCS V5.2 using the "Import Legacy CCSv3.3 Project" option in CCS V5.2.
My project shows the CDB file from the CCS V3.1 project.
I converted the CDB file to a TCF file using cdb2tcf.exe.
A TCF file was created in the same directory as the old CDB file and the CDB file was renamed.
How do I get the TCF file into and connected to the project and do I get rid of the CDB file (a simple add files, delete files)?
Once in the project, how do I access the TCF file to allow me to add SECTIONS and change the properties?