Hi All...
I'm using Faxlib (faxlib_C55_CPU3_2_1_0_1) on 5535 Ezdsp with DSP/BIOS.
I'm using the example project and source files. I'm trying to feed the DIS packets at the "siuNetInterface". The DIS packet file used is given below for reference:
000001060000
000001060000
000001060000
000001060000
000001060000
000001060000
0001010600010100
000101060000
000101060000
000101060000
000101060000
000101060000
000101060000
000101060000
000101060000
000101060000
000101060000
000101060000
000101060000
000101060000
000206c001800000ff
000306c001800000c0
000406c00180000002
000506c00180000004
000606c00180000004
000706c00180000004
000806c00180000004
000906c00180000004
000a06c00180000004
000b06c00180000004
000c06c00180000004
000d06c00180000004
000e06c00180000004
000f06c00180000004
001006c00180000004
001106c00180000004
001206c00180000004
001306c00180000004
001406c00180000004
001506c00180000004
001606c0018000002c
001706c0018000000c
001807c0028000008c20
001807c0028000008c20
001906c001800000ff
001a06c001800000c8
001b06c00180000001
001c06c00180000000
001d06c00180000076
001e06c0018000005f
001f06c00180000001
002006c00180000001
002106c001800000f9
002206c00180000001
002306c00180000001
002406c00180000001
002507c0028000000020
002603c00110
002701000000
002701000000
002701000000
002701000000
002701000000
After getting the 7th packet i.e., "0001010600010100", it fmSendOut starts playing the preamble but it plays for infinite duration. The fmSendIn and in turn the fiu doesn't produce any more packets. It will never come to the "siuNetInterface" module...so no new packets will be read from "000206c001800000ff" onwards...
I guess a similar issue was discussed in the below thread but could not make out what the issue is.

I have not changed any of the fmopen or fiuopen initializations from the example.
Please help me out.
Thanks & regards,
Ashok