Hello Folks,
Approach1:12MP resolution camera module+DM8168
1. whether DM8168 can interface 12MP resolution camera?
2. what is the maximum resolution image can be captured?
3. Since DM8168 has two video input port support ,can we split up one 12MP resolution image into two and combine it inside the chip?Is there any limitation?
Approach2: 12MP resolution camera sensor+SN65LVDS324+DM8168
1. Whether this approach is feasible for 4k x 3k resolution capture mode? Is there any limitation?
2. Whether SN65LVDS324 output resolution is max. 1080p60?
Below is the link for sony CMOS image sensor considered:
Attached the throughput calculation for the 2nd approach.
Please provide your valuable comments.
DM8168_LVDS324throughputcalc_280115.pdf
Please suggest any other alternatives for 12MP resolution camera module interface to DM8168
Thanks,
Srijan