This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Trouble with Noise/ wrong configuration?

Other Parts Discussed in Thread: OMAPL138

Hi, 

 I'm working on LCDK6748 with TIRTOS v. 2.0.1.23 , XDC 3.30.3.47 and CCS v6.0.1.00040. Codec is AIC3106 and DSP is OMAPL138. I wrote a simple program to perform Audio Echo chanel sample by sample.  I'm generating sine wave with 400Hz and amplitude 390mV. My code alows me to acquire sine wave :   

,but returned signal  is heavily distorted :  

I have no idea what is the issue of this distortion. Is anybody have any clue what am I doing wrong? Below  I attach file with my init codes for McAsp, codec and with main(). 

Thanks,

Best Regards

Mirek  

int main(void)
{
	/*PinMuxSetup for all peripherals*/
    I2CPinMuxSetup(0);
    McASPPinMuxSetup();

    /*PowerUp modules */
   PSCModuleControl(SOC_PSC_1_REGS, HW_PSC_MCASP0, PSC_POWERDOMAIN_ALWAYS_ON,
	     PSC_MDCTL_NEXT_ENABLE);

	BIOS_start();
}


void runningThread(void)
{
	/* i2c init */
	I2CCodecIfInit(SOC_I2C_0_REGS ,INT_CHANNEL_I2C , I2C_SLAVE_CODEC_AIC31);
	/* codec configuration */
	codecInit();
	/* mcasp configuration */
	McASPConfigure();

	while(1)
	{
      /* loop */
	}
}


/* McAsp ISR */
void McASP_ISR(void)
{
	  Sample = McASPRxBufRead(SOC_MCASP_0_CTRL_REGS, MCASP_XSER_RX);
	  Swi_post(AudioSWI);
}

/* SWI */
void AudioProcessSWI(void)
{
	static UInt j =0,k =0;

	/* Data from left channel */
	if(HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RSLOT))
	{
	  Buffer[j]=(Int16)Sample;
	  //Sample = Buffer[j];
	   j+=1;
	   j= j%256;

	}
	else
	{
	  Buffer2[k]=(Int16)Sample;

	   k+=1;
	   k= k%256;
	   Sample = 0 ;
	}


  while(!(HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XSTAT)&0x20)); /* wait untill empty */
       McASPTxBufWrite(SOC_MCASP_0_CTRL_REGS, MCASP_XSER_TX,Sample);//(Int)sinetable[i]);
  while((HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XSTAT)&0x20)); /* wait untill full */
}


    /* AIC3106 configuration:  */

 /* Set the sample Rate */
    CodecRegWrite(baseAddr, AIC31_P0_REG2, 0x00);
  
    CodecRegWrite(baseAddr, AIC31_P0_REG3, 0x22);

    /* use PLL_CLK_IN as MCLK */
    CodecRegWrite(baseAddr, AIC31_P0_REG102, 0x00);

    /* Use PLL DIV OUT as codec CLK IN */
    CodecRegBitClr(baseAddr, AIC31_P0_REG101, 0x01);

    /* Select GPIO to output the divided PLL IN */
    //CodecRegWrite(baseAddr, AIC31_P0_REG98, 0x20);


    CodecRegWrite(baseAddr, AIC31_P0_REG4, 0x40);

    /* Configure the PLL divide registers */
    CodecRegWrite(baseAddr, AIC31_P0_REG5, 0x6D);
    CodecRegWrite(baseAddr, AIC31_P0_REG6, 0x60);

    CodecRegWrite(baseAddr, AIC31_P0_REG11, 0x01);

    /* Enable the codec to be master for fs and bclk */
    CodecRegWrite(baseAddr, AIC31_P0_REG8, 0x00); /* Slave Mode */
    //CodecRegWrite(baseAddr, AIC31_P0_REG8, 0xD0);  /* Master Mode */

    CodecRegWrite(baseAddr, AIC31_P0_REG7, 0x0A);

    /* Write the data type and  slot width */
    CodecRegWrite(baseAddr, AIC31_P0_REG9, 0x06);
  
    /* valid data after dataOff number of clock cycles */
    CodecRegWrite(baseAddr, AIC31_P0_REG10, 0x00);


	/* ADC Mono */
    /* enable the programmable PGA for left and right ADC  */
    CodecRegWrite(baseAddr, AIC31_P0_REG15, 0x00);
    CodecRegWrite(baseAddr, AIC31_P0_REG16, 0x80); /* Right ADC is muted  */


    /* power off the Line L1L */
    CodecRegWrite(baseAddr, AIC31_P0_REG19, 0x04);

    /* power on the Line LIR */
    CodecRegWrite(baseAddr, AIC31_P0_REG22, 0x00);



    /* power up the left and right(off) DACs */
    CodecRegWrite(baseAddr, AIC31_P0_REG37, 0xA0);

    /* select the DAC L1 R1 Paths */
    CodecRegWrite(baseAddr, AIC31_P0_REG41, 0x00); /* Mono settings */
    CodecRegWrite(baseAddr, AIC31_P0_REG42, 0x6C); /* Driver power-on time/ ramp-up step time*/


    /* DAC L to HPLOUT Is NOT connected */
    CodecRegWrite(baseAddr, AIC31_P0_REG47, 0x7F);
    CodecRegWrite(baseAddr, AIC31_P0_REG51, 0x7F);/* is off*/

    /* DAC R to HPROUT is NOT connected */
    CodecRegWrite(baseAddr, AIC31_P0_REG64, 0x7F);
    CodecRegWrite(baseAddr, AIC31_P0_REG65, 0x7F); /* is off */

    /* DACL1 connected to LINE1 LOUT */
    CodecRegWrite(baseAddr, AIC31_P0_REG82, 0x80); /* DAC_L1 is connected */
    CodecRegWrite(baseAddr, AIC31_P0_REG86, 0x09); /* unmuted/power on */

    /* DACR1 connected to LINE1 ROUT */
    CodecRegWrite(baseAddr, AIC31_P0_REG92, 0x00); /* DAC_R1 is not connected */
    CodecRegWrite(baseAddr, AIC31_P0_REG93, 0x00); /* muted/power off */

    /* unmute the DAC */
    CodecRegWrite(baseAddr, AIC31_P0_REG43, 0x00);/* left channel is mute */
    CodecRegWrite(baseAddr, AIC31_P0_REG44, 0x80);



  /* McASP configuration: */
  
  /* reset MCasp (GBLCTL) */
    HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RGBLCTL)= 0;
    HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XGBLCTL) = 0;

   /* Receiver configuration */
   /* Configure Mask */
    HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RMASK) = 0x0000FFFF;
   /* Configure format of receive section */
    HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RFMT) = 0x0001807C; /* 1 bit delay/MSB/slot size 16bit/read from Periph */
   /* Clocks control */
    HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_AFSRCTL) = 0x00000112; /* I2S mode/ internal frame clock/ rising edge */
    HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_ACLKRCTL) = 0x000000AF; /* rising edge/ Divide by 16  */
    HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_AHCLKRCTL) = 0x00000000; /* Divide by 1/ clock source from AUCLKX */
   /* Set Active Slots */
    HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RTDM) = 0x00000003;
    /* Configure receiver clock check circuit */
    HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RCLKCHK) = 0x00FF0008;

    /* Transmitter configuration */
    /* Configure Mask */
     HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XMASK) = 0x0000FFFF;
    /* Configure format of transmitt section */
     HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XFMT) = 0x0001807C;  /* 1 bit delay/MSB/slot size 16bit/read from Periph */
    /* Clocks control */
     HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_AFSXCTL) = 0x00000112; /* I2S mode/ internal frame clock/ rising edge */
     HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_ACLKXCTL) = 0x000000AF;
     HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_AHCLKXCTL) = 0x00000000;
    /* Set Active Slots */
     HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XTDM) = 0x00000003;
     /* Configure transmitter clock check circuit */
     HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XCLKCHK) = 0x00FF0008;

     /* Set serializers numbers */
     HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_SRCTL(13u)) = 0x0000000D; /* Set serializer13 as transmitter */
     HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_SRCTL(14u)) = 0x0000000E; /* Set serializer13 as receiver */

     /* Configure pins */
     /* Set McASP as GPIO */
     HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_PFUNC) = 0;
     /* Set Pins Direction */
     HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_PDIR) = 0x14002000;
     /* Enable DIT mode transmission */
     HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_DITCTL) = 0x00000000;
     /* Enable DLB mode transmission */
     HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_DLBCTL) = 0x00000000;
     /* Configure McAsp Mute */
     HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_AMUTE) = 0x00000000; /* if clk clock failed set mute */
	 
	 
	  /* Start McAsp :  */
	 
	 
	   /* Transmit high-frequency clock divider is running */
	HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_XGBLCTL) |= 0x00000200; /* XHCLKRST */
	/* Wait untill it's working */
	while(!(HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_XGBLCTL)&(0x00000200)));

	/* Receive high-frequency clock divider is running */
	HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_RGBLCTL) |= 0x00000002; /* RHCLKRST */
	/* Wait untill it's working */
	while(!(HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_RGBLCTL)&(0x00000002)));

	/* Transmit clock divider is running*/
	HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_XGBLCTL) |= 0x00000100; /* XCLKRST */
	/* Wait untill it's working */
	while(!(HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_XGBLCTL)&&0x00000100));

	/* Receive clock divider is running*/
	HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_RGBLCTL) |= 0x00000001; /* RCLKRST */
	/* Wait untill it's working */
	while(!(HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_RGBLCTL)&&0x00000001));


	 /* Set Interrupts */
	 HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RINTCTL) = 0x00000020; /* Data ready Interrupt */
	 HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XINTCTL) = 0x00000020; /* Transmit Data ready/ Sync Frame Start Interrupts */

	 HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RSTAT) = 0x0000FFFF; /* Clear Receiver Status Register */
	 HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XSTAT) = 0x0000FFFF; /* Clear Transmitter Status Register */


    /* Transmit serializers are active */
	HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_XGBLCTL) |= 0x00000400; /* XSRLCR */
	/* Wait untill it's working */
	while(!(HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_XGBLCTL)&(0x00000400)));

	/* Receive serializers are active */
	HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_RGBLCTL) |= 0x00000004; /* RSRLCR */
	/* Wait untill it's working */
	while(!(HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_RGBLCTL)&(0x00000004)));

	/* Send 0, so that no underrun occurs after releasing the staet machine */
	McASPTxBufWrite(SOC_MCASP_0_CTRL_REGS, MCASP_XSER_TX, 0);

    /* Transmit state machine is released from reset */
	HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_XGBLCTL) |= 0x00000800; /* XSMRST */
	/* Wait untill it's working */
	while(!(HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_XGBLCTL)&(0x00000800)));

	/* Receive state machine is released from reset */
	HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_RGBLCTL) |= 0x00000008; /* RSMRST */
	/* Wait untill it's working */
	while(!(HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_RGBLCTL)&(0x00000008)));


    /* Transmit frame sync generator is active */
	HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_XGBLCTL) |= 0x00001000; /* XFRST */
	/* Wait untill it's working */
	while(!(HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_XGBLCTL)&(0x00001000)));

	/* Receive frame sync generator is active */
	HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_RGBLCTL) |= 0x00000010; /* RFRST */
	/* Wait untill it's working */
	while(!(HWREG(SOC_MCASP_0_CTRL_REGS +  MCASP_RGBLCTL)&(0x00000010)));

	while(!(HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XSTAT)&0x20));
	McASPTxBufWrite(SOC_MCASP_0_CTRL_REGS, MCASP_XSER_TX, 0);
	 

  • Hi,

    Thanks for your post.

    I think, you have to tune your DAC codec register configuration since it has more probability to append more noise & distortion on DAC. Could you please tune & validate your DAC codec register configuration with your AIC3106 codec datasheet? Please tune the below DAC L & R codec registers to LINEOUT & HPOUT:

    /* DAC L to HPLOUT Is NOT connected */

       CodecRegWrite(baseAddr, AIC31_P0_REG47, 0x7F);

       CodecRegWrite(baseAddr, AIC31_P0_REG51, 0x7F);/* is off*/

       /* DAC R to HPROUT is NOT connected */

       CodecRegWrite(baseAddr, AIC31_P0_REG64, 0x7F);

       CodecRegWrite(baseAddr, AIC31_P0_REG65, 0x7F); /* is off */

       /* DACL1 connected to LINE1 LOUT */

       CodecRegWrite(baseAddr, AIC31_P0_REG82, 0x80); /* DAC_L1 is connected */

       CodecRegWrite(baseAddr, AIC31_P0_REG86, 0x09); /* unmuted/power on */

       /* DACR1 connected to LINE1 ROUT */

       CodecRegWrite(baseAddr, AIC31_P0_REG92, 0x00); /* DAC_R1 is not connected */

       CodecRegWrite(baseAddr, AIC31_P0_REG93, 0x00); /* muted/power off */

    Also, please follow the McASP initialization sequence mentioned as per mentioned in the TRM and kindly ensure  your McASP configuration is compliant to the initialization sequence as per section 23.2.4.1 mentioned in the c6748 TRM below which really matters in tuning audio ouput with out noise and distortion:

    http://www.ti.com/lit/ug/spruh79a/spruh79a.pdf

    Kindly tune the McASP internal or external bit clock and high frequency master clock as well framesync to reduce ouput distortion. Please refer the TRM above for more details

    Thanks & regads,

    Sivaraj K

    -------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question

    -------------------------------------------------------------------------------------------------------