Hi Experts,
I am using AM335x EVMSK, Linux SDK 7.0 with 3.12 kernel.
When I tried disabling the USB gadget mode in the meun config, then the Inventra driver options disappears in the Host side as well.
But I need only the host functionality. So I chose the Host Only mode in the Inventra driver options.
How the Gadget driver options and the host driver options are linked together ?
Is it like the OTG functionality is kept under the control of the USB Gadget ?