This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

pandaboard ES Ver.B3 Long packet



Hello,

DSI's long packet has 65541 bytes,

But I send a long packet with 5800 bytes.

Minicom said, my packet is too long.

How many is the maximum number of long packet?

THX

  • Hi Yuan-Heng,

    Is this the message you are observing? 

    if (dsi->vc[channel].tx_fifo_size * 32 * 4 < len + 4) {

                   DSSERR("unable to send long packet: packet too long.\n");

                  return -EINVAL;

           }

    You must check the size of your buffer also. It might be  because it is limited to specific threshold. If that is the case I suggest you increase it.

    Regards,

    Boyko

  • I declare "int length=0; " and add source code "length=vc[channel].tx_fifo_size * 32 * 4 ; ".
    But compiling , I have a error. What error happen ? Is datatype not match ?