This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

zImage of Linux 3.14 replaced into Linux SDK 7.0 doesn't works

Hi Experts,

I have the SD card flashed with LInux SDK 7.0 3.12 kernel with rootfs and boot partitions for AM335x EVM.

When I tried replacing the zImage alone with the Linux 3.14 kernel into /rootfs/boot/zImage-xx

But the kernel doesn't starts.


What are all the things which needs to be changed on flashing new zImage.


Example :

zImage

dtb

u-boot.img

MLO