Hello everybody,
I am developing a DSP/BIOS based application on the c5517 chip. For several reasons I have to insert custom dedicated sections in the memory map (for example, a DARAM block entirely dedicated to a timing critical buffer).
When I open the .tcf file though, in the Memory Section Manager, I see that the base addresses listed for every native memory sections are different than the ones specified in the datasheet. For example:
DARAM:
DSP/BIOS base address: 0x60
Datasheet base address: 0xC0
SARAM:
DSP/BIOS base address: 0x8000
Datasheet base address: 0x10000
Could anybody explain why this happens and, if it is a problem, how to solve it? thank you very much