I can't understand the instruction about BCC L8, cond of c55x.
Opcode : L8 0000 010E xCCC CCCC LLLL LLLL
Operands : cond, Lx
Description: This instruction evaluates a single condition defined by the cond field in the
read phase of the pipeline. If the condition is true, a branch occurs to the
program address label assembled into Lx.
the disassembly address and instruction about the Bcc L8, cond .
This instruction evaluates a single condition defined by the cond field in the
read phase of the pipeline. If the condition is true, a branch occurs to the
program address label assembled into l4.
0028b1: 368f NOT AR0,AR7
0028b3: 040f29 BCC #0x0028df,AR7 == #0
0028b6: aa03 MOV *AR0+,AR2
0028b8: 040a24 BCC #0x0028df,AR2 == #0
#0x0028df is what and how get it?
thanks .