This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The CVDD condition for TMS320C6454.

Other Parts Discussed in Thread: TMS320C6454

Hi,
I want to confirm the CVDD Condition for TMS320C6454.
SPRS311I  (6.2 Recommended Operating Conditions) Mentioned CVDD as 
Following.
 1000 MHz → 1.25V
  850 MHz → 1.20V
  720 MHz → 1.20V
We want to use 1Ghz Device in 850Mhz Operation.
In this case.CVDD is 1.25v or 1.20 v?
Best Regards