This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[DM365] Is there any new toolchain version for fix the security hole [CVE-2015-0235]



Dear All

Our DM365 platform are using  "arm-davinci-linux-gnueabi" toolchain which using glibc V2.6 which have the GHOST security hole [CVE-2015-0235],

Is there any new version of toolchain or glibc library available to fix it?

Or anyother way to fix this issue?

TheGHOST security hole [CVE-2015-0235]:

http://grahamcluley.com/2015/01/ghost-vulnerability-faq/