Hi,
I met a issue with your document( http://processors.wiki.ti.com/index.php/Optimize_Linux_Boot_Time )
U-Boot SPL 2013.01.01-00123-g2830d15-dirty (Feb 04 2015 - 03:24:56)
OMAP SD/MMC: 0
reading u-boot.img
reading u-boot.img
U-Boot 2013.01.01-00123-g2830d15-dirty (Feb 04 2015 - 03:24:56)
I2C: ready
DRAM: 256 MiB
WARNING: Caches not enabled
NAND: No NAND device found!!!
0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - readenv() failed, using default environment
Hit any key to stop autoboot: 0
mmc0 is current device
Unknown command 'if' - try 'help'
Unknown command 'then' - try 'help'
Unknown command 'if' - try 'help'
Unknown command 'then' - try 'help'
Importing environment from mmc ...
Unknown command 'fi' - try 'help'
Unknown command 'if' - try 'help'
Unknown command 'then' - try 'help'
## Error: "uenvcmd" not defined
Unknown command 'fi' - try 'help'
Unknown command 'if' - try 'help'
Unknown command 'then' - try 'help'
Unknown command 'elif' - try 'help'
Unknown command 'then' - try 'help'
Unknown command 'else' - try 'help'
Unknown command 'fi' - try 'help'
Unknown command 'else' - try 'help'
Unknown command 'fi' - try 'help'
U-Boot#
Could you please give any solution for me ?
Thanks,
Carl