This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ata driver c55x in CSL



Hi,

I'm using the ATA - Driver of the latest CSL both on C5515 and now also C5534.

This works just fine, but I wonder if I can somehow change the date and time of a file which I create with that driver. I see, there is a time and date field in  struct CSL_MMCCardObj, but these are always zero. I see an get_time and get:_date function pointer, but this seem to point nowhere.


However, if I open an saved file, the data field Time and Date of CSL_MMCCardObj do have some values unequal zero. Can I change this date and time fields of a new file somehow?

Thanks

Micky